4.2. CDD_IPC¶
4.2.1. Introduction¶
This document describes the functionality, API and configuration of the AUTOSAR BSW module Complex Device driver for IPC on AM263px device.
- Supported AUTOSAR Release:
4.3.1
- Supported Configuration Variants:
Post-Build
- Vendor ID:
CDD_IPC_VENDOR_ID (44)
- Module ID:
CDD_IPC_MODULE_ID (255)
- Supported Platform:
AM263px
The Complex Device Driver main tasks are the following:
Initialization of the mailbox driver
Simplifies reading and writing to the mailbox peripheral.
4.2.2. Complex Device Driver Architecture¶
The following figure shows where the Complex device driver is located in the AUTOSAR architecture.
Fig. 4.1 CDD in AUTOSAR architecture¶
4.2.3. Functional Description¶
4.2.3.1. Features Supported and Not Supported¶
Supported |
Not Supported |
|---|---|
Open/Close mailbox instance |
Multiple mailbox channels between the cores. |
Send/Receive both Notify and RpMsg messages. |
Applications are validated only for the R50_0 core |
RpMsg Callback functionality supported |
4.2.3.2. Initialization¶
The initialization covers the following steps
Initialize the mailbox peripheral
Cdd_Ipc_Init should be called only once during initialization.
No other CDD API can be invoked until this API is called.
4.2.3.3. Error Handling¶
4.2.3.3.1. Development Errors¶
Development errors are reported to the DET using the service Det_ReportError() if development error reporting is enabled (i.e. pre-compile parameter CDD_IPC_DEV_ERROR_DETECT== STD_ON). The reported service IDs identify the services which are described in 3.4. The following table presents the service IDs and the related services
The errors reported to DET and DEM are described in the following table
Error Code |
Symbolic Name |
Description |
|---|---|---|
0x01U |
CDD_IPC_E_UNINIT |
Error code indicating the IPC is uninitialized |
0x02U |
CDD_IPC_E_REGISTER_CLIENT_FAILED |
Error code indicating register client failed event |
0x03U |
CDD_IPC_E_INIT_FAILED |
Error code indicating IPC Initilization Failed |
0x04U |
CDD_IPC_E_DEINIT_FAILED |
Error code indicating IPC Deinitilization Failed |
0x05U |
CDD_IPC_E_PARAM_POINTER |
Error code indicating invalid parameter |
0x06U |
CDD_IPC_E_ALREADY_INITIALIZED |
Error code indicating IPC already initialized |
0x07U |
CDD_IPC_E_PARAM_VALUE |
Error code indicating Service called with wrong param |
0x08U |
CDD_IPC_E_PARAM_LENGTH |
Error code indicating Service called with invalid length |
0x09U |
CDD_IPC_E_INVALID_CHANNEL |
Error code indicating invalid IPC Channel |
0x0AU |
CDD_IPC_E_INVALID_CONFIG |
Error code indicating invalid IPC configuration |
0x0BU |
CDD_IPC_E_WRITE_FAILED |
Error code indicating IPC Write Failed configuration |
0x0CU |
CDD_IPC_E_UNREGISTER_CLIENT_FAILED |
Error code indicating unregister client failed event |
0x0DU |
CDD_IPC_E_CONSTRUCT_FAILED |
Error code indicating construct failed event |
0x0EU |
CDD_IPC_E_RPMSG_WRITE_FAILED |
Error code indicating RpMsg Write failed event |
0x0FU |
CDD_IPC_E_RPMSG_READ_FAILED |
Error code indicating Rpmsg read failed event |
0x10U |
CDD_IPC_E_DESTRUCT_FAILED |
Error code indicating destruct failed event |
4.2.3.3.2. Parameter Checking¶
AUTOSAR requires that API functions check the validity of their parameters. These checks are for development error reporting and can be en-/disabled via the parameter CDD_IPC_DEV_ERROR_DETECT. The following table shows which parameter checks are performed on which services:
Services |
CDD_IPC_E_UNINIT |
CDD_IPC_E_REGISTER_CLIENT_FAILED |
CDD_IPC_E_UNREGISTER_CLIENT_FAILED |
CDD_IPC_E_PARAM_POINTER |
CDD_IPC_E_ALREADY_INITIALIZED |
CDD_IPC_E_PARAM_VALUE |
CDD_IPC_E_WRITE_FAILED |
CDD_IPC_E_CONSTRUCT_FAILED |
CDD_IPC_E_RPMSG_WRITE_FAILED |
CDD_IPC_E_RPMSG_READ_FAILED |
|---|---|---|---|---|---|---|---|---|---|---|
Cdd_Ipc_Init |
● |
● |
||||||||
Cdd_Ipc_DeInit |
● |
● |
||||||||
Cdd_Ipc_Notify_RegisterClient |
● |
● |
● |
|||||||
Cdd_Ipc_Notify_UnregisterClient |
● |
● |
● |
|||||||
Cdd_Ipc_Notify_Write |
● |
● |
● |
● |
||||||
Cdd_Ipc_Construct |
● |
● |
||||||||
Cdd_Ipc_Destruct |
● |
● |
||||||||
Cdd_Ipc_RpMsg_SendMsg |
● |
● |
● |
|||||||
Cdd_Ipc_RpMsg_RecvMsg |
● |
● |
● |
4.2.3.4. Scope of Delivery¶
File Name |
Description |
|---|---|
Cdd_Ipc.h |
This file contains interface header for Complex device driver for IPC |
Cdd_Ipc_Irq.h |
This file contains ISR function declaration for Complex Device Driver |
Cdd_Ipc.c |
This file contains function definitions for the Complex device driver for IPC and helper functions. |
Cdd_Ipc_Irq.c |
This file contains ISR function definitions for Complex Device Driver |
4.2.4. Include Structure¶
Fig. 4.2 CDD header file include structure¶
4.2.5. Memory mapping¶
Memory Mapping Sections |
CDD_CODE |
CDD_CODE_ISR |
CDD_VAR_NO_INIT |
CDD_VAR_ZERO_INIT |
|---|---|---|---|---|
CDD_IPC_START_SEC_VAR_INIT_UNSPECIFIED(.bss) CDD_IPC_STOP_SEC_VAR_INIT_UNSPECIFIED |
● |
|||
CDD_IPC_START_SEC_CODE_APPL(.text) CDD_IPC_STOP_SEC_CODE_APPL |
● |
|||
CDD_IPC_START_SEC_VAR_UNSPECIFIED(.data) CDD_IPC_STOP_SEC_VAR_UNSPECIFIED |
● |
|||
CDD_IPC_START_SEC_CODE(.text) CDD_IPC_START_SEC_CODE |
● |
4.2.6. Services used by Complex device Driver¶
The CDD does not provide any call back functions.
4.2.6.1. Notifications¶
At its configurable interfaces the CDD defines notifications that can be mapped to callback functions provided by other modules. The mapping is not statically defined by the CDD but can be performed at configuration time. The function prototypes that can be used for the configuration have to match the appropriate function prototype signatures, which are described in the following. Cdd_Ipc_notify_msgHandler: This is defined in the Cdd_Ipc_notify_app.c for reference.
Dependencies on SW modules
OSEK/AUTOSAR OS (Optional)
An operating system can be used for task scheduling, interrupt handling, global suspend and restore of interrupts and creating of the Interrupt Vector Table. The CDD module may use OSEK/AUTOSAR OS to suspend and restore global interrupts
DET (Optional)
The module CDD depends on the DET (by default) in order to report development errors. Detection and reporting of development errors can be enabled or disabled by the switch CDD_IPC_DEV_ERROR_DETECT = STD_ON in the Cdd_Ipc_Cfg.h o Critical Sections The mailbox operations like write, read are protected by a critical section.
Service ID |
Service |
|---|---|
0x01 |
Cdd_Ipc_Init |
0x02 |
Cdd_IpcGetVersionInfo |
0x03 |
Cdd_Ipc_RpMsg_RecvMsg |
0x04 |
Cdd_Ipc_RpMsg_SendMsg |
0x05 |
Cdd_Ipc_Notify_RegisterClient |
0x06 |
Cdd_Ipc_Construct |
0x07 |
Cdd_Ipc_DeInit |
0x09 |
Cdd_Ipc_Notify_UnregisterClient |
0x0A |
Cdd_Ipc_Destruct |
4.2.7. API Definition¶
Refer the MCAL_ApiGuide for API documentation and Type definition
4.2.7.1. Supported API’s¶
Cdd_Ipc_Init : This API will act as Service for CDD IPC Initialization.
Cdd_Ipc_DeInit : This API will act as Service for deinitializing CDD IPC.
Cdd_Ipc_Notify_RegisterClient : This API will act as Service to register a client for IPC.
Cdd_Ipc_Notify_UnregisterClient : This API will act as Service to un-register a client for IPC.
Cdd_Ipc_Notify_Write : This API will act as Service to write ipc notify message.
Cdd_Ipc_Construct : Used to Create a RPMessage object to receive messages at a specified end-point
Cdd_Ipc_Destruct : This API will act as Service to delete a previously created RPMessage object
Cdd_Ipc_RpMsg_SendMsg : This API will act as Service to Send a message to a remote core at a specified remote end point
Cdd_Ipc_RpMsg_RecvMsg : Blocking API to wait till a message is received from any CPU at the specified local end point.
Cdd_Ipc_Notify_SyncAll : This API will act as Service to sync all the cores that are participating in the IPC.
4.2.8. Configuration Parameter¶
There are following different parameter which user can configure from the EB tresos:
CddIpcTimeout : This parameter will help to configure timeout which will be used to terminate if our execution time exceed the timeout time.
CddIpcNumOfBuffers : This parameter will be used to configure number of buffer in VRING. And this parameter will be used in case of RPMsg transfer.
CddIpcMaxBufferSize : This parameter will be used to configure the size of the buffer in VRING.And this will also be used in case of RPMsg transfer.
CddIpcRpMsgEnable : This checkbox parameter will act as STD_ON/STD_OFF. So in case user want RPMsg enable then they can tick this otherwise in else case configuration will be generated considering notify transfer only.
CddIpcRecvCallBack : This parameter is used when user want to register a callback along with the RPMsg transfer.
CddIpcLocalCoreId : Used to select which coreID user want as a local core or the core on which MCAL will run.
CddIpcRemoteCoreList : In this user get option to select what all remote they want in there communication and accord’list all those under this list.
CddIpcEndPtConfig : This will suggest what EndPoint is used for the communication between the cores.
Note: In case of CddIpcRecvCallBack , when RPMsg arrive then that is invoked along with the data in the VRING buffer.So now if the msg size is less then what we are transfering between cores then we will send the echo msg back to the core from which we are receiving and will do UNLOCK of core only if complete msg transfer happens.So by this way we are acknowledging the remote core.
For details of configuration supported refer the MCAL_Configurator_UserGuide.pdf present in mcal_config/docs folder
4.2.9. Example Application¶
CDD example application demonstrating the Complex device driver features 2 different examples namely ipc_notify_app and ipc_rpmsg_app.
4.2.9.1. Ipc_notify_app_working¶
This application is low payload, low latency message type where user will be able to send a maximum of 28bits of data as the payload. The first 4 bits are used internally by the driver for the client ID. Notify app sends 1000000, to all the other 3 cores and waits for all of them to echo back. To make the example work with lesser cores, edit the following parameters in the example.
#define MAX 4To the number of cores user needs to reduce.uint32 gRemoteCoreId[];Enable only the cores that are required.uint32 gIpcTransferMutex[MAX]Remove the extra Lock variables (These can be replced with any kind of mutex or semaphore implementation at the user End)In addition to these please also ensure the Cdd_Ipc_PBCfg.c has the proper cores configured from the XDM file.
The same changes stand valid for the rpmsg_echo_app as well.
4.2.9.2. Ipc_rpmsg_app working¶
RpMsg application uses Vrings as the medium to send larger data whose size and buffer depth can be configured using the parameters CDD_IPC_NUM_OF_BUFFERS and CDD_IPC_MAX_BUFFER_SIZE
The application exchanges 100000 messages, the payload data is integer value where it gets incremented on every echo back from each core. In order to change the data from the integer to other data i.e., String or characters for command use-cases please change the following line
snprintf(msgBuf, MAX_MSG_SIZE-1, "%d", msg);
To
snprintf(msgBuf, MAX_MSG_SIZE-1, "%s", “Your String Data”);
The notify application is present under the path <MCAL_ROOT>/examples/Ipc/Ipc_app_notify. This
application can be built from the build folder by giving “gmake -s ipc_notify_app”.
The rpmsg application is present under the path <MCAL_ROOT>/examples/Ipc/Ipc_app_rpmsg. This
application can be built from the build folder by giving “gmake -s ipc_rpmsg_app”.
4.2.9.3. Changing and Compiling SDK examples:¶
Examples to import from SDK to validate the CDD_IPC example,
Use all the other cores except R50-0 (this is where CDD_IPC app will be run), the path to the examples inside MCU+SDK directory
$(MCU_PLUS_SDK_PATH)examplesdriversipcipc_notify_echoam263x-cc
$(MCU_PLUS_SDK_PATH) examplesdriversipcipc_rpmsg_echoam263x-cc
4.2.9.3.1. Notify App Sample Output:¶
4.2.9.3.2. RPMsg App Sample Output:¶