5.19. SPI

5.19.1. Types

Base type

Type Name

Brief

enum

Spi_HwUnitType

This type defines a range of specific status for SPI Handler/Driver.

enum

Spi_StatusType

enum

Spi_JobResultType

This type defines a range of specific Jobs status for SPI Handler/Driver.

enum

Spi_SeqResultType

This type defines a range of specific Sequences status for SPI Handler/Driver.

enum

Spi_HwUnitResultType

This type defines a range of specific HW unit status for SPI Handler/Driver.

enum

Spi_AsyncModeType

Specifies the asynchronous mechanism mode for SPI busses handled asynchronously in LEVEL 2.

enum

Spi_TransferType

Word transfer order - MSB first or LSB first.

enum

Spi_LevelType

Type for SPI Chip Select Polarity and Clock Idle Level.

enum

Spi_CsPinType

SPI Chip Select Pin.

enum

Spi_ClkMode

SPI Clock Mode - sets the clock polarity and phase. Note: These values are a direct register mapping. So don’t change value.

enum

Spi_TxRxMode

SPI TX/RX Mode.

enum

Spi_JobPriorityType

SPI Job Priority.

enum

Spi_CsModeType

SPI Chip Select Mode.

enum

Spi_DataDelayType

Spi_DataDelayType defines the number of interface clock cycles between CS toggling and first or last edge of MCSPI clock.

enum

Spi_DataLineReceiveType

Spi_DataLineReceiveType defines the lines selected for reception.

enum

Spi_DataLineTransmitType

Spi_DataLineTransmitType defines the lines selected for transmission.

enum

Mcspi_IrqStatusType

Irq status and std return type.

typedef void(*)(void)

Spi_JobEndNotifyType

Typedef for job end notification function pointer.

typedef void(*)(void)

Spi_SeqEndNotifyType

Typedef for sequence end notification function pointer.

5.19.1.1. enum Spi_HwUnitType

Enumerator

Value

Description

CSIB0

0U

MCSPI0 instance.

CSIB1

MCSPI1 instance.

CSIB2

MCSPI2 instance.

CSIB3

MCSPI3 instance.

Brief: This type defines a range of specific status for SPI Handler/Driver.

5.19.1.2. enum Spi_StatusType

Enumerator

Value

Description

SPI_UNINIT

0U

The SPI Handler/Driver is not initialized or not usable.

SPI_IDLE

1U

The SPI Handler/Driver is not currently transmitting any Job.

SPI_BUSY

2U

The SPI Handler/Driver is performing a SPI Job (transmit)

5.19.1.3. enum Spi_JobResultType

Enumerator

Value

Description

SPI_JOB_OK

0U

The last transmission of the Job has been finished successfully.

SPI_JOB_PENDING

1U

The SPI Handler/Driver is performing a SPI Job. The meaning of this status is equal to SPI_BUSY.

SPI_JOB_FAILED

2U

The last transmission of the Job has failed.

SPI_JOB_QUEUED

3U

An asynchronous transmit Job has been accepted, while actual transmission for this Job has not started yet.

Brief: This type defines a range of specific Jobs status for SPI Handler/Driver.

5.19.1.4. enum Spi_SeqResultType

Enumerator

Value

Description

SPI_SEQ_OK

0U

The last transmission of the Sequence has been finished successfully.

SPI_SEQ_PENDING

1U

The SPI Handler/Driver is performing a SPI Sequence. The meaning of this status is equal to SPI_BUSY.

SPI_SEQ_FAILED

2U

The last transmission of the Sequence has failed.

SPI_SEQ_CANCELLED

3U

The last transmission of the Sequence has been canceled by user.

Brief: This type defines a range of specific Sequences status for SPI Handler/Driver.

5.19.1.5. enum Spi_HwUnitResultType

Enumerator

Value

Description

SPI_HW_UNIT_OK

0U

HW unit result is ok.

SPI_HW_UNIT_PENDING

1U

HW unit result is pending.

SPI_HW_UNIT_FAILED

2U

HW unit result is failed.

Brief: This type defines a range of specific HW unit status for SPI Handler/Driver.

5.19.1.6. enum Spi_AsyncModeType

Enumerator

Value

Description

SPI_POLLING_MODE

0U

The asynchronous mechanism is ensured by polling, so interrupts related to SPI busses handled asynchronously are disabled.

SPI_INTERRUPT_MODE

1U

The asynchronous mechanism is ensured by interrupt, so interrupts related to SPI busses handled asynchronously are enabled.

Brief: Specifies the asynchronous mechanism mode for SPI busses handled asynchronously in LEVEL 2.

5.19.1.7. enum Spi_TransferType

Enumerator

Value

Description

SPI_MSB

0U

MSB is transferred first. Only this is supported.

SPI_LSB

1U

LSB is transferred first. This is not supported.

Brief: Word transfer order - MSB first or LSB first.

5.19.1.8. enum Spi_LevelType

Enumerator

Value

Description

SPI_LOW

(0x00U)

Low clock or chip select.

SPI_HIGH

High clock or chip select.

Brief: Type for SPI Chip Select Polarity and Clock Idle Level.

5.19.1.9. enum Spi_CsPinType

Enumerator

Value

Description

SPI_CS0

0U

Chip select 0.

SPI_CS1

Chip select 1.

SPI_CS2

Chip select 2.

SPI_CS3

Chip select 3.

Brief: SPI Chip Select Pin.

5.19.1.10. enum Spi_ClkMode

Enumerator

Value

Description

SPI_CLK_MODE_0

0x00U

SPI Clock Phase = 0 (rising edge latch), Polarity = 0 (Active HIGH)

SPI_CLK_MODE_1

0x01U

SPI Clock Phase = 1 (falling edge latch), Polarity = 0 (Active HIGH)

SPI_CLK_MODE_2

0x02U

SPI Clock Phase = 0 (rising edge latch), Polarity = 1 (Active LOW)

SPI_CLK_MODE_3

0x03U

SPI Clock Phase = 1 (falling edge latch), Polarity = 1 (Active LOW)

Brief: SPI Clock Mode - sets the clock polarity and phase. Note: These values are a direct register mapping. So don’t change value.

5.19.1.11. enum Spi_TxRxMode

Enumerator

Value

Description

SPI_TX_RX_MODE_BOTH

0x00U

Both TX and RX are enabled.

SPI_TX_RX_MODE_TX_ONLY

0x02U

Only TX is enabled.

Brief: SPI TX/RX Mode.

Note:

  1. These values are a direct register mapping. So don’t change value

  2. RX only mode doesn’t make sense in master mode because to receive data the master has to generate clock, which means it should transmit. Hence this mode is not supported. The user can alternatively set the TX buffer pointer to NULL and set the default TX value (defaultTxData) to make TX data line at the desired level.

5.19.1.12. enum Spi_JobPriorityType

Enumerator

Value

Description

SPI_JOB_PRIORITY_0

0U

Job priority 0 - low.

SPI_JOB_PRIORITY_1

Job priority 1.

SPI_JOB_PRIORITY_2

Job priority 2.

SPI_JOB_PRIORITY_3

Job priority 3 - High.

Brief: SPI Job Priority.

5.19.1.13. enum Spi_CsModeType

Enumerator

Value

Description

SPI_SINGLE

0U

Chip select mode - single. Active only when transfer is on.

SPI_CONTINUOUS

1U

Chip select mode - continuous. Active throughout.

Brief: SPI Chip Select Mode.

5.19.1.14. enum Spi_DataDelayType

Enumerator

Value

Description

SPI_DATADELAY_0

0U

0.5 clock cycles delay

SPI_DATADELAY_1

1U

1.5 clock cycles delay

SPI_DATADELAY_2

2U

2.5 clock cycles delay

SPI_DATADELAY_3

3U

3.5 clock cycles delay

Brief: Spi_DataDelayType defines the number of interface clock cycles between CS toggling and first or last edge of MCSPI clock.

5.19.1.15. enum Spi_DataLineReceiveType

Enumerator

Value

Description

DATA_LINE_0_RECEPTION

0U

Data line 0 (SPIDAT[0]) selected for reception.

DATA_LINE_1_RECEPTION

1U

Data line 1 (SPIDAT[1]) selected for reception.

Brief: Spi_DataLineReceiveType defines the lines selected for reception.

5.19.1.16. enum Spi_DataLineTransmitType

Enumerator

Value

Description

DATA_LINE_NO_TRANSMISSION

0x3U

No transmission on data lines.

DATA_LINE_0_TRANSMISSION

0x2U

Data line 0 (SPIDAT[0]) selected for transmission.

DATA_LINE_1_TRANSMISSION

0x1U

Data line 1 (SPIDAT[1]) selected for transmission.

DATA_LINE_BOTH_TRANSMISSION

0x0U

Data line 0 and 1 (SPIDAT[0] & SPIDAT[1]) selected for transmission.

Brief: Spi_DataLineTransmitType defines the lines selected for transmission.

5.19.1.17. enum Mcspi_IrqStatusType

Enumerator

Value

Description

SPI_NO_EVENT

0U

No event ocuurs in Overflow/Under flow.

SPI_EVENT_PENDING

1U

Event occurs in Overflow/Under flow.

SPI_STATUS_READ_FAIL

2U

The status reading fails.

Brief: Irq status and std return type.

5.19.1.18. typedef Spi_JobEndNotifyType

typedef void(* Spi_JobEndNotifyType) (void);

Brief: Typedef for job end notification function pointer.

5.19.1.19. typedef Spi_SeqEndNotifyType

typedef void(* Spi_SeqEndNotifyType) (void);

Brief: Typedef for sequence end notification function pointer.

5.19.2. Structures

Name

Brief

Spi_ChannelConfigType

SPI Channel configuration structure.

Spi_McspiExternalDeviceConfigType

SPI Job configuration structure specific to McSPI peripheral.

Spi_ExternalDeviceConfigType

SPI external device specific configuration structure .

Spi_JobConfigType

SPI Job configuration structure.

Spi_SeqConfigType

SPI Sequence configuration structure.

Spi_HwUnitConfigType

SPI Hardware unit configuration structure.

Spi_ConfigType

SPI config structure.

Spi_ChannelConfigType_PC

SPI channel config structure parameters Pre-Compile only.

Spi_JobConfigType_PC

SPI job config structure parameters Pre-Compile only.

Spi_SeqConfigType_PC

SPI sequence config structure parameters Pre-Compile only.

Spi_RegisterReadbackType

SPI register readback structure.

5.19.3. Defines

Name

Brief

SPI_SW_MAJOR_VERSION

Driver Implementation Major Version.

SPI_SW_MINOR_VERSION

Driver Implementation Minor Version.

SPI_SW_PATCH_VERSION

Driver Implementation Patch Version.

SPI_AR_RELEASE_MAJOR_VERSION

AUTOSAR Major version specification implemented by SPI Driver.

SPI_AR_RELEASE_MINOR_VERSION

AUTOSAR Minor version specification implemented by SPI Driver.

SPI_AR_RELEASE_REVISION_VERSION

AUTOSAR Patch version specification implemented by SPI Driver.

SPI_VENDOR_ID

Texas Instruments Vendor ID.

SPI_MODULE_ID

SPI Driver Module ID.

SPI_INSTANCE_ID

SPI Driver Instance ID.

SPI_IB_ALIGNMENGT

SPI IB

SPI_IB

Buffer definitions IB - internal buffers.

SPI_EB

Buffer definitions EB - external buffers. Only this is supported.

SPI_IB_EB

Buffer definitions IB/EB - internal/external buffers.

SPI_ISR_VOID

void ISR type

SPI_ISR_CAT1

Category 1 ISR type.

SPI_ISR_CAT2

Category 2 ISR type.

SPI_E_PARAM_CHANNEL

API service called with wrong parameter.

SPI_E_PARAM_JOB

API service called with wrong parameter.

SPI_E_PARAM_SEQ

API service called with wrong parameter.

SPI_E_PARAM_LENGTH

API service called with wrong parameter.

SPI_E_PARAM_UNIT

API service called with wrong parameter.

SPI_E_PARAM_POINTER

APIs called with a Null Pointer.

SPI_E_UNINIT

API service used without module initiali-zation.

SPI_E_SEQ_PENDING

Services called in a wrong sequence.

SPI_E_SEQ_IN_PROCESS

Synchronous transmission service called at wrong time.

SPI_E_ALREADY_INITIALIZED

API Spi_Init service called while the SPI driver has already been initialized.

SPI_E_SEQUENCE_NOT_OK

Sequence did not complete successfully.

SPI_SID_INIT

Spi_Init() API Service ID.

SPI_SID_DEINIT

Spi_DeInit() API Service ID.

SPI_SID_WRITE_IB

Spi_WriteIB() API Service ID.

SPI_SID_ASYNC_TRANSMIT

Spi_AsyncTransmit() API Service ID.

SPI_SID_READ_IB

Spi_ReadIB() API Service ID.

SPI_SID_SETUP_EB

Spi_SetupEB() API Service ID.

SPI_SID_GET_STATUS

Spi_GetStatus() API Service ID.

SPI_SID_GET_JOB_RESULT

Spi_GetJobResult() API Service ID.

SPI_SID_GET_SEQ_RESULT

Spi_GetSequenceResult() API Service ID.

SPI_SID_GET_VERSION_INFO

Spi_GetVersionInfo() API Service ID.

SPI_SID_SYNC_TRANSMIT

Spi_SyncTransmit() API Service ID.

SPI_SID_GET_HW_UNIT_STATUS

Spi_GetHWUnitStatus() API Service ID.

SPI_SID_CANCEL

Spi_Cancel() API Service ID.

SPI_SID_SET_ASYNC_MODE

Spi_SetAsyncMode() API Service ID.

SPI_SID_MAINFUNCTION_HANDLING

Spi_MainFunction_Handling() API Service ID.

SPI_MCSPI_FCLK

MCSPI functional clock input in Hz. This clock is used to generate the serial clock output after the divider. Note: This is given here for reference and can’t be changed.

5.19.4. Functions

Return type

Function Name

Brief

void

Spi_Init(const Spi_ConfigType * CfgPtr)

Service for SPI initialization.

Std_ReturnType

Spi_DeInit(void )

Service for SPI de-initialization.

Spi_StatusType

Spi_GetStatus(void )

Service returns the SPI Handler/Driver software module status.

Spi_JobResultType

Spi_GetJobResult(Spi_JobType Job)

This service returns the last transmission result of the specified Job.

Spi_SeqResultType

Spi_GetSequenceResult(Spi_SequenceType Sequence)

This service returns the last transmission result of the specified Sequence.

void

Spi_GetVersionInfo(Std_VersionInfoType * versioninfo)

This service returns the version information of this module.

Spi_StatusType

Spi_GetHWUnitStatus(Spi_HWUnitType HWUnit)

This service returns the status of the specified SPI Hardware microcontroller peripheral.

Std_ReturnType

Spi_WriteIB(Spi_ChannelType Channel, const Spi_DataBufferType * DataBufferPtr)

Service for writing one or more data to an IB SPI Handler/Driver Channel specified by parameter.

Std_ReturnType

Spi_ReadIB(Spi_ChannelType Channel, Spi_DataBufferType * DataBufferPointer)

Service for reading synchronously one or more data from an IB SPI SPI Handler/Driver Channel specified by parameter.

Std_ReturnType

Spi_SetupEB(Spi_ChannelType Channel, const Spi_DataBufferType * SrcDataBufferPtr, Spi_DataBufferType * DesDataBufferPtr, Spi_NumberOfDataType Length)

Service to setup the buffers and the length of data for the EB SPI Handler/Driver Channel specified.

Std_ReturnType

Spi_AsyncTransmit(Spi_SequenceType Sequence)

Service to transmit data on the SPI bus.

void

Spi_Cancel(Spi_SequenceType Sequence)

Service cancels the specified ongoing sequence transmission.

Std_ReturnType

Spi_SyncTransmit(Spi_SequenceType Sequence)

Service to transmit data on the SPI bus.

Std_ReturnType

Spi_SetAsyncMode(Spi_AsyncModeType Mode)

Service to set the asynchronous mechanism mode for SPI busses handled asynchronously.

void

Spi_MainFunction_Handling(void )

This function polls the SPI interrupts linked to HW Units allocated to the transmission of SPI sequences to enable the evolution of transmission state machine.

Std_ReturnType

Spi_RegisterReadback(Spi_HWUnitType HWUnit, Spi_RegisterReadbackType * RegRbPtr)

This function reads the important registers of the hardware unit and returns the value in the structure.

Std_ReturnType

Spi_SetLoopbackMode(Spi_HWUnitType HWUnit, boolean LoopbkEn)

This function enables or disables the internal loopback mode of SPI. Note: Only MiBSPI HW units supports this feature.

void

Spi_reportDetRuntimeError(uint8 apiId, uint8 errorId)

5.19.4.1. function Spi_Init

void Spi_Init(
    const Spi_ConfigType * CfgPtr
)

Brief: Service for SPI initialization.

Service ID[hex] - 0x00

Sync/Async - Synchronous

Reentrancy - Non Reentrant

Parameters:

  • CfgPtr - Pointer to configuration set

Returns:

  • None

Return: None

5.19.4.2. function Spi_DeInit

Std_ReturnType Spi_DeInit(
    void 
)

Brief: Service for SPI de-initialization.

Service ID[hex] - 0x01

Sync/Async - Synchronous

Reentrancy - Non Reentrant

Returns:

  • E_OK - de-initialisation command has been accepted

  • E_NOT_OK - de-initialisation command has not been accepted

Return: Std_ReturnType

5.19.4.3. function Spi_GetStatus

Spi_StatusType Spi_GetStatus(
    void 
)

Brief: Service returns the SPI Handler/Driver software module status.

Status of register can be either SPI_UNINIT ,SPI_IDLE or SPI_BUSY

Service ID[hex] - 0x06

Sync/Async - Synchronous

Reentrancy - Reentrant

Returns:

  • Service for SPI de-initialization

Return: Spi_StatusType

5.19.4.4. function Spi_GetJobResult

Spi_JobResultType Spi_GetJobResult(
    Spi_JobType Job
)

Brief: This service returns the last transmission result of the specified Job.

Service ID[hex] - 0x07

Sync/Async - Synchronous

Reentrancy - Reentrant

Parameters:

  • Job - Job ID. An invalid job ID will return an undefined result

Returns:

  • SPI_JOB_OK - last transmission of the Job has been finished successfully

  • SPI_JOB_PENDING - Driver is performing a SPI Job(Busy)

  • SPI_JOB_FAILED - last transmission of the Job has failed

  • SPI_JOB_QUEUED - transmission for this Job has not started yet

Return: Spi_JobResultType

5.19.4.5. function Spi_GetSequenceResult

Spi_SeqResultType Spi_GetSequenceResult(
    Spi_SequenceType Sequence
)

Brief: This service returns the last transmission result of the specified Sequence.

Service ID[hex] - 0x08

Sync/Async - Synchronous

Reentrancy - Reentrant

Parameters:

  • Sequence - Sequence ID. An invalid job ID will return an undefined result

Returns:

  • SPI_SEQ_OK - last transmission of the Sequence has been finished successfully

  • SPI_SEQ_PENDING - Driver is performing a SPI Sequence (Busy)

  • SPI_SEQ_FAILED - last transmission of the Sequence has failed

  • SPI_SEQ_CANCELLED - transmission for this Sequence has been canceled by user

Return: Spi_JobResultType

5.19.4.6. function Spi_GetVersionInfo

void Spi_GetVersionInfo(
    Std_VersionInfoType * versioninfo
)

Brief: This service returns the version information of this module.

Service ID[hex] - 0x09

Sync/Async - Synchronous

Reentrancy - Reentrant

Parameters:

  • versioninfo - Pointer to where to store the version information of this module

Returns:

  • None

Return: None

5.19.4.7. function Spi_GetHWUnitStatus

Spi_StatusType Spi_GetHWUnitStatus(
    Spi_HWUnitType HWUnit
)

Brief: This service returns the status of the specified SPI Hardware microcontroller peripheral.

Service ID[hex] - 0x0B

Sync/Async - Synchronous

Reentrancy - Reentrant

Parameters:

  • HWUnit - SPI Hardware microcontroller peripheral unit ID. information of this module

Returns:

  • SPI_UNINIT - not initialized or not usable

  • SPI_IDLE - not currently transmitting any Job

  • SPI_BUSY - is performing a SPI Job (transmit)

Return: Spi_StatusType

5.19.4.8. function Spi_WriteIB

Std_ReturnType Spi_WriteIB(
    Spi_ChannelType Channel,
    const Spi_DataBufferType * DataBufferPtr
)

Brief: Service for writing one or more data to an IB SPI Handler/Driver Channel specified by parameter.

Service ID[hex] - 0x02

Sync/Async - Synchronous

Reentrancy - Reentrant

Parameters:

  • Channel - Channel ID

  • DataBufferPtr-Pointer to source data buffer. If this pointer is null, it is assumed that the data to be transmitted is not relevant and the default transmit value of this channel will be used instead.

Returns:

  • E_OK - Write command has been accepted

  • E_NOT_OK - Write command has not been accepted

Return: Std_ReturnType

5.19.4.9. function Spi_ReadIB

Std_ReturnType Spi_ReadIB(
    Spi_ChannelType Channel,
    Spi_DataBufferType * DataBufferPointer
)

Brief: Service for reading synchronously one or more data from an IB SPI SPI Handler/Driver Channel specified by parameter.

Service ID[hex] - 0x04

Sync/Async - Synchronous

Reentrancy - Reentrant

Parameters:

  • Channel - Channel ID

  • DataBufferPtr-Pointer to destination data buffer.

Returns:

  • E_OK - Read command has been accepted

  • E_NOT_OK - Read command has not been accepted

Return: Std_ReturnType

5.19.4.10. function Spi_SetupEB

Std_ReturnType Spi_SetupEB(
    Spi_ChannelType Channel,
    const Spi_DataBufferType * SrcDataBufferPtr,
    Spi_DataBufferType * DesDataBufferPtr,
    Spi_NumberOfDataType Length
)

Brief: Service to setup the buffers and the length of data for the EB SPI Handler/Driver Channel specified.

Service ID[hex] - 0x05

Sync/Async - Synchronous

Reentrancy - Reentrant

Parameters:

  • Channel - Channel ID

  • SrcDataBufferPtr-Pointer to source data buffer.

  • DesDataBufferPtr-Pointer to destination data buffer.

  • Length - Length (number of data elements) of the data to be transmitted from SrcDataBufferPtr and/or received from DesDataBufferPtr Min.: 1 Max.: Max of data specified at configuration for this channel.

Returns:

  • E_OK - Setup command has been accepted

  • E_NOT_OK - Setup command has not been accepted

Return: Std_ReturnType

5.19.4.11. function Spi_AsyncTransmit

Std_ReturnType Spi_AsyncTransmit(
    Spi_SequenceType Sequence
)

Brief: Service to transmit data on the SPI bus.

Service ID[hex] - 0x03

Sync/Async - Asynchronous

Reentrancy - Reentrant

Parameters:

  • Sequence - Sequence ID

Returns:

  • E_OK - Transmission command has been accepted

  • E_NOT_OK - Transmission command has not been accepted

Return: Std_ReturnType

5.19.4.12. function Spi_Cancel

void Spi_Cancel(
    Spi_SequenceType Sequence
)

Brief: Service cancels the specified ongoing sequence transmission.

Service ID[hex] - 0x0C

Sync/Async - Asynchronous

Reentrancy - Reentrant

Parameters:

  • Sequence - Sequence ID

Returns:

  • None

Return: None

5.19.4.13. function Spi_SyncTransmit

Std_ReturnType Spi_SyncTransmit(
    Spi_SequenceType Sequence
)

Brief: Service to transmit data on the SPI bus.

Service ID[hex] - 0x0A

Sync/Async - Synchronous

Reentrancy - Reentrant

Parameters:

  • Sequence - Sequence ID

Returns:

  • E_OK - Transmission command has been completed

  • E_NOT_OK - Transmission command has not been completed

Return: Std_ReturnType

5.19.4.14. function Spi_SetAsyncMode

Std_ReturnType Spi_SetAsyncMode(
    Spi_AsyncModeType Mode
)

Brief: Service to set the asynchronous mechanism mode for SPI busses handled asynchronously.

Service ID[hex] - 0x0D

Sync/Async - Synchronous

Reentrancy - Non Reentrant

Parameters:

  • Mode - New mode required.

Returns:

  • E_OK - Setting command has been done

  • E_NOT_OK - Setting command has not been accepted

Return: Std_ReturnType

5.19.4.15. function Spi_MainFunction_Handling

void Spi_MainFunction_Handling(
    void 
)

Brief: This function polls the SPI interrupts linked to HW Units allocated to the transmission of SPI sequences to enable the evolution of transmission state machine.

Service ID[hex] - 0x10

Sync/Async - Synchronous

Reentrancy - Non Reentrant

Returns:

  • None

Return: None

5.19.4.16. function Spi_RegisterReadback

Std_ReturnType Spi_RegisterReadback(
    Spi_HWUnitType HWUnit,
    Spi_RegisterReadbackType * RegRbPtr
)

Brief: This function reads the important registers of the hardware unit and returns the value in the structure.

This API should be called after Spi_Init is called. Otherwise this API will return E_NOT_OK.

This API could be used to readback the register contents after Spi_Init and then the readback value could be compared during SPI execution to check the correctness of the HW unit. Since this API is used for this purpose, the register returned are the ones which doesn’t change after init based on job or channel config.

Service ID[hex] - None

Sync/Async - Synchronous

Reentrancy - Non Reentrant

Parameters:

  • HWUnit - SPI Hardware microcontroller peripheral unit ID. If this is invalid, then the API will return E_NOT_OK.

  • RegRbPtr - Pointer to where to store the readback values. If If this pointer is NULL_PTR, then the API will return E_NOT_OK.

Returns:

  • E_OK - Register read back has been done

  • E_NOT_OK - Register read back failed

Return: Std_ReturnType

5.19.4.17. function Spi_SetLoopbackMode

Std_ReturnType Spi_SetLoopbackMode(
    Spi_HWUnitType HWUnit,
    boolean LoopbkEn
)

Brief: This function enables or disables the internal loopback mode of SPI. Note: Only MiBSPI HW units supports this feature.

This API should be called after Spi_Init is called. Otherwise this API will return E_NOT_OK. Also this API should not be called when the HW unit is busy.

This API could be used to check the integrity of the SPI module. When the loopback mode is enabled, the data transferred is received back and hence the caller can verify and compare the TX buffer with RX buffer for any HW failures.

Service ID[hex] - None

Sync/Async - Asynchronous

Reentrancy - Reentrant

Parameters:

  • HWUnit - SPI Hardware microcontroller peripheral unit ID. If this is invalid, then the API will return E_NOT_OK.

  • LpbkEnable - Loopback enable/disable: TRUE - Enable loopback, FALSE - Disable loopback

Returns:

  • E_OK - Loop back mode done

  • E_NOT_OK - Loop back mode failed

Return: Std_ReturnType

5.19.4.18. function Spi_reportDetRuntimeError

void Spi_reportDetRuntimeError(
    uint8 apiId,
    uint8 errorId
)