5.12. FLS

5.12.1. Types

Base type

Type Name

Brief

enum

Fls_EraseType

ENUM for erase type names.

enum

Fls_ResetPinMode

ENUM for Reset pin states.

enum

Fls_OSPI_Modes

OSPI modes.

typedef uint32

Fls_AddressType

FLS Address type.

typedef uint32

Fls_LengthType

FLS Length type.

5.12.1.1. enum Fls_EraseType

Enumerator

Value

Description

FLS_SECTOR_ERASE

Sector Erase.

FLS_BLOCK_ERASE

Block Erase.

FLS_CHIP_ERASE

Chip Erase.

Brief: ENUM for erase type names.

5.12.1.2. enum Fls_ResetPinMode

Enumerator

Value

Description

FLS_RESET_PIN_STATE_LOW

Reset pin state low.

FLS_RESET_PIN_STATE_HIGH

Reset pin state high.

Brief: ENUM for Reset pin states.

5.12.1.3. enum Fls_OSPI_Modes

Enumerator

Value

Description

FLS_OSPI_RX_1S_1S_1S

1

FLS_OSPI_RX_1S_1S_2S

2

FLS_OSPI_RX_1S_1S_4S

3

FLS_OSPI_RX_1S_1S_8S

4

FLS_OSPI_RX_4S_4S_4S

5

FLS_OSPI_RX_4S_4D_4D

6

FLS_OSPI_RX_8S_8S_8S

7

FLS_OSPI_RX_8D_8D_8D

8

Brief: OSPI modes.

5.12.1.4. typedef Fls_AddressType

typedef uint32 Fls_AddressType;

Brief: FLS Address type.

5.12.1.5. typedef Fls_LengthType

typedef uint32 Fls_LengthType;

Brief: FLS Length type.

5.12.2. Structures

Name

Brief

Fls_SectorType

FLS Module Flashable Sectors and pages.

Fls_ConfigType

FLS Module Configuration Structure.

Fls_EraseConfig

FLS external flash erase configuration items.

Fls_ReadIdConfig

FLS external flash device informations.

Fls_RegEnConfig

FLS external flash protocol specific configuration parameters.

Fls_ProtoEnableConfig

FLS external flash protocol specific commands.

Fls_ConfigSfdp

FLS external flash generic parameters.

Fls_RegisterReadbackType

Register readback type.

5.12.3. Defines

Name

Brief

FLS_ISR_VOID

void ISR type

FLS_ISR_CAT1

Category 1 ISR type.

FLS_ISR_CAT2

Category 2 ISR type.

FLS_SW_MAJOR_VERSION

Driver Implementation Major Version.

FLS_SW_MINOR_VERSION

Driver Implementation Minor Version.

FLS_SW_PATCH_VERSION

Driver Implementation Patch Version.

FLS_AR_RELEASE_MAJOR_VERSION

AUTOSAR Major version specification implemented by FLS Driver.

FLS_AR_RELEASE_MINOR_VERSION

AUTOSAR Minor version specification implemented by FLS Driver.

FLS_AR_RELEASE_REVISION_VERSION

AUTOSAR Patch version specification implemented by FLS Driver.

FLS_VENDOR_ID

Texas Instruments Vendor ID.

FLS_MODULE_ID

FLS Driver Module ID.

FLS_INSTANCE_ID

FLS Driver Instance ID.

FLS_E_PARAM_CONFIG

API service called with wrong parameter.

FLS_E_PARAM_ADDRESS

API service called with wrong parameter.

FLS_E_PARAM_LENGTH

API service called with wrong parameter.

FLS_E_PARAM_DATA

API service called with wrong parameter.

FLS_E_UNINIT

API service used without module initiali-zation.

FLS_E_BUSY

APIs called when module is busy.

FLS_E_PARAM_POINTER

APIs called with a Null Pointer.

FLS_E_VERIFY_ERASE_FAILED

APIs service Erase Verification (BlankCheck) failed.

FLS_E_VERIFY_WRITE_FAILED

APIs serice Write Verification (Compare) failed.

FLS_E_TIMEOUT

APIs Timeout Exceeded.

FLS_E_MEMAP_INTERRUPT_OFF_DMA_ON

APIs MEMMAP/INTERRUPT OFF but DMA ON.

FLS_E_ERASE_FAILED

Flash Erase Failed in HW.

FLS_E_WRITE_FAILED

Flash Write Failed in HW.

FLS_E_READ_FAILED

Flash Read Failed in HW.

FLS_E_COMPARE_FAILED

Flash Compare Failediin HW.

FLS_E_UNEXPECTED_FLASH_ID

Expected HW ID not matched.

FLS_SID_INIT

FLS_Init() API Service ID.

FLS_SID_ERASE

FLS_Erase() API Service ID.

FLS_SID_WRITE

FLS_Write() API Service ID.

FLS_SID_CANCEL

FLS_Cancel() API Service ID.

FLS_SID_GET_STATUS

FLS_GetStatus() API Service ID.

FLS_SID_GET_JOB_RESULT

Fls_GetJobResult() API Service ID.

FLS_SID_READ

FLS_Read() API Service ID.

FLS_SID_COMPARE

FLS_Compare() API Service ID.

FLS_SID_SET_MODE

FLS_SetMode() API Service ID.

FLS_SID_GET_VERSION_INFO

Fls_GetVersionInfo() API Service ID.

FLS_SID_BLANK_CHECK

FLS_BlankCheck() API Service ID.

FLS_SID_MAIN_FUNCTION

FLS_MainFunction() API Service ID.

FLS_SID_REGISTERREADBACK

Fls_RegisterReadback() API Service ID.

FLS_SID_SET_ERASE_TYPE

Fls_SetEraseType() API Service ID.

FLS_BASE_ADDRESS_REQ

FLS Address type.

5.12.4. Functions

Return type

Function Name

Brief

void

Fls_Init(const Fls_ConfigType * ConfigPtr)

Initializes the Flash Driver.

Std_ReturnType

Fls_Erase(Fls_AddressType TargetAddress, Fls_LengthType Length)

Erases flash sector(s).

Std_ReturnType

Fls_Write(Fls_AddressType TargetAddress, const uint8 * SourceAddressPtr, Fls_LengthType Length)

Writes one or more complete flash pages.

Std_ReturnType

Fls_Read(Fls_AddressType SourceAddress, uint8 * TargetAddressPtr, Fls_LengthType Length)

Reads from flash memory.

Std_ReturnType

Fls_Compare(Fls_AddressType SourceAddress, const uint8 * TargetAddressPtr, Fls_LengthType Length)

Compares the contents of an area of flash memory with that of an application data buffer.

Std_ReturnType

Fls_BlankCheck(Fls_AddressType Address, Fls_LengthType Length)

The function Fls_BlankCheck shall verify, whether a given memory area has been erased but not (yet) programmed.

MemIf_StatusType

Fls_GetStatus(void )

Returns the driver state.

Std_ReturnType

Fls_GetVersionInfo(Std_VersionInfoType * versioninfo)

This service returns the version information of this module.

MemIf_JobResultType

Fls_GetJobResult(void )

Returns the result of the last job.

void

Fls_MainFunction(void )

Performs the processing of jobs.

void

Fls_Cancel(void )

Cancels an ongoing job.

void

Fls_SetMode(MemIf_ModeType Mode)

Sets the flash driver’s operation mode This is a dummy API which is not supported and Added for integration purposes.

uint32

Fls_SetEraseType(Fls_EraseType erasetype)

Sets the parameters for required erase type. Sets the parameters required in application, based on the erase type parameter passed to this function while calling from Application.

Std_ReturnType

Fls_RegisterReadback(Fls_RegisterReadbackType * RegRbPtr)

Register readback function.

Std_ReturnType

Fls_Set3ByteAddressMode(void )

Sets the Flash Addressing Mode to 3 byte.

Std_ReturnType

Fls_setResetPinMode(Fls_ResetPinMode pinMode)

Updates the Flash Pin Value. Use this API to Reset Flash Step1: pinMode = FLS_RESET_PIN_STATE_HIGH Step2: pinMode = FLS_RESET_PIN_STATE_LOW Works for Am263Px-SIP and AM263Px- Rev A board.

5.12.4.1. function Fls_Init

void Fls_Init(
    const Fls_ConfigType * ConfigPtr
)

Brief: Initializes the Flash Driver.

Mode : Supervisor Mode (Privileged Mode)

Service ID[hex] : 0x00

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • ConfigPtr - Pointer to flash driver configuration set

Returns:

  • None

Return: None

5.12.4.2. function Fls_Erase

Std_ReturnType Fls_Erase(
    Fls_AddressType TargetAddress,
    Fls_LengthType Length
)

Brief: Erases flash sector(s).

Mode : Supervisor Mode (Privileged Mode)

Service ID[hex] : 0x01

Sync/Async : Asynchronous

Reentrancy : Non-Reentrant

Parameters:

  • TargetAddress - Target address in flash memory. This address offset will be added to the flash memory base address.

  • Length - Number of bytes to erase

Returns:

  • E_OK erase command has been accepted

  • E_NOT_OK erase command has not been accepted

Return: Std_ReturnType

5.12.4.3. function Fls_Write

Std_ReturnType Fls_Write(
    Fls_AddressType TargetAddress,
    const uint8 * SourceAddressPtr,
    Fls_LengthType Length
)

Brief: Writes one or more complete flash pages.

Mode : Supervisor Mode (Privileged Mode)

Service ID[hex] : 0x02

Sync/Async : Asynchronous

Reentrancy : Non-Reentrant

Parameters:

  • TargetAddress - Target address in flash memory. This address offset will be added to the flash memory base address.

  • SourceAddressPtr - Pointer to source data buffer

  • Length - Number of bytes to write

Returns:

  • E_OK write command has been accepted

  • E_NOT_OK write command has not been accepted

Return: Std_ReturnType

5.12.4.4. function Fls_Read

Std_ReturnType Fls_Read(
    Fls_AddressType SourceAddress,
    uint8 * TargetAddressPtr,
    Fls_LengthType Length
)

Brief: Reads from flash memory.

Mode : Supervisor Mode (Privileged Mode)

Service ID[hex] : 0x07

Sync/Async : Asynchronous

Reentrancy : Non-Reentrant

Parameters:

  • SourceAddress - Source address in flash memory. This address offset will be added to the flash memory base address.

  • TargetAddressPtr - Pointer to target data buffer

  • Length - Number of bytes to read

Returns:

  • E_OK read command has been accepted

  • E_NOT_OK read command has not been accepted

Return: Std_ReturnType

5.12.4.5. function Fls_Compare

Std_ReturnType Fls_Compare(
    Fls_AddressType SourceAddress,
    const uint8 * TargetAddressPtr,
    Fls_LengthType Length
)

Brief: Compares the contents of an area of flash memory with that of an application data buffer.

Mode : User Mode (Non-Privileged Mode)

Service ID[hex] : 0x08

Sync/Async : Asynchronous

Reentrancy : Non-Reentrant

Parameters:

  • SourceAddress - Source address in flash memory. This address offset will be added to the flash memory base address.

  • TargetAddressPtr - Pointer to target data buffer

  • Length - Number of bytes to compare

Returns:

  • E_OK compare command has been accepted

  • E_NOT_OK compare command has not been accepted

Return: Std_ReturnType

5.12.4.6. function Fls_BlankCheck

Std_ReturnType Fls_BlankCheck(
    Fls_AddressType Address,
    Fls_LengthType Length
)

Brief: The function Fls_BlankCheck shall verify, whether a given memory area has been erased but not (yet) programmed.

Mode : User Mode (Non-Privileged Mode)

Service ID[hex] : 0x0a

Sync/Async : Asynchronous

Reentrancy : Non-Reentrant

Parameters:

  • Address - Source address in flash memory. This address offset will be added to the flash memory base address.

  • Length - Number of bytes to compare

Returns:

  • E_OK BlankCheck command has been accepted

  • E_NOT_OK BlankCheck command has not been accepted

Return: Std_ReturnType

5.12.4.7. function Fls_GetStatus

MemIf_StatusType Fls_GetStatus(
    void 
)

Brief: Returns the driver state.

Mode : User Mode (Non-Privileged Mode)

Service ID[hex] : 0x04

Sync/Async : Synchronous

Reentrancy : Reentrant

Parameters:

  • None

Returns:

  • Returns the state

Return: MemIf_StatusType

5.12.4.8. function Fls_GetVersionInfo

Std_ReturnType Fls_GetVersionInfo(
    Std_VersionInfoType * versioninfo
)

Brief: This service returns the version information of this module.

Mode : User Mode (Non-Privileged Mode)

Service ID[hex] : 0x10

Sync/Async : Synchronous

Reentrancy : Reentrant

Parameters:

  • versioninfo - Pointer to where to store the version information of this module

Returns:

  • E_OK command has been accepted

  • E_NOT_OK command has not been accepted

Return: Std_ReturnType

5.12.4.9. function Fls_GetJobResult

MemIf_JobResultType Fls_GetJobResult(
    void 
)

Brief: Returns the result of the last job.

Mode : User Mode (Non-Privileged Mode)

Service ID[hex] : 0x05

Sync/Async : Synchronous

Reentrancy : Reentrant

Parameters:

  • None

Returns:

  • Returns the MemIf Job result type. Refer enum MemIf_JobResultType for the values

Return: MemIf_JobResultType

5.12.4.10. function Fls_MainFunction

void Fls_MainFunction(
    void 
)

Brief: Performs the processing of jobs.

Mode : Supervisor Mode (Privileged Mode)

Service ID[hex] : 0x06

Parameters:

  • None

Returns:

  • None

Return: None

5.12.4.11. function Fls_Cancel

void Fls_Cancel(
    void 
)

Brief: Cancels an ongoing job.

Mode : User Mode (Non-Privileged Mode)

Service ID[hex] : 0x03

Parameters:

  • None

Returns:

  • None

Return: None

5.12.4.12. function Fls_SetMode

void Fls_SetMode(
    MemIf_ModeType Mode
)

Brief: Sets the flash driver’s operation mode This is a dummy API which is not supported and Added for integration purposes.

Mode : User Mode (Non-Privileged Mode)

Service ID[hex] : 0x09

Sync/Async : Synchronous

Reentrancy : Non Reentrant

Parameters:

  • Mode - MEMIF_MODE_SLOW: Slow read access / normal SPI access, MEMIF_MODE_FAST: Fast read access / SPI burst access.

Returns:

  • None

Return: None

5.12.4.13. function Fls_SetEraseType

uint32 Fls_SetEraseType(
    Fls_EraseType erasetype
)

Brief: Sets the parameters for required erase type. Sets the parameters required in application, based on the erase type parameter passed to this function while calling from Application.

Mode : User Mode (Non-Privileged Mode)

Service ID[hex] : NA

Parameters:

  • erasetype - Type of erase

Returns:

  • Returns sector or block size

Return: uint32

5.12.4.14. function Fls_RegisterReadback

Std_ReturnType Fls_RegisterReadback(
    Fls_RegisterReadbackType * RegRbPtr
)

Brief: Register readback function.

Service ID[hex] : NA

Parameters:

  • RegRbPtr - Register readback pointer

Returns:

  • E_OK success

  • E_NOT_OK failure

Return: Std_ReturnType

5.12.4.15. function Fls_Set3ByteAddressMode

Std_ReturnType Fls_Set3ByteAddressMode(
    void 
)

Brief: Sets the Flash Addressing Mode to 3 byte.

Service ID[hex] : NA

Returns:

  • E_OK success

  • E_NOT_OK failure

Return: Std_ReturnType

5.12.4.16. function Fls_setResetPinMode

Std_ReturnType Fls_setResetPinMode(
    Fls_ResetPinMode pinMode
)

Brief: Updates the Flash Pin Value. Use this API to Reset Flash Step1: pinMode = FLS_RESET_PIN_STATE_HIGH Step2: pinMode = FLS_RESET_PIN_STATE_LOW Works for Am263Px-SIP and AM263Px- Rev A board.

Service ID[hex] : NA

Returns:

  • E_OK success

  • E_NOT_OK failure

Return: Std_ReturnType