Input parameters for Sciclient_service function.
Data Fields | |
| uint16_t | messageType |
| uint32_t | flags |
| const uint8_t * | pReqPayload |
| uint32_t | reqPayloadSize |
| uint32_t | timeout |
| uint16_t Sciclient_ReqPrm_t::messageType |
[IN] Type of message
| uint32_t Sciclient_ReqPrm_t::flags |
[IN] Flags for messages that are being transmitted.
| const uint8_t* Sciclient_ReqPrm_t::pReqPayload |
[IN] Pointer to the payload to be transmitted
| uint32_t Sciclient_ReqPrm_t::reqPayloadSize |
[IN] Size of the payload to be transmitted (in bytes)
| uint32_t Sciclient_ReqPrm_t::timeout |
[IN] Timeout(number of iterations) for receiving response (Refer SystemP_Timeout)