AM64x MCU+ SDK  12.01.00
EnetUdma_SGList Struct Reference

Detailed Description

Transmit packet scatter list info.

This structure contains info on the scatter list used for transmitting packets that are split into list of fragments. Using a scatter list allows application to transmit packet that are not a single continuous buffer but a list of scatter fragments chained together. Support for scatter list is needed for supporting zero copy in network stacks protocols like UDP

Data Fields

uint32_t numScatterSegments
 
EnetUdma_SGListEntry list [ENET_UDMA_CPSW_MAX_SG_LIST]
 

Field Documentation

◆ numScatterSegments

uint32_t EnetUdma_SGList::numScatterSegments

Number of valid scatter segments in the packet to be transmitted If packet is made of a single continuous buffer then numScatterSegments = 1

◆ list

Array of scatterList having info on each individual scatter segment