AM64x MCU+ SDK  12.01.00
ieee802-dot1ab-lldp_access.h File Reference

Go to the source code of this file.

Data Structures

struct  attribute_pair_t
 
struct  lldp_remote_portid_info_t
 

Enumerations

enum  lldp_port_id_subtype_t {
  ePORT_ID_SUBTYPE_INTERFACE_ALIAS =0x01, ePORT_ID_SUBTYPE_PORT_COMPONENT, ePORT_ID_SUBTYPE_MAC_ADDRESS, ePORT_ID_SUBTYPE_NETWORK_ADDRESS,
  ePORT_ID_SUBTYPE_INTERFACE_NAME, ePORT_ID_SUBTYPE_AGENT_CIRCUIT_ID, ePORT_ID_SUBTYPE_LOCAL, ePORT_ID_SUBTYPE_MAX
}
 

Functions

int ydbi_get_item_abk1vk0 (yang_db_item_access_t *ydbia, void **rval, uint8_t k1, bool status)
 
int ydbi_get_item_abk2vk0 (yang_db_item_access_t *ydbia, void **rval, uint8_t k1, uint8_t k2, bool status)
 
int ydbi_set_item_abk1vk0 (yang_db_item_access_t *ydbia, void *rval, uint32_t vsize, uint8_t k1, bool status, uint8_t notice)
 
int ydbi_set_item_abk2vk0 (yang_db_item_access_t *ydbia, void *rval, uint32_t vsize, uint8_t k1, uint8_t k2, bool status, uint8_t notice)
 
int ydbi_get_item_abknvkn (yang_db_item_access_t *ydbia, void **rval, uint8_t kn[], uint8_t kn_sz, attribute_pair_t attrs[], uint8_t kvs_sz, bool status)
 Get val base on n key from LLDP until end Also provided vkn as attribute. More...
 
int ydbi_set_item_abknvkn (yang_db_item_access_t *ydbia, uint8_t kn[], uint8_t kn_sz, attribute_pair_t attrs[], uint8_t kvs_sz, bool status, void *value, uint32_t vsize, uint8_t notice)
 Set val base on n key from LLDP until end Also provided vkn as attribute. More...
 
int ydbi_del_item_abknvkn (yang_db_item_access_t *ydbia, uint8_t kn[], uint8_t kn_sz, attribute_pair_t attrs[], uint8_t kvs_sz, bool status, uint8_t notice)
 Set val base on n key from LLDP until end Also provided vkn as attribute. More...
 
void ydbi_set_dbpara_abk1vk1 (yang_db_item_access_t *ydbia, char *brname, char *name, uint8_t *destmac, uint8_t k1, bool ismirror, bool iswildcard)
 set ydbi db parameters for remote-systems-data leafs More...
 
int ydbi_iterate_portid (yang_db_item_access_t *ydbia, uc_range **range, lldp_remote_portid_info_t *portid, bool ismirror)
 iterate remote port-id data in db More...
 
int ydbi_get_portid_subtype (yang_db_item_access_t *ydbia, lldp_remote_portid_info_t *portid, bool ismirror)
 get the port-id-subtype of the given port-id info More...
 
int ydbi_del_remote_systems_data (yang_db_item_access_t *ydbia, uint8_t k1, lldp_remote_portid_info_t *portid, bool ismirror)
 deleted the given remote-system-data leaf (k1) with the given port-id info More...
 

Enumeration Type Documentation

◆ lldp_port_id_subtype_t

Enumerator
ePORT_ID_SUBTYPE_INTERFACE_ALIAS 
ePORT_ID_SUBTYPE_PORT_COMPONENT 
ePORT_ID_SUBTYPE_MAC_ADDRESS 
ePORT_ID_SUBTYPE_NETWORK_ADDRESS 
ePORT_ID_SUBTYPE_INTERFACE_NAME 
ePORT_ID_SUBTYPE_AGENT_CIRCUIT_ID 
ePORT_ID_SUBTYPE_LOCAL 
ePORT_ID_SUBTYPE_MAX 

Function Documentation

◆ ydbi_get_item_abk1vk0()

int ydbi_get_item_abk1vk0 ( yang_db_item_access_t *  ydbia,
void **  rval,
uint8_t  k1,
bool  status 
)

◆ ydbi_get_item_abk2vk0()

int ydbi_get_item_abk2vk0 ( yang_db_item_access_t *  ydbia,
void **  rval,
uint8_t  k1,
uint8_t  k2,
bool  status 
)

◆ ydbi_set_item_abk1vk0()

int ydbi_set_item_abk1vk0 ( yang_db_item_access_t *  ydbia,
void *  rval,
uint32_t  vsize,
uint8_t  k1,
bool  status,
uint8_t  notice 
)

◆ ydbi_set_item_abk2vk0()

int ydbi_set_item_abk2vk0 ( yang_db_item_access_t *  ydbia,
void *  rval,
uint32_t  vsize,
uint8_t  k1,
uint8_t  k2,
bool  status,
uint8_t  notice 
)

◆ ydbi_get_item_abknvkn()

int ydbi_get_item_abknvkn ( yang_db_item_access_t *  ydbia,
void **  rval,
uint8_t  kn[],
uint8_t  kn_sz,
attribute_pair_t  attrs[],
uint8_t  kvs_sz,
bool  status 
)

Get val base on n key from LLDP until end Also provided vkn as attribute.

◆ ydbi_set_item_abknvkn()

int ydbi_set_item_abknvkn ( yang_db_item_access_t *  ydbia,
uint8_t  kn[],
uint8_t  kn_sz,
attribute_pair_t  attrs[],
uint8_t  kvs_sz,
bool  status,
void *  value,
uint32_t  vsize,
uint8_t  notice 
)

Set val base on n key from LLDP until end Also provided vkn as attribute.

◆ ydbi_del_item_abknvkn()

int ydbi_del_item_abknvkn ( yang_db_item_access_t *  ydbia,
uint8_t  kn[],
uint8_t  kn_sz,
attribute_pair_t  attrs[],
uint8_t  kvs_sz,
bool  status,
uint8_t  notice 
)

Set val base on n key from LLDP until end Also provided vkn as attribute.

◆ ydbi_set_dbpara_abk1vk1()

void ydbi_set_dbpara_abk1vk1 ( yang_db_item_access_t *  ydbia,
char *  brname,
char *  name,
uint8_t *  destmac,
uint8_t  k1,
bool  ismirror,
bool  iswildcard 
)

set ydbi db parameters for remote-systems-data leafs

Parameters
ydbiaydbia handle
brnameuc-mirror bridge name (used only if ismirror=true)
nameport's name key value
destmacport's dest-mac-address key value
k1key of the target leaf
ismirrorset to true to set uc-mirror prefix.
iswildcardset to true to set default kss value even if kvs is NULL.

◆ ydbi_iterate_portid()

int ydbi_iterate_portid ( yang_db_item_access_t *  ydbia,
uc_range **  range,
lldp_remote_portid_info_t *  portid,
bool  ismirror 
)

iterate remote port-id data in db

Parameters
ydbiaydbia handle
rangeif NULL crate a new range. not NULL continue
portidremote system data structure return.
ismirrorif set to true, mirrored(prefixed) db data will be search. if false, local (non-prefixed) db data will be search.
Returns
-1: error, 0:okay, 1:no more data
Note
the created range is released when it returns non-ZERO

◆ ydbi_get_portid_subtype()

int ydbi_get_portid_subtype ( yang_db_item_access_t *  ydbia,
lldp_remote_portid_info_t *  portid,
bool  ismirror 
)

get the port-id-subtype of the given port-id info

Parameters
ydbiaydbia handle
portidremote system data structure return. 'ifname', 'dstmacaddr', 'timemarks', and 'remoteidx' must be defined.
ismirrorif set to true, mirrored(prefixed) db data will return. if false, local (non-prefixed) db data will be return.
Returns
-1: error, 0:sucess

◆ ydbi_del_remote_systems_data()

int ydbi_del_remote_systems_data ( yang_db_item_access_t *  ydbia,
uint8_t  k1,
lldp_remote_portid_info_t *  portid,
bool  ismirror 
)

deleted the given remote-system-data leaf (k1) with the given port-id info

Parameters
ydbiaydbia handle
k1remote-system-data leaf to be deleted
portidremote system data structure return. 'ifname', 'dstmacaddr', 'timemarks', and 'remoteidx' must be defined.
ismirrorif set to true, mirrored(prefixed) db data will be deleted. if false, local (non-prefixed) db data will be deleted.
Returns
-1: error, 0:success