Go to the source code of this file.
Data Structures | |
| struct | ICSS_EMAC_FwStaticMmap |
| ICSS EMAC Static Firmware Memory Map offsets. These are offsets for PRU0 and PRU1 DRAM memory. More... | |
| struct | ICSS_EMAC_FwDynamicMmap |
| ICSS EMAC Dynamic Firmware Memory Map offsets. More... | |
| struct | ICSS_EMAC_FwVlanFilterParams |
| ICSS EMAC VLAN Filtering Parameters. More... | |
| struct | ICSS_EMAC_FwMulticastFilterParams |
| ICSS EMAC Multicast Filtering Parameters. More... | |
| struct | ICSS_EMAC_Attrs |
| struct | ICSS_EMAC_InternalObject |
| Opaque ICSS EMAC driver object. More... | |
| struct | ICSS_EMAC_Config |
| Base EMAC handle containing pointers to all modules required for driver to work. More... | |
| struct | ICSS_EMAC_CallBackConfig |
| Generic callback configuration for protocol specific callbacks. ICSS_EMAC_CallBack is the function prototype used. While calling this, first argument is always of type ICSS_EMAC_Handle, second argument is specific to the callback (see ICSS_EMAC_CallBackObject), and third argument is userArg as specified in this structure. More... | |
| struct | ICSS_EMAC_CallBackObject |
| Different callbacks which can be registered. While calling the function set in ICSS_EMAC_CallBack, first argument is always of type ICSS_EMAC_Handle, second argument is specific to the callback (as mentioned in the member descriptions), and third argument is userArg as specified in ICSS_EMAC_CallBackConfig. More... | |
| struct | ICSS_EMAC_Params |
| ICSS_EMAC Parameters. More... | |
| struct | ICSS_EMAC_RxArgument |
| Rx packet processing information block that needs to passed into call to ICSS_EMAC_RxPktGet. More... | |
| struct | ICSS_EMAC_TxArgument |
| Tx packet processing information block that needs to passed into call to ICSS_EMAC_txPacket. More... | |
| struct | ICSS_EMAC_IoctlCmd |
| IOCTL command members for configuring switch/EMAC. More... | |
| struct | ICSS_EMAC_PruStatistics |
| Statistics structure for capturing statistics on PRU. More... | |
Macros | |
| #define | ICSS_EMAC_MAX_PORTS_PER_INSTANCE (2) |
| Maximum number of Ports in a single ICSS More... | |
| #define | ICSS_EMAC_NUMQUEUES ((uint32_t)17U) |
| Total Queues available. More... | |
| #define | ICSS_EMAC_MAXMTU (1518U) |
| Maximum Valid size (incl header + VLAN TAG..., no CRC) More... | |
| #define | ICSS_EMAC_MINMTU (14U) |
| Minimum Valid size ( DA + SA + Ethertype) More... | |
| #define | ICSS_EMAC_PORT_0 (0) |
| Used to specify host side port. More... | |
| #define | ICSS_EMAC_PORT_1 (1U) |
| Used to specify physical port 1 MII 0 (tx) More... | |
| #define | ICSS_EMAC_PORT_2 (2U) |
| Used to specify physical port 2 MII 1 (tx) More... | |
| #define | ICSS_EMAC_IOCTL_PORT_CTRL_DISABLE (0u) |
| ICSS_EMAC_IOCTL_PORT_CTRL options. More... | |
| #define | ICSS_EMAC_IOCTL_PORT_CTRL_ENABLE (1u) |
| Generic IOCTL Disable macro. More... | |
| #define | ICSS_EMAC_LEARNING_PORT_STATE_LEARNING (0U) |
| Macros for different port states in learning module. More... | |
| #define | ICSS_EMAC_LEARNING_PORT_STATE_NOT_LEARNING (1U) |
| #define | ICSS_EMAC_LEARNING_PORT_STATE_LOCKED (2U) |
| #define | ICSS_EMAC_OBJECT_SIZE_IN_BYTES (42000U) |
ICSS EMAC Modes | |
| #define | ICSS_EMAC_MODE_MAC1 (1U) |
| Single EMAC Mode. Port 1 Enabled. More... | |
| #define | ICSS_EMAC_MODE_MAC2 (2U) |
| Single EMAC Mode. Port 2 Enabled. More... | |
| #define | ICSS_EMAC_MODE_SWITCH (3U) |
| Switch Mode. More... | |
| #define | ICSS_EMAC_MODE_DUALMAC (4U) |
| Dual MAC Mode. Both Ports Enabled. More... | |
ICSS EMAC PHY to MAC Interface Modes | |
| #define | ICSS_EMAC_MII_MODE (0U) |
| Media-independent Interface. More... | |
| #define | ICSS_EMAC_RGMII_MODE (1U) |
| Reduced Gigabit Media-independent Interface More... | |
ICSS EMAC Learning Modes | |
| #define | ICSS_EMAC_LEARNING_DISABLE (0U) |
| Driver-based Learning Mode Disabled More... | |
| #define | ICSS_EMAC_LEARNING_ENABLE (1U) |
| Driver-based Learning Mode Enabled More... | |
ICSS EMAC Interrupt Pacing Configuration | |
| #define | ICSS_EMAC_ENABLE_PACING (0) |
| Interrupt pacing enabled. More... | |
| #define | ICSS_EMAC_DISABLE_PACING (1) |
| Interrupt pacing disabled. More... | |
ICSS EMAC Interrupt Pacing Modes | |
| #define | ICSS_EMAC_INTR_PACING_MODE1 (0) |
| Frame Count based Interrupt pacing. More... | |
ICSS EMAC Queues | |
| #define | ICSS_EMAC_QUEUE1 ((uint32_t)0U) |
| Priority Queue 1. More... | |
| #define | ICSS_EMAC_QUEUE2 ((uint32_t)1U) |
| Priority Queue 2. More... | |
| #define | ICSS_EMAC_QUEUE3 ((uint32_t)2U) |
| Priority Queue 3. More... | |
| #define | ICSS_EMAC_QUEUE4 ((uint32_t)3U) |
| Priority Queue 4. More... | |
| #define | ICSS_EMAC_QUEUE5 ((uint32_t)4U) |
| Priority Queue 5. More... | |
| #define | ICSS_EMAC_QUEUE6 ((uint32_t)5U) |
| Priority Queue 6. More... | |
| #define | ICSS_EMAC_QUEUE7 ((uint32_t)6U) |
| Priority Queue 7. More... | |
| #define | ICSS_EMAC_QUEUE8 ((uint32_t)7U) |
| Priority Queue 8. More... | |
| #define | ICSS_EMAC_QUEUE9 ((uint32_t)8U) |
| Priority Queue 9. More... | |
| #define | ICSS_EMAC_QUEUE10 ((uint32_t)9U) |
| Priority Queue 10. More... | |
| #define | ICSS_EMAC_QUEUE11 ((uint32_t)10U) |
| Priority Queue 11. More... | |
| #define | ICSS_EMAC_QUEUE12 ((uint32_t)11U) |
| Priority Queue 12. More... | |
| #define | ICSS_EMAC_QUEUE13 ((uint32_t)12U) |
| Priority Queue 13. More... | |
| #define | ICSS_EMAC_QUEUE14 ((uint32_t)13U) |
| Priority Queue 14. More... | |
| #define | ICSS_EMAC_QUEUE15 ((uint32_t)14U) |
| Priority Queue 15. More... | |
| #define | ICSS_EMAC_QUEUE16 ((uint32_t)15U) |
| Priority Queue 16. More... | |
| #define | ICSS_EMAC_COLQUEUE ((uint32_t)16U) |
| Collision Queue. More... | |
ICSS EMAC Error Codes | |
| #define | ICSS_EMAC_SWITCH_ERROR_BASE ((uint32_t)0x21Fu) |
| Switch Error Base. More... | |
| #define | ICSS_EMAC_SWITCH_ERROR_CODE (ICSS_EMAC_SWITCH_ERROR_BASE) |
| Switch Error Code. More... | |
| #define | ICSS_EMAC_SWITCH_ERROR_INFO (ICSS_EMAC_SWITCH_ERROR_CODE) |
| Switch Error/Informational. More... | |
| #define | ICSS_EMAC_SWITCH_ERROR_WARNING (ICSS_EMAC_SWITCH_ERROR_CODE | 0x1000u) |
| Switch Error/Warning. More... | |
| #define | ICSS_EMAC_SWITCH_ERROR_MINOR (ICSS_EMAC_SWITCH_ERROR_CODE | 0x2000u) |
| Switch Error Minor. More... | |
| #define | ICSS_EMAC_SWITCH_ERROR_MAJOR (ICSS_EMAC_SWITCH_ERROR_CODE | 0x3000u) |
| Switch Error Major. More... | |
| #define | ICSS_EMAC_SWITCH_ERROR_CRITICAL (ICSS_EMAC_SWITCH_ERROR_CODE | 0x4000u) |
| Switch Error Critical. More... | |
| #define | ICSS_EMAC_SWITCH_SUCCESS (0u) |
| Success code. More... | |
| #define | ICSS_EMAC_PORT1_TX_ERROR_MASK (0xFFFFu) |
| #define | ICSS_EMAC_PORT2_TX_ERROR_MASK (0xFFFF0000u) |
| #define | ICSS_EMAC_ERR_DEV_NOT_INSTANTIATED (ICSS_EMAC_SWITCH_ERROR_MAJOR + 1u) |
| Device is not instantiated yet. More... | |
| #define | ICSS_EMAC_ERR_SWITCH_INVALID_PARAM (ICSS_EMAC_SWITCH_ERROR_MAJOR + 2u) |
| Function or calling parameter is invalid. More... | |
| #define | ICSS_EMAC_ERR_CH_INVALID (ICSS_EMAC_SWITCH_ERROR_CRITICAL + 3u) |
| Channel number invalid. More... | |
| #define | ICSS_EMAC_ERR_CH_ALREADY_INIT (ICSS_EMAC_SWITCH_ERROR_MAJOR + 4u) |
| Channel already initialized and setup. More... | |
| #define | ICSS_EMAC_ERR_TX_CH_ALREADY_CLOSED (ICSS_EMAC_SWITCH_ERROR_MAJOR + 5u) |
| Tx Channel already closed. Channel close failed. More... | |
| #define | ICSS_EMAC_ERR_TX_CH_NOT_OPEN (ICSS_EMAC_SWITCH_ERROR_MAJOR + 6u) |
| Tx Channel not open. More... | |
| #define | ICSS_EMAC_ERR_TX_NO_LINK (ICSS_EMAC_SWITCH_ERROR_MAJOR + 7u) |
| Tx Link not up. More... | |
| #define | ICSS_EMAC_ERR_TX_OUT_OF_BD (ICSS_EMAC_SWITCH_ERROR_MAJOR + 8u) |
| Tx ran out of Buffer descriptors to use. More... | |
| #define | ICSS_EMAC_ERR_RX_CH_INVALID (ICSS_EMAC_SWITCH_ERROR_CRITICAL + 9u) |
| Rx Channel invalid number. More... | |
| #define | ICSS_EMAC_ERR_RX_CH_ALREADY_INIT (ICSS_EMAC_SWITCH_ERROR_MAJOR + 10u) |
| Rx Channel already setup. More... | |
| #define | ICSS_EMAC_ERR_RX_CH_ALREADY_CLOSED (ICSS_EMAC_SWITCH_ERROR_MAJOR + 11u) |
| Rx Channel already closed. Channel close failed. More... | |
| #define | ICSS_EMAC_ERR_RX_CH_NOT_OPEN (ICSS_EMAC_SWITCH_ERROR_MAJOR + 12u) |
| Rx Channel not open yet. More... | |
| #define | ICSS_EMAC_ERR_DEV_ALREADY_CREATED (ICSS_EMAC_SWITCH_ERROR_MAJOR + 13u) |
| EMAC device already created. More... | |
| #define | ICSS_EMAC_ERR_DEV_NOT_OPEN (ICSS_EMAC_SWITCH_ERROR_MAJOR + 14u) |
| Device is not open or not ready. More... | |
| #define | ICSS_EMAC_ERR_DEV_ALREADY_CLOSED (ICSS_EMAC_SWITCH_ERROR_MAJOR + 15u) |
| Device close failed. Device already closed. More... | |
| #define | ICSS_EMAC_ERR_DEV_ALREADY_OPEN (ICSS_EMAC_SWITCH_ERROR_MAJOR + 16u) |
| Device open failed. Device already open. More... | |
| #define | ICSS_EMAC_ERR_RX_BUFFER_ALLOC_FAIL (ICSS_EMAC_SWITCH_ERROR_CRITICAL + 17u) |
| Rx Buffer Descriptor allocation failed. More... | |
| #define | ICSS_EMAC_SWITCH_INTERNAL_FAILURE (ICSS_EMAC_SWITCH_ERROR_MAJOR + 18u) |
| EMAC Internal failure. More... | |
| #define | ICSS_EMAC_SWITCH_VLAN_UNAWARE_MODE (ICSS_EMAC_SWITCH_ERROR_MAJOR + 19u) |
| VLAN support not enabled in EMAC. More... | |
| #define | ICSS_EMAC_SWITCH_ALE_TABLE_FULL (ICSS_EMAC_SWITCH_ERROR_MAJOR + 20u) |
| ALE Table full. More... | |
| #define | ICSS_EMAC_SWITCH_ADDR_NOTFOUND (ICSS_EMAC_SWITCH_ERROR_MAJOR + 21u) |
| Multicast/Unicast/OUI Address not found in ALE. More... | |
| #define | ICSS_EMAC_SWITCH_INVALID_VLANID (ICSS_EMAC_SWITCH_ERROR_MAJOR + 22u) |
| Invalid VLAN Id. More... | |
| #define | ICSS_EMAC_SWITCH_INVALID_PORT (ICSS_EMAC_SWITCH_ERROR_MAJOR + 23u) |
| Invalid Port Specified. More... | |
| #define | ICSS_EMAC_SWITCH_BD_ALLOC_FAIL (ICSS_EMAC_SWITCH_ERROR_MAJOR + 24u) |
| Buffer Descriptor Allocation failure. OOM. More... | |
| #define | ICSS_EMAC_ERR_BADPACKET (ICSS_EMAC_SWITCH_ERROR_MAJOR + 25u) |
| Supplied packet was invalid. More... | |
| #define | ICSS_EMAC_ERR_COLLISION_FAIL (ICSS_EMAC_SWITCH_ERROR_MAJOR + 26u) |
| Collision queue was full. More... | |
| #define | ICSS_EMAC_ERR_MACFATAL (ICSS_EMAC_SWITCH_ERROR_CRITICAL + 26u) |
| Fatal Error - ICSS_EMAC_close required. More... | |
ICSS-EMAC Storm Prevention IOCTL Command Options | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_ENABLE (0u) |
| IOCTL Storm Control Enable command. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_DISABLE (1u) |
| IOCTL Storm Control Disable command. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_SET_CREDITS (2u) |
| IOCTL Storm Control set credit command. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_INIT (3u) |
| IOCTL Storm Control initialize command. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_RESET (4u) |
| IOCTL Storm Control reset command. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_ENABLE_BC (5u) |
| IOCTL Storm Control Enable command for BC traffic. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_DISABLE_BC (6u) |
| IOCTL Storm Control Disable command for BC traffic. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_SET_CREDITS_BC (7u) |
| IOCTL Storm Control set credit command for BC traffic. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_INIT_BC (8u) |
| IOCTL Storm Control initialize command for BC traffic. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_RESET_BC (9u) |
| IOCTL Storm Control reset command for BC traffic. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_ENABLE_MC (10u) |
| IOCTL Storm Control Enable command for MC traffic. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_DISABLE_MC (11u) |
| IOCTL Storm Control Disable command for MC traffic. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_SET_CREDITS_MC (12u) |
| IOCTL Storm Control set credit command for MC traffic. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_INIT_MC (13u) |
| IOCTL Storm Control initialize command for MC traffic. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_RESET_MC (14u) |
| IOCTL Storm Control reset command for MC traffic. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_ENABLE_UC (15u) |
| IOCTL Storm Control Enable command for UC traffic. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_DISABLE_UC (16u) |
| IOCTL Storm Control Disable command for UC traffic. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_SET_CREDITS_UC (17u) |
| IOCTL Storm Control set credit command for UC traffic. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_INIT_UC (18u) |
| IOCTL Storm Control initialize command for UC traffic. More... | |
| #define | ICSS_EMAC_STORM_PREV_CTRL_RESET_UC (19u) |
| IOCTL Storm Control reset command for UC traffic. More... | |
ICSS-EMAC Learning Control IOCTL Command Options | |
| #define | ICSS_EMAC_LEARN_CTRL_UPDATE_TABLE (0u) |
| IOCTL Learning Table update command. More... | |
| #define | ICSS_EMAC_LEARN_CTRL_CLR_TABLE (1u) |
| IOCTL Learning Table clear table command. More... | |
| #define | ICSS_EMAC_LEARN_CTRL_AGEING (2u) |
| IOCTL Learning Table age out entry command. More... | |
| #define | ICSS_EMAC_LEARN_CTRL_FIND_MAC (3u) |
| IOCTL Learning Table find port from MAC ID command. More... | |
| #define | ICSS_EMAC_LEARN_CTRL_REMOVE_MAC (4u) |
| IOCTL Learning Table remove a MAC ID from table command. More... | |
| #define | ICSS_EMAC_LEARN_CTRL_INC_COUNTER (5u) |
| IOCTL Learning Table increment counters (for ageing) command. More... | |
| #define | ICSS_EMAC_LEARN_CTRL_INIT_TABLE (6u) |
| IOCTL Learning Table initialize command. More... | |
| #define | ICSS_EMAC_LEARN_CTRL_SET_PORTSTATE (7u) |
| IOCTL Learning Table set port state command. More... | |
ICSS-EMAC Statistics IOCTL Command Options | |
| #define | ICSS_EMAC_IOCTL_STAT_CTRL_GET (0u) |
| IOCTL Statistics get from PRU command. More... | |
| #define | ICSS_EMAC_IOCTL_STAT_CTRL_CLEAR (1u) |
| IOCTL Statistics clear all counters command. More... | |
ICSS-EMAC IOCTL Command for selecting a module | |
| #define | ICSS_EMAC_IOCTL_PORT_CTRL (0u) |
| IOCTL select port control APIs command. More... | |
| #define | ICSS_EMAC_IOCTL_LEARNING_CTRL (1u) |
| IOCTL select learning Table APIs command. More... | |
| #define | ICSS_EMAC_IOCTL_STORM_PREV_CTRL (2u) |
| IOCTL select Storm Prevention APIs command. More... | |
| #define | ICSS_EMAC_IOCTL_STATS_CTRL (3u) |
| IOCTL select Statistics APIs command. More... | |
| #define | ICSS_EMAC_IOCTL_PROMISCUOUS_CTRL (4u) |
| IOCTL select Promiscuous Mode APIs command. More... | |
| #define | ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL (5u) |
| IOCTL select Multicast filtering APIs command. More... | |
| #define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL (6u) |
| IOCTL select Vlan filtering APIs command. More... | |
| #define | ICSS_EMAC_IOCTL_PORT_FLUSH_CTRL (7u) |
| IOCTL select Port flush APIs command. More... | |
| #define | ICSS_EMAC_IOCTL_SPECIAL_UNICAST_MAC_CTRL (8u) |
| IOCTL select Special Unicast MAC address APIs command. More... | |
| #define | ICSS_EMAC_IOCTL_PORT_FWD_CTRL (9u) |
| IOCTL select Port Forwarding APIs command. More... | |
ICSS-EMAC Multicast Filtering IOCTL Command Options | |
| #define | ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_ENABLE (0u) |
| IOCTL Multicast filter Control Enable command. More... | |
| #define | ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_DISABLE (1u) |
| IOCTL Multicast filter Control Disable command. More... | |
| #define | ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_OVERRIDE_HASHMASK (2u) |
| IOCTL Multicast filter Control override hashmask command. More... | |
| #define | ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_ADD_MACID (3u) |
| IOCTL Multicast filter Control allow MC MAC ID command. More... | |
| #define | ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_REMOVE_MACID (4u) |
| IOCTL Multicast filter Control do not allow MC MAC ID command. More... | |
| #define | ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_GET_DROPPED (5u) |
| IOCTL Multicast filter Control do not allow MC MAC ID command. More... | |
ICSS-EMAC VLAN Filtering IOCTL Command Options | |
| #define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_ENABLE_CMD (0u) |
| IOCTL Vlan filter Control Enable command. More... | |
| #define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_DISABLE_CMD (1u) |
| IOCTL Vlan filter Control Disable command. More... | |
| #define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_UNTAG_HOST_RCV_ALL_CMD (2u) |
| IOCTL Vlan filter allow Untagged frames Host Receive command. More... | |
| #define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_UNTAG_HOST_RCV_NAL_CMD (3u) |
| IOCTL Vlan filter do not allow Untagged frames Host Receive command. More... | |
| #define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_PRIOTAG_HOST_RCV_ALL_CMD (4u) |
| IOCTL Vlan filter allow Priority Tag frames Host Receive command. More... | |
| #define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_PRIOTAG_HOST_RCV_NAL_CMD (5u) |
| IOCTL Vlan filter do not allow Priority Tag frames Host Receive command. More... | |
| #define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_ADD_VID_CMD (6u) |
| IOCTL Vlan filter 4096 VIDs, 1 bit VIDs => 4096 bits = 512 bytes, ADD VLAN ID to allow packet to host More... | |
| #define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_REMOVE_VID_CMD (7u) |
| IOCTL Vlan filter 4096 VIDs, 1 bit VIDs => 4096 bits = 512 bytes, Remove VLAN ID to do not allow packet to host More... | |
ICSS-EMAC Special Unicast MAC IOCTL Command Options | |
| #define | ICSS_EMAC_IOCTL_SPECIAL_UNICAST_MAC_CTRL_DISABLE_CMD (0u) |
| IOCTL Special Unicast MAC Disable command. More... | |
| #define | ICSS_EMAC_IOCTL_SPECIAL_UNICAST_MAC_CTRL_ENABLE_CMD (1u) |
| IOCTL Special Unicast MAC Enable command. More... | |
ICSS-EMAC Port Forwarding IOCTL Command Options | |
| #define | ICSS_EMAC_IOCTL_PORT_FWD_CTRL_ENABLE_CMD (0u) |
| IOCTL Port Forwarding Enable command. More... | |
| #define | ICSS_EMAC_IOCTL_PORT_FWD_CTRL_DISABLE_CMD (1u) |
| IOCTL Port Forwarding Disable command. More... | |
Typedefs | |
| typedef struct ICSS_EMAC_Config_s * | ICSS_EMAC_Handle |
| Alias for ICSS EMAC Handle containing base addresses and modules. More... | |
| typedef int32_t(* | ICSS_EMAC_CallBack) (void *arg0, void *arg1, void *arg2) |
| Definition for a generic callback function used in ICSS-EMAC. While calling this, first argument is always of type ICSS_EMAC_Handle, second argument is specific to the callback (see ICSS_EMAC_CallBackObject), and third argument is userArg as specified in ICSS_EMAC_CallBackConfig. More... | |
Enumerations | |
| enum | ICSS_EMAC_pruRstIsoState { RESET_ISOLATION_DISABLED = 0U, RESET_ISOLATION_ENABLED = 1U, RESET_ISOLATION_NOT_SUPPORTED = 2U } |
Functions | |
| void | ICSS_EMAC_init (void) |
| This function initializes the ICSS_EMAC module. More... | |
| void | ICSS_EMAC_deinit (void) |
| This function de-initializes the ICSS_EMAC module. More... | |
| void | ICSS_EMAC_Params_init (ICSS_EMAC_Params *params) |
| Initialize the parmeters data structure with defaults. More... | |
| ICSS_EMAC_Handle | ICSS_EMAC_open (uint32_t idx, const ICSS_EMAC_Params *params) |
| API to initialize and configure ICSS in MAC/Switch Mode. More... | |
| void | ICSS_EMAC_close (ICSS_EMAC_Handle icssEmacHandle) |
| API to stop MAC/Switch Mode. More... | |
| int32_t | ICSS_EMAC_ioctl (ICSS_EMAC_Handle icssEmacHandle, uint32_t ioctlCommand, uint8_t portNo, void *ioctlParams) |
| IOCTL Function for ICSS EMAC. More... | |
| int32_t | ICSS_EMAC_rxPktGet (ICSS_EMAC_RxArgument *rxArg, void *userArg) |
| Retrieves a frame from a host queue and copies it in the allocated stack buffer. More... | |
| int32_t | ICSS_EMAC_rxPktInfo (ICSS_EMAC_Handle icssEmacHandle, int32_t *portNumber, int32_t *queueNumber) |
| API to retrieve the information about the received frame which is then used to dequeue the frame from the host queues. More... | |
| int32_t | ICSS_EMAC_txPacket (const ICSS_EMAC_TxArgument *txArg, void *userArg) |
| API to queue a frame which has to be transmitted on the specified port queue. More... | |
| ICSS_EMAC_pruRstIsoState | ICSS_EMAC_getResetIsolationStatus (ICSS_EMAC_Handle emacHandle) |
| Gets the reset isolation status from the ICSS_EMAC handle. More... | |