AM64x MCU+ SDK  12.01.00
enet_phymdio_dflt.h File Reference

Introduction

This file contains the interface to the default implementation of the MDIO driver defined by the Ethernet PHY driver (EnetPhy).

Go to the source code of this file.

Functions

int32_t EnetPhyMdioDflt_isAlive (uint32_t phyAddr, bool *isAlive, Mdio_Obj *hMdio)
 
int32_t EnetPhyMdioDflt_isLinked (uint32_t phyAddr, bool *isLinked, Mdio_Obj *hMdio)
 
int32_t EnetPhyMdioDflt_readC22 (uint32_t group, uint32_t phyAddr, uint32_t reg, uint16_t *val, Mdio_Obj *hMdio)
 
int32_t EnetPhyMdioDflt_writeC22 (uint32_t group, uint32_t phyAddr, uint32_t reg, uint16_t val, Mdio_Obj *hMdio)
 
int32_t EnetPhyMdioDflt_readC45 (uint32_t group, uint32_t phyAddr, uint8_t mmd, uint16_t reg, uint16_t *val, Mdio_Obj *hMdio)
 
int32_t EnetPhyMdioDflt_writeC45 (uint32_t group, uint32_t phyAddr, uint8_t mmd, uint16_t reg, uint16_t val, Mdio_Obj *hMdio)
 
EnetPhy_MdioHandle EnetPhyMdioDflt_getPhyMdio (void)
 Get handle to the default Enet MDIO implementation. More...
 
int32_t EnetPhyMdioDflt_ioctl (EnetPhy_Handle hPhy, uint32_t cmd, Enet_IoctlPrms *prms)
 Run an IOCTL operation on a PHY. More...
 

Function Documentation

◆ EnetPhyMdioDflt_isAlive()

int32_t EnetPhyMdioDflt_isAlive ( uint32_t  phyAddr,
bool *  isAlive,
Mdio_Obj *  hMdio 
)

◆ EnetPhyMdioDflt_isLinked()

int32_t EnetPhyMdioDflt_isLinked ( uint32_t  phyAddr,
bool *  isLinked,
Mdio_Obj *  hMdio 
)

◆ EnetPhyMdioDflt_readC22()

int32_t EnetPhyMdioDflt_readC22 ( uint32_t  group,
uint32_t  phyAddr,
uint32_t  reg,
uint16_t *  val,
Mdio_Obj *  hMdio 
)

◆ EnetPhyMdioDflt_writeC22()

int32_t EnetPhyMdioDflt_writeC22 ( uint32_t  group,
uint32_t  phyAddr,
uint32_t  reg,
uint16_t  val,
Mdio_Obj *  hMdio 
)

◆ EnetPhyMdioDflt_readC45()

int32_t EnetPhyMdioDflt_readC45 ( uint32_t  group,
uint32_t  phyAddr,
uint8_t  mmd,
uint16_t  reg,
uint16_t *  val,
Mdio_Obj *  hMdio 
)

◆ EnetPhyMdioDflt_writeC45()

int32_t EnetPhyMdioDflt_writeC45 ( uint32_t  group,
uint32_t  phyAddr,
uint8_t  mmd,
uint16_t  reg,
uint16_t  val,
Mdio_Obj *  hMdio 
)

◆ EnetPhyMdioDflt_getPhyMdio()

EnetPhy_MdioHandle EnetPhyMdioDflt_getPhyMdio ( void  )

Get handle to the default Enet MDIO implementation.

Gets a handle to the default EnetPhy MDIO driver implementation which is based on the Enet MDIO module.

Returns
Handle to the Enet based MDIO default implementation.

◆ EnetPhyMdioDflt_ioctl()

int32_t EnetPhyMdioDflt_ioctl ( EnetPhy_Handle  hPhy,
uint32_t  cmd,
Enet_IoctlPrms *  prms 
)

Run an IOCTL operation on a PHY.

Runs an IOCTL operation on a given PHY using the ENETPHY driver APIs. This IOCTL function can be used by Enet Peripheral drivers to handle PHY IOCTL commands if they use an ENETPHY driver.

Parameters
hPhyPHY handle
cmdIOCTL command Id
prmsIOCTL parameters
Returns
Enet_ErrorCodes