AM64x MCU+ SDK  12.01.00
enet_osal.h File Reference

Introduction

This file contains the OSAL API of the Enet driver.

Go to the source code of this file.

Data Structures

struct  SemaphoreP_enetOsal
 Semaphore structure. More...
 
struct  HwiP_enetOsal
 Hwi structure. More...
 

Typedefs

typedef void(* EnetOsal_Isr) (uintptr_t arg)
 Enet OSAL ISR callback function prototype. More...
 

Enumerations

enum  EnetOSAL_armGicTrigType_t {
  ENETOSAL_ARM_GIC_TRIG_TYPE_LEVEL = 1, ENETOSAL_ARM_GIC_TRIG_TYPE_EDGE = 2, ENETOSAL_ARM_GIC_TRIG_TYPE_HIGH_LEVEL = 3, ENETOSAL_ARM_GIC_TRIG_TYPE_LOW_LEVEL = 4,
  ENETOSAL_ARM_GIC_TRIG_TYPE_RISING_EDGE = 5, ENETOSAL_ARM_GIC_TRIG_TYPE_FALLING_EDGE = 6
}
 Enumerates the types different trigger types. Please refer to Section 4.3.13 Interrupt Configuration Registers, GICD_ICFGRn of ARM Generic Interrupt Controller Architecture version 2.0 Architecture Specification document for details. More...
 

Functions

uintptr_t EnetOsal_disableAllIntr (void)
 Enet OSAL intr disable function prototype. More...
 
void EnetOsal_restoreAllIntr (uintptr_t cookie)
 Enet OSAL intr restore function prototype. More...
 
HwiP_enetOsal * EnetOsal_registerIntr (EnetOsal_Isr isrFxn, uint32_t coreIntrNum, uint32_t intrPriority, uint32_t intrTrigType, void *arg)
 Register an ISR for an interrupt. More...
 
void EnetOsal_unregisterIntr (HwiP_enetOsal *hHwi)
 Unregister an interrupt. More...
 
void EnetOsal_enableIntr (uint32_t coreIntrNum)
 Enable interrupt. More...
 
void EnetOsal_disableIntr (uint32_t coreIntrNum)
 Disable interrupt. More...
 
SemaphoreP_enetOsal * EnetOsal_createMutex (void)
 Create a mutex. More...
 
void EnetOsal_deleteMutex (SemaphoreP_enetOsal *hMutex)
 Delete a mutex. More...
 
void EnetOsal_lockMutex (SemaphoreP_enetOsal *hMutex)
 Lock a mutex. More...
 
void EnetOsal_unlockMutex (SemaphoreP_enetOsal *hMutex)
 Unlock a mutex. More...
 
void EnetOsal_cacheInv (void *addr, int32_t size)
 Invalidate cache. More...
 
void EnetOsal_cacheWb (void *addr, int32_t size)
 Write-back cache. More...
 
void EnetOsal_cacheWbInv (void *addr, int32_t size)
 Write-back and invalidate cache. More...
 
bool EnetOsal_isCacheCoherent (void)
 
uint32_t EnetOsal_timerGetDiff (uint32_t startTime)
 Get the time difference with respect to timestamp. More...
 
uint32_t EnetOsal_timerRead (void)
 Read current timer value. More...
 

Typedef Documentation

◆ EnetOsal_Isr

typedef void(* EnetOsal_Isr) (uintptr_t arg)

Enet OSAL ISR callback function prototype.

Parameters
argApp data

Enumeration Type Documentation

◆ EnetOSAL_armGicTrigType_t

Enumerates the types different trigger types. Please refer to Section 4.3.13 Interrupt Configuration Registers, GICD_ICFGRn of ARM Generic Interrupt Controller Architecture version 2.0 Architecture Specification document for details.

Enumerator
ENETOSAL_ARM_GIC_TRIG_TYPE_LEVEL 

Corresponding interrupt is level sensitive

ENETOSAL_ARM_GIC_TRIG_TYPE_EDGE 

Corresponding interrupt is edge sensitive

ENETOSAL_ARM_GIC_TRIG_TYPE_HIGH_LEVEL 

Coressponding interrupt is high level sensitive

ENETOSAL_ARM_GIC_TRIG_TYPE_LOW_LEVEL 

Coressponding interrupt is low level sensitive

ENETOSAL_ARM_GIC_TRIG_TYPE_RISING_EDGE 

Coressponding interrupt is rising edge sensitive

ENETOSAL_ARM_GIC_TRIG_TYPE_FALLING_EDGE 

Coressponding interrupt is falling edge sensitive

Function Documentation

◆ EnetOsal_disableAllIntr()

uintptr_t EnetOsal_disableAllIntr ( void  )

Enet OSAL intr disable function prototype.

Returns
Cookie to be passed back to enable interrupt function

◆ EnetOsal_restoreAllIntr()

void EnetOsal_restoreAllIntr ( uintptr_t  cookie)

Enet OSAL intr restore function prototype.

Parameters
cookieThis is returned in disable interrupt function

◆ EnetOsal_registerIntr()

HwiP_enetOsal* EnetOsal_registerIntr ( EnetOsal_Isr  isrFxn,
uint32_t  coreIntrNum,
uint32_t  intrPriority,
uint32_t  intrTrigType,
void *  arg 
)

Register an ISR for an interrupt.

Parameters
isrFxnInterrupt service routine
coreIntrNumInterrupt number
intrPriorityInterrupt priority
intrTrigTypeInterrupt trigger type
argArgument to ISR function
Returns
Interrupt handle pointer

◆ EnetOsal_unregisterIntr()

void EnetOsal_unregisterIntr ( HwiP_enetOsal *  hHwi)

Unregister an interrupt.

Parameters
hHwiInterrupt handle pointer

◆ EnetOsal_enableIntr()

void EnetOsal_enableIntr ( uint32_t  coreIntrNum)

Enable interrupt.

Parameters
coreIntrNumInterrupt number

◆ EnetOsal_disableIntr()

void EnetOsal_disableIntr ( uint32_t  coreIntrNum)

Disable interrupt.

Parameters
coreIntrNumInterrupt number

◆ EnetOsal_createMutex()

SemaphoreP_enetOsal* EnetOsal_createMutex ( void  )

Create a mutex.

Returns
Mutex handle pointer

◆ EnetOsal_deleteMutex()

void EnetOsal_deleteMutex ( SemaphoreP_enetOsal *  hMutex)

Delete a mutex.

Parameters
hMutexMutex handle pointer

◆ EnetOsal_lockMutex()

void EnetOsal_lockMutex ( SemaphoreP_enetOsal *  hMutex)

Lock a mutex.

Parameters
hMutexMutex handle pointer

◆ EnetOsal_unlockMutex()

void EnetOsal_unlockMutex ( SemaphoreP_enetOsal *  hMutex)

Unlock a mutex.

Parameters
hMutexMutex handle pointer

◆ EnetOsal_cacheInv()

void EnetOsal_cacheInv ( void *  addr,
int32_t  size 
)

Invalidate cache.

Invalidates cache in a range of memory.

Parameters
addrStart address of the cache line(s)
sizeSize (in bytes) of the memory to invalidate

◆ EnetOsal_cacheWb()

void EnetOsal_cacheWb ( void *  addr,
int32_t  size 
)

Write-back cache.

Writes back cache a range of memory from cache.

Parameters
addrStart address of the cache line(s)
sizeSize (in bytes) of the memory to be written back

◆ EnetOsal_cacheWbInv()

void EnetOsal_cacheWbInv ( void *  addr,
int32_t  size 
)

Write-back and invalidate cache.

Writes back and invalidates a range of memory.

Parameters
addrStart address of the cache line/s
sizeSize (in bytes) of the memory to be written back

◆ EnetOsal_isCacheCoherent()

bool EnetOsal_isCacheCoherent ( void  )

◆ EnetOsal_timerGetDiff()

uint32_t EnetOsal_timerGetDiff ( uint32_t  startTime)

Get the time difference with respect to timestamp.

Gets the difference between time value passed to this function and current time from timer.

Returns
Time difference

◆ EnetOsal_timerRead()

uint32_t EnetOsal_timerRead ( void  )

Read current timer value.

Returns
Timer's read value