This file contains the type definitions and helper macros for the DP83TC812 Ethernet PHY.
Go to the source code of this file.
Data Structures | |
| struct | Dp83tc812_Cfg |
| DP83TC812 PHY configuration parameters. More... | |
Enumerations | |
| enum | Dp83tc812_MasterSlaveMode { DP83TC812_MASTER_SLAVE_STRAP = 0x0U, DP83TC812_MASTER_MODE = 0x1U, DP83TC812_SLAVE_MODE = 0x2U } |
| DP83TC812 Master/Slave modes. More... | |
Functions | |
| void | Dp83tc812_initCfg (Dp83tc812_Cfg *cfg) |
| Initialize DP83TC812 PHY specific config params. More... | |
| void | Dp83tc812_bind (EthPhyDrv_Handle *hPhy, uint8_t phyAddr, Phy_RegAccessCb_t *pRegAccessCb) |
| bool | Dp83tc812_isPhyDevSupported (EthPhyDrv_Handle hPhy, const void *pversion) |
| bool | Dp83tc812_isMacModeSupported (EthPhyDrv_Handle hPhy, Phy_Mii mii) |
| int32_t | Dp83tc812_config (EthPhyDrv_Handle hPhy, const void *pExtCfg, const uint32_t extCfgSize, Phy_Mii mii, bool loopbackEn) |
| int32_t | Dp83tc812_reset (EthPhyDrv_Handle hPhy) |
| int32_t | Dp83tc812_isResetComplete (EthPhyDrv_Handle hPhy, bool *pCompleted) |
| void | Dp83tc812_printRegs (EthPhyDrv_Handle hPhy) |