This file contains the type definitions and helper macros for the DP83822 Ethernet PHY.
Go to the source code of this file.
Data Structures | |
| struct | Dp83822_Cfg |
| DP83822 PHY configuration parameters. More... | |
Functions | |
| void | Dp83822_initCfg (Dp83822_Cfg *cfg) |
| Initialize DP83822 PHY specific config params. More... | |
| void | Dp83822_bind (EthPhyDrv_Handle *hPhy, uint8_t phyAddr, Phy_RegAccessCb_t *pRegAccessCb) |
| bool | Dp83822_isPhyDevSupported (EthPhyDrv_Handle hPhy, const void *pVersion) |
| bool | Dp83822_isMacModeSupported (EthPhyDrv_Handle hPhy, Phy_Mii mii) |
| int32_t | Dp83822_config (EthPhyDrv_Handle hPhy, const void *pExtCfg, const uint32_t extCfgSize, Phy_Mii mii, bool loopbackEn) |
| void | Dp83822_printRegs (EthPhyDrv_Handle hPhy) |