AM64x MCU+ SDK  12.01.00
v0 Directory Reference

Files

file  canfd.h [code]
 This is the header file for the CANFD driver which exposes the data structures and exported API which can be used by the applications to use the CANFD driver.
 
file  mcan.h [code]
 This file contains the prototypes of the APIs present in the device abstraction layer file of MCAN. This also contains some related macros.