AM64x MCU+ SDK  12.01.00

Introduction

This file contains the prototypes of the APIs present in the device abstraction layer file of ADC. This also contains some related macros.

Go to the source code of this file.

ADC Fifo Num

#define ADC_CHANNEL_1   (ADC_STEPCONFIG_SEL_INM_SWC_CHANNEL_1)
 
#define ADC_CHANNEL_2   (ADC_STEPCONFIG_SEL_INM_SWC_CHANNEL_2)
 
#define ADC_CHANNEL_3   (ADC_STEPCONFIG_SEL_INM_SWC_CHANNEL_3)
 
#define ADC_CHANNEL_4   (ADC_STEPCONFIG_SEL_INM_SWC_CHANNEL_4)
 
#define ADC_CHANNEL_5   (ADC_STEPCONFIG_SEL_INM_SWC_CHANNEL_5)
 
#define ADC_CHANNEL_6   (ADC_STEPCONFIG_SEL_INM_SWC_CHANNEL_6)
 
#define ADC_CHANNEL_7   (ADC_STEPCONFIG_SEL_INM_SWC_CHANNEL_7)
 
#define ADC_CHANNEL_8   (ADC_STEPCONFIG_SEL_INM_SWC_CHANNEL_8)
 
#define ADC_FIFO_NUM_0   (0x0U)
 
#define ADC_FIFO_NUM_1   (0x1U)
 
typedef uint32_t adcChannel_t
 Enum to select the channel for input. More...
 
typedef uint32_t adcFIFONum_t
 Enum to select FIFO to store the data. More...
 

ADC Step Id

#define ADC_STEP_1   (ADC_ADCSTAT_STEP_ID_STEP1)
 
#define ADC_STEP_2   (ADC_ADCSTAT_STEP_ID_STEP2)
 
#define ADC_STEP_3   (ADC_ADCSTAT_STEP_ID_STEP3)
 
#define ADC_STEP_4   (ADC_ADCSTAT_STEP_ID_STEP4)
 
#define ADC_STEP_5   (ADC_ADCSTAT_STEP_ID_STEP5)
 
#define ADC_STEP_6   (ADC_ADCSTAT_STEP_ID_STEP6)
 
#define ADC_STEP_7   (ADC_ADCSTAT_STEP_ID_STEP7)
 
#define ADC_STEP_8   (ADC_ADCSTAT_STEP_ID_STEP8)
 
#define ADC_STEP_9   (ADC_ADCSTAT_STEP_ID_STEP9)
 
#define ADC_STEP_10   (ADC_ADCSTAT_STEP_ID_STEP10)
 
#define ADC_STEP_11   (ADC_ADCSTAT_STEP_ID_STEP11)
 
#define ADC_STEP_12   (ADC_ADCSTAT_STEP_ID_STEP12)
 
#define ADC_STEP_13   (ADC_ADCSTAT_STEP_ID_STEP13)
 
#define ADC_STEP_14   (ADC_ADCSTAT_STEP_ID_STEP14)
 
#define ADC_STEP_15   (ADC_ADCSTAT_STEP_ID_STEP15)
 
#define ADC_STEP_16   (ADC_ADCSTAT_STEP_ID_STEP16)
 
typedef uint32_t adcStepId_t
 Enum to select the step for operation. More...
 

ADC Operation Mode

#define ADC_OPERATION_MODE_SINGLE_SHOT   (ADC_STEPCONFIG_MODE_SW_EN_ONESHOT)
 
#define ADC_OPERATION_MODE_CONTINUOUS   (ADC_STEPCONFIG_MODE_SW_EN_CONTINUOUS)
 
typedef uint32_t adcOperationMode_t
 Enum to select the ADC Operation Mode. More...
 

ADC Averaging

#define ADC_AVERAGING_NONE   (ADC_STEPCONFIG_AVERAGING_NOAVG)
 
#define ADC_AVERAGING_2_SAMPLES   (ADC_STEPCONFIG_AVERAGING_2_SAMPLESAVG)
 
#define ADC_AVERAGING_4_SAMPLES   (ADC_STEPCONFIG_AVERAGING_4_SAMPLESAVG)
 
#define ADC_AVERAGING_8_SAMPLES   (ADC_STEPCONFIG_AVERAGING_8_SAMPLESAVG)
 
#define ADC_AVERAGING_16_SAMPLES   (ADC_STEPCONFIG_AVERAGING_16_SAMPLESAV)
 
typedef uint32_t adcAveraging_t
 Enum to number of samplings to average. More...
 

ADC Interrupt source

#define ADC_INTR_SRC_END_OF_SEQUENCE   (ADC_IRQENABLE_SET_END_OF_SEQUENCE_MASK)
 
#define ADC_INTR_SRC_FIFO0_THRESHOLD   (ADC_IRQENABLE_SET_FIFO0_THR_MASK)
 
#define ADC_INTR_SRC_FIFO0_OVERRUN   (ADC_IRQENABLE_SET_FIFO0_OVERRUN_MASK)
 
#define ADC_INTR_SRC_FIFO0_UNDERFLOW   (ADC_IRQENABLE_SET_FIFO0_UNDERFLOW_MASK)
 
#define ADC_INTR_SRC_FIFO1_THRESHOLD   (ADC_IRQENABLE_SET_FIFO1_THR_MASK)
 
#define ADC_INTR_SRC_FIFO1_OVERRUN   (ADC_IRQSTATUS_FIFO1_OVERRUN_MASK)
 
#define ADC_INTR_SRC_FIFO1_UNDERFLOW   (ADC_IRQENABLE_SET_FIFO1_UNDERFLOW_MASK)
 
#define ADC_INTR_SRC_OUT_OF_RANGE   (ADC_IRQENABLE_SET_OUT_OF_RANGE_MASK)
 
typedef uint32_t adcIntrSrc_t
 Enum for ADC interrupts. More...
 

ADC Idle mode

#define ADC_IDLE_MODE_FORCE_IDLE   (ADC_SYSCONFIG_IDLEMODE_FORCE)
 
#define ADC_IDLE_MODE_NO_IDLE   (ADC_SYSCONFIG_IDLEMODE_NO_IDLE)
 
#define ADC_IDLE_MODE_SMART_IDLE   (ADC_SYSCONFIG_IDLEMODE_SMART_IDLE)
 
typedef uint32_t adcIdleMode_t
 Enum to configure ADC idle mode.Applicable for TDA3XX Only. More...
 

Data Structures

struct  adcRevisionId_t
 Structure for accessing Revision ID of ADC module. More...
 
struct  adcStepConfig_t
 Structure containing parameters for ADC step configuration. More...
 
struct  adcSequencerStatus_t
 Structure for reporting ADC sequencer status. More...
 

Macros

#define ADC_INTR_STATUS_ALL
 Macro defines mask for all the interrupts status for ADC. More...
 
#define ADC_INTR_ENABLE_ALL
 Macro defines mask for all the interrupts to enable for ADC. More...
 
#define ADC_INTR_DISABLE_ALL
 Macro defines mask for all the interrupts to disable for ADC. More...
 
#define ADC_INTR_ALL   (ADC_INTR_STATUS_ALL)
 Macro defines mask for all the interrupts for ADC. More...
 
#define ADC_OPENDELAY_MAX   (0x3FFFFU)
 Macro defines the maximum value of open delay for a step for ADC. More...
 
#define ADC_SAMPLEDELAY_MAX   (0xFFU)
 Macro defines the maximum value of sample delay for a step for ADC. More...
 
#define ADC_RANGE_MAX   (0x3FFU)
 Macro defines the maximum allowable range for ADC. More...
 
#define ADC_RANGE_MIN   (0x0U)
 Macro defines the minimum allowable range for ADC. More...
 
#define ADC_FIFO_SIZE   (64U)
 Macro defines the maximum number of samples FIFO0 can store. More...
 
#define ADC_MAX_NUM_CHN   (uint32_t)(8U)
 Macro defines the maximum number of channels in ADC. More...
 
#define ADC_GET_RANGE(bit)   (((uint32_t) 1U) << (bit))
 Returns the ADC max range given the bit support. More...
 

Functions

void ADCPowerUp (uint32_t baseAddr, uint32_t powerUp)
 This API will power up ADC Module. More...
 
uint32_t AdcIsPoweredUp (uint32_t baseAddr)
 This function checks if the ADC module is powered up. More...
 
int32_t ADCSetClkDivider (uint32_t baseAddr, uint32_t clkDivider)
 This API will configure clock divider for the ADC Module. More...
 
void ADCInit (uint32_t baseAddr, uint32_t errCorrection, uint32_t errOffset, uint32_t calibration)
 This API is used to initialize the ADC module. More...
 
void ADCFIFODMAAccessEnable (uint32_t baseAddr, uint32_t fifoNum, uint32_t dmaLineEnable)
 This API will enable DMA access for FIFO. More...
 
int32_t ADCSetStepParams (uint32_t baseAddr, uint32_t stepId, const adcStepConfig_t *configParams)
 This API will configure a step for analog to digital conversion. More...
 
void ADCStepEnable (uint32_t baseAddr, uint32_t stepId, uint32_t stepEnable)
 This API will enable ADC step. More...
 
void ADCClearAllSteps (uint32_t baseAddr)
 This API will clear all the ADC steps. More...
 
void ADCStart (uint32_t baseAddr, uint32_t adcEnable)
 This API will start ADC. More...
 
void ADCStepIdTagEnable (uint32_t baseAddr, uint32_t stepIdTag)
 This API is used to configure the ADC module for storing step ID along with ADC data. More...
 
uint32_t ADCGetFIFOData (uint32_t baseAddr, uint32_t fifoNum)
 This API will read and return FIFO data. More...
 
uint32_t ADCGetFIFOWordCount (uint32_t baseAddr, uint32_t fifoNum)
 This API will return number of word present in the FIFO. More...
 
int32_t ADCSetCPUFIFOThresholdLevel (uint32_t baseAddr, uint32_t fifoNum, uint32_t threshold)
 This API will configure threshold level for a FIFO. More...
 
uint32_t ADCGetCPUFIFOThresholdLevel (uint32_t baseAddr, uint32_t fifoNum)
 This API will read and return threshold level for a FIFO. More...
 
int32_t ADCSetDMAFIFOThresholdLevel (uint32_t baseAddr, uint32_t fifoNum, uint32_t threshold)
 This API will configure DMA request level for a FIFO. More...
 
uint32_t ADCGetDMAFIFOThresholdLevel (uint32_t baseAddr, uint32_t fifoNum)
 This API will read and return DMA request level for a FIFO. More...
 
void ADCEnableIntr (uint32_t baseAddr, uint32_t intrMask)
 This API is used to enable interrupts. More...
 
void ADCDisableIntr (uint32_t baseAddr, uint32_t intrMask)
 This API is used to disable interrupts. More...
 
void ADCWriteEOI (uint32_t baseAddr)
 This API is used for EOI for ADC. More...
 
uint32_t ADCGetIntrStatus (uint32_t baseAddr)
 This API is used to get the pending interrupts. More...
 
void ADCClearIntrStatus (uint32_t baseAddr, uint32_t intrMask)
 This API is used to clear the interrupt status. More...
 
uint32_t ADCGetIntrRawStatus (uint32_t baseAddr)
 This API is used to get the raw interrupt status. More...
 
int32_t ADCSetRange (uint32_t baseAddr, uint32_t highRange, uint32_t lowRange)
 This API is used to configure the range for ADC. More...
 
void ADCGetRange (uint32_t baseAddr, uint32_t *highRange, uint32_t *lowRange)
 This API is used to get the range for conversion. More...
 
void ADCGetSequencerStatus (uint32_t baseAddr, adcSequencerStatus_t *status)
 This API is used to get the Sequencer status. More...
 
void ADCSetIdleMode (uint32_t baseAddr, uint32_t idleMode)
 This API is used to configure ADC idle mode. More...
 
void ADCGetRevisionId (uint32_t baseAddr, adcRevisionId_t *revId)
 This API is used get the ADC revision ID. More...