Files | |
file | cb_lld_ethernet.h |
TI ENET LLD specific network layer part. | |
Data Structures | |
struct | ethhdr |
Ethernet header structure. More... | |
struct | lld_sockaddr_t |
Structure representing the lld_sockaddr instance. More... | |
struct | sockaddr |
struct | lld_ethdev_t |
Structure representing the lld_ethdev instance. More... | |
struct | cb_socket_lldcfg_update_t |
Structure representing the cb_socket_lldcfg_update instance. More... | |
Functions | |
struct ethhdr | __attribute__ ((packed)) |
int | cb_lld_init_devs_table (lld_ethdev_t *ethdevs, uint32_t ndevs, uint32_t enet_type, uint32_t instance_id) |
Initialize a LLD device table. More... | |
int | cb_socket_set_lldcfg_update_cb (cb_socket_lldcfg_update_cb_t lldcfg_update_cb) |
This function sets the callback for updating LLD config parameters. It enables the user to update config parameters for the Enet LLD layer that are not supported by the CB socket. It is important to note that this function should only be called once. More... | |
int | cb_lld_netdev_to_macport (const char *netdev) |
Convert net device name to mac port. More... | |
int | cb_lld_sendto (CB_SOCKET_T sfd, void *sdata, int psize, int flags, CB_SOCKADDR_LL_T *addr, int addrsize) |
Send a TX ethernet L2 packet. More... | |
int | cb_lld_recv (CB_SOCKET_T sfd, void *buf, int size, int *port) |
Receive a RX ethernet L2 packet. This should be called after a rxnotify_cb is invoked. More... | |
int | cb_lld_set_txnotify_cb (CB_SOCKET_T sfd, void(*txnotify_cb)(void *arg), void *arg) |
Set the TX notify callback that is invoked when an TX packet is sent successfully. More... | |
int | cb_lld_set_rxnotify_cb (CB_SOCKET_T sfd, void(*rxnotify_cb)(void *arg), void *arg) |
Set the RX notify callback that is invoked when an RX packet is ready to be received. More... | |
int | cb_lld_get_type_instance (uint32_t *enet_type, uint32_t *instance_id) |
Get enet type and instance that is set via cb_lld_init_devs_table() More... | |
int | cb_lld_get_netdevs (char *netdevs[], int *len) |
Get all virtual network interfaces which were defined for the TI platform. More... | |
int | cb_lld_get_link_state (CB_SOCKET_T cfd, const char *dev, uint32_t *linkstate) |
get link state from device name like 'eth0' More... | |
int | cb_lld_get_link_info (CB_SOCKET_T cfd, const char *dev, uint32_t *speed, uint32_t *duplex) |
get link info(speed and duplex) from device name like 'eth0' More... | |
Typedefs | |
typedef int(* | cb_ipcsocket_server_rdcb) (void *cbdata, uint8_t *rdata, int size, struct sockaddr *addr) |
typedef struct lld_socket | lld_socket_t |
Structure representing the lld_socket instance. More... | |
typedef int(* | cb_socket_lldcfg_update_cb_t) (cb_socket_lldcfg_update_t *update_cfg) |
Callback function type for cb_socket_lldcfg_update. More... | |
Macros | |
#define | htons __htons |
#define | ntohs __ntohs |
#define | htonl __htonl |
#define | ntohl __ntohl |
#define | MAX_NUMBER_ENET_DEVS LLDENET_MAX_PORTS |
#define | CB_SOCKET_VALID(x) ((x)!=NULL) |
#define | CB_SOCKET_INVALID_VALUE NULL |
#define | CB_SOCKET_T lld_socket_t* |
#define | CB_ETHHDR_T struct ethhdr |
#define | CB_SOCKADDR_LL_T lld_sockaddr_t |
#define | CB_SOCK_SENDTO cb_lld_sendto |
#define | CB_IN_ADDR_T void* |
#define | IFNAMSIZ 16 |
#define | ETH_ALEN 6 /* Octets in one ethernet addr */ |
#define | ETH_HLEN 14 /* Total octets in header. */ |
#define | ETH_DATA_LEN 1500 /* Max. octets in payload */ |
#define | ETH_P_8021Q 0x8100 /* 802.1Q VLAN Extended Header */ |
#define | ETH_P_1588 0x88F7 /* IEEE 1588 Timesync */ |
#define | ETH_P_TSN 0x22F0 /* TSN (IEEE 1722) packet */ |
#define | ETH_P_NETLINK 0x22F1 /* A virtual prototol for netlink rawsockt on TI platforms */ |
#define | CB_MAX_NETDEVNAME IFNAMSIZ |
#define | MKPIPE(x) (-1) |
#define | CB_LLD_MAX_ETH_FRAME_SIZE (1522U) |
#define htons __htons |
#define ntohs __ntohs |
#define htonl __htonl |
#define ntohl __ntohl |
#define MAX_NUMBER_ENET_DEVS LLDENET_MAX_PORTS |
#define CB_SOCKET_VALID | ( | x | ) | ((x)!=NULL) |
#define CB_SOCKET_INVALID_VALUE NULL |
#define CB_SOCKET_T lld_socket_t* |
#define CB_ETHHDR_T struct ethhdr |
#define CB_SOCKADDR_LL_T lld_sockaddr_t |
#define CB_SOCK_SENDTO cb_lld_sendto |
#define CB_IN_ADDR_T void* |
#define IFNAMSIZ 16 |
#define ETH_ALEN 6 /* Octets in one ethernet addr */ |
#define ETH_HLEN 14 /* Total octets in header. */ |
#define ETH_DATA_LEN 1500 /* Max. octets in payload */ |
#define ETH_P_8021Q 0x8100 /* 802.1Q VLAN Extended Header */ |
#define ETH_P_1588 0x88F7 /* IEEE 1588 Timesync */ |
#define ETH_P_TSN 0x22F0 /* TSN (IEEE 1722) packet */ |
#define ETH_P_NETLINK 0x22F1 /* A virtual prototol for netlink rawsockt on TI platforms */ |
#define CB_MAX_NETDEVNAME IFNAMSIZ |
#define MKPIPE | ( | x | ) | (-1) |
#define CB_LLD_MAX_ETH_FRAME_SIZE (1522U) |
typedef int(* cb_ipcsocket_server_rdcb) (void *cbdata, uint8_t *rdata, int size, struct sockaddr *addr) |
typedef struct lld_socket lld_socket_t |
Structure representing the lld_socket instance.
cb_socket_lldcfg_update_cb_t |
Callback function type for cb_socket_lldcfg_update.
update_cfg | Pointer to the cb_socket_lldcfg_update instance. |
struct ethhdr __attribute__ | ( | (packed) | ) |
int cb_lld_init_devs_table | ( | lld_ethdev_t * | ethdevs, |
uint32_t | ndevs, | ||
uint32_t | enet_type, | ||
uint32_t | instance_id | ||
) |
Initialize a LLD device table.
This function should only be called once, before calling any net functions from the combase. It is recommended to call once in the main() application, not in any TSN module source. If the ethdevs[i].srcmac is all zero, the srcmac will be alloced dynamically by the the LLD layer. Please note that ethdevs[i].netdev must point to a global memory address, not a stack memory address.
ethdevs | an arrays of ethernet devices |
ndevs | number of devices in the array |
enet_type | LLD ethernet type |
instance_id | LLD ethernet instance ID |
int cb_socket_set_lldcfg_update_cb | ( | cb_socket_lldcfg_update_cb_t | lldcfg_update_cb | ) |
This function sets the callback for updating LLD config parameters. It enables the user to update config parameters for the Enet LLD layer that are not supported by the CB socket. It is important to note that this function should only be called once.
lldcfg_update_cb | update callback |
int cb_lld_netdev_to_macport | ( | const char * | netdev | ) |
Convert net device name to mac port.
netdev | net device name e.g. eth0 |
int cb_lld_sendto | ( | CB_SOCKET_T | sfd, |
void * | sdata, | ||
int | psize, | ||
int | flags, | ||
CB_SOCKADDR_LL_T * | addr, | ||
int | addrsize | ||
) |
Send a TX ethernet L2 packet.
sfd | socket fd |
sdata | ethernet L2 packet |
psize | packet size |
flags | it is unused now, keep it to make it compatible with POSIX sendto |
addr | destination address info |
addrsize | address size |
int cb_lld_recv | ( | CB_SOCKET_T | sfd, |
void * | buf, | ||
int | size, | ||
int * | port | ||
) |
Receive a RX ethernet L2 packet. This should be called after a rxnotify_cb is invoked.
sfd | socket fd |
buf | packet buffer |
size | buffer size |
port | RX port |
int cb_lld_set_txnotify_cb | ( | CB_SOCKET_T | sfd, |
void(*)(void *arg) | txnotify_cb, | ||
void * | arg | ||
) |
Set the TX notify callback that is invoked when an TX packet is sent successfully.
sfd | socket fd |
txnotify_cb | callback |
arg | callback argument |
int cb_lld_set_rxnotify_cb | ( | CB_SOCKET_T | sfd, |
void(*)(void *arg) | rxnotify_cb, | ||
void * | arg | ||
) |
Set the RX notify callback that is invoked when an RX packet is ready to be received.
sfd | socket fd |
rxnotify_cb | callback |
arg | callback argument |
int cb_lld_get_type_instance | ( | uint32_t * | enet_type, |
uint32_t * | instance_id | ||
) |
Get enet type and instance that is set via cb_lld_init_devs_table()
enet_type | ethernet type |
instance_id | ethernet instance ID |
int cb_lld_get_netdevs | ( | char * | netdevs[], |
int * | len | ||
) |
Get all virtual network interfaces which were defined for the TI platform.
netdevs | an array of pointer points to the net devices acquired by this api. |
len | how many net devices are returned by this api. |
int cb_lld_get_link_state | ( | CB_SOCKET_T | cfd, |
const char * | dev, | ||
uint32_t * | linkstate | ||
) |
get link state from device name like 'eth0'
cfd | a socket handle coressponding to the ethernet device name specified via the second argument dev |
dev | ethernet device name like 'eth0' |
linkstate | a pointer for storing link state value (0:down, 1:up) |
int cb_lld_get_link_info | ( | CB_SOCKET_T | cfd, |
const char * | dev, | ||
uint32_t * | speed, | ||
uint32_t * | duplex | ||
) |
get link info(speed and duplex) from device name like 'eth0'
cfd | a socket handle coressponding to the ethernet device name specified via the second argument dev |
dev | ethenert device name like 'eth0' |
speed | a pointer for storing speed value (0:unknow, 10:10Mbps, 100:100Mbps, 1000:1Gbps) |
duplex | a pointer for storing duplex value (0:unknow, 1:Full, 2:Half) |
struct UInteger224 __attribute__ |
UInteger224 (802.1AS, 10.3.4 time-synchronization spanning tree priority vectors )