AM64x MCU+ SDK  09.00.00
cb_lld_ethernet.h File Reference

Introduction

TI ENET LLD specific network layer part.

Go to the source code of this file.

Data Structures

struct  ethhdr
 Ethernet header structure. More...
 
struct  lld_sockaddr_t
 Structure representing the lld_sockaddr instance. More...
 
struct  sockaddr
 
struct  lld_ethdev_t
 Structure representing the lld_ethdev instance. More...
 
struct  cb_socket_lldcfg_update_t
 Structure representing the cb_socket_lldcfg_update instance. More...
 

Macros

#define htons   __htons
 
#define ntohs   __ntohs
 
#define htonl   __htonl
 
#define ntohl   __ntohl
 
#define MAX_NUMBER_ENET_DEVS   LLDENET_MAX_PORTS
 
#define CB_SOCKET_VALID(x)   ((x)!=NULL)
 
#define CB_SOCKET_INVALID_VALUE   NULL
 
#define CB_SOCKET_T   lld_socket_t*
 
#define CB_ETHHDR_T   struct ethhdr
 
#define CB_SOCKADDR_LL_T   lld_sockaddr_t
 
#define CB_SOCK_SENDTO   cb_lld_sendto
 
#define CB_IN_ADDR_T   void*
 
#define IFNAMSIZ   16
 
#define ETH_ALEN   6 /* Octets in one ethernet addr */
 
#define ETH_HLEN   14 /* Total octets in header. */
 
#define ETH_DATA_LEN   1500 /* Max. octets in payload */
 
#define ETH_P_8021Q   0x8100 /* 802.1Q VLAN Extended Header */
 
#define ETH_P_1588   0x88F7 /* IEEE 1588 Timesync */
 
#define ETH_P_TSN   0x22F0 /* TSN (IEEE 1722) packet */
 
#define ETH_P_NETLINK   0x22F1 /* A virtual prototol for netlink rawsockt on TI platforms */
 
#define CB_MAX_NETDEVNAME   IFNAMSIZ
 
#define MKPIPE(x)   (-1)
 
#define CB_LLD_MAX_ETH_FRAME_SIZE   (1522U)
 

Typedefs

typedef int(* cb_ipcsocket_server_rdcb) (void *cbdata, uint8_t *rdata, int size, struct sockaddr *addr)
 
typedef struct lld_socket lld_socket_t
 Structure representing the lld_socket instance. More...
 
typedef int(* cb_socket_lldcfg_update_cb_t) (cb_socket_lldcfg_update_t *update_cfg)
 Callback function type for cb_socket_lldcfg_update. More...
 

Functions

struct ethhdr __attribute__ ((packed))
 
int cb_lld_init_devs_table (lld_ethdev_t *ethdevs, uint32_t ndevs, uint32_t enet_type, uint32_t instance_id)
 Initialize a LLD device table. More...
 
int cb_socket_set_lldcfg_update_cb (cb_socket_lldcfg_update_cb_t lldcfg_update_cb)
 This function sets the callback for updating LLD config parameters. It enables the user to update config parameters for the Enet LLD layer that are not supported by the CB socket. It is important to note that this function should only be called once. More...
 
int cb_lld_netdev_to_macport (const char *netdev)
 Convert net device name to mac port. More...
 
int cb_lld_sendto (CB_SOCKET_T sfd, void *sdata, int psize, int flags, CB_SOCKADDR_LL_T *addr, int addrsize)
 Send a TX ethernet L2 packet. More...
 
int cb_lld_recv (CB_SOCKET_T sfd, void *buf, int size, int *port)
 Receive a RX ethernet L2 packet. This should be called after a rxnotify_cb is invoked. More...
 
int cb_lld_set_txnotify_cb (CB_SOCKET_T sfd, void(*txnotify_cb)(void *arg), void *arg)
 Set the TX notify callback that is invoked when an TX packet is sent successfully. More...
 
int cb_lld_set_rxnotify_cb (CB_SOCKET_T sfd, void(*rxnotify_cb)(void *arg), void *arg)
 Set the RX notify callback that is invoked when an RX packet is ready to be received. More...
 
int cb_lld_get_type_instance (uint32_t *enet_type, uint32_t *instance_id)
 Get enet type and instance that is set via cb_lld_init_devs_table() More...
 
int cb_lld_get_netdevs (char *netdevs[], int *len)
 Get all virtual network interfaces which were defined for the TI platform. More...
 
int cb_lld_get_link_state (CB_SOCKET_T cfd, const char *dev, uint32_t *linkstate)
 get link state from device name like 'eth0' More...
 
int cb_lld_get_link_info (CB_SOCKET_T cfd, const char *dev, uint32_t *speed, uint32_t *duplex)
 get link info(speed and duplex) from device name like 'eth0' More...
 

Variables

typedef __attribute__
 UInteger224 (802.1AS, 10.3.4 time-synchronization spanning tree priority vectors ) More...
 
uint8_t h_dest [ETH_ALEN]
 
uint8_t h_source [ETH_ALEN]
 
uint16_t h_proto
 

Variable Documentation

◆ h_dest

uint8_t h_dest[ETH_ALEN]

Destination Ethernet address.

◆ h_source

uint8_t h_source[ETH_ALEN]

Source Ethernet address.

◆ h_proto

uint16_t h_proto

Ethernet type in the ethernet frame