IO-Link Master1.09.04
IOLM_SMI_SWSingleScanStatusList Struct Reference

This structure is used for the Scan Status List of a single scan result. More...

#include <IOLM_SMI_Types.h>

Data Fields

INT16U u16ArgBlockID
 Big endian.
 
INT8U u8ScanStatus
 Scan status.
 
INT8U u8ScanResults
 Number of scan results (max 255).
 
IOLM_SMI_SScanStatusResult asResult [1]
 array of scan results
 

Detailed Description

This structure is used for the Scan Status List of a single scan result.

The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_WScanStatusList = 0x9201.