IO-Link Master1.09.04
IOLM_SMI_SSPDUIn Struct Reference

This structure is used for SPDU input. More...

#include <IOLM_SMI_Types.h>

Data Fields

INT16U u16ArgBlockID
 Big endian.
 
INT8U au8Data [32]
 32 bytes.
 

Detailed Description

This structure is used for SPDU input.

The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_SPDUIn = 0x1101.