IO-Link Master1.09.04
IOLM_SMI_SPDInIQ Struct Reference

This structure is used for IQ input. More...

#include <IOLM_SMI_Types.h>

Data Fields

INT16U u16ArgBlockID
 Big endian.
 
INT8U u8IQ
 Input IQ signal.
 

Detailed Description

This structure is used for IQ input.

The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_PDInIQ = 0x1FFE.