IO-Link Master1.09.04
IOLM_SMI_SOnRequestData Struct Reference

This structure is used for On-request Data. More...

#include <IOLM_SMI_Types.h>

Data Fields

INT16U u16ArgBlockID
 Big endian.
 
INT16U u16Index
 Big endian.
 
INT8U u8Subindex
 
INT8U au8Data [(238)]
 

Detailed Description

This structure is used for On-request Data.

The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_OnRequestData = 0x3000.