IO-Link Master1.09.04
IOLM_SMI_SFSPortStatusList Struct Reference

This structure is used to store FS port status. More...

#include <IOLM_SMI_Types.h>

Data Fields

INT16U u16ArgBlockID
 Big endian.
 
INT8U u8PortStatusInfo
 IOLM_SMI_EPortStatus.
 
INT8U u8PortQualityInfo
 
INT8U u8RevisionID
 
INT8U u8TransmissionRate
 
INT8U u8MasterCycleTime
 
INT8U u8InputDataLength
 
INT8U u8OutputDataLength
 
INT16U u16VendorID
 Big endian.
 
INT32U u32DeviceID
 Big endian.
 
INT8U u8NumberOfDiags
 
INT8U au8DiagData [3 *5]
 

Detailed Description

This structure is used to store FS port status.

The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_FSPortStatusList = 0x9100.