IO-Link Master1.09.04
IOLM_SMI_SFSPortConfigList Struct Reference

This structure is used to store FS port configuration. More...

#include <IOLM_SMI_Types.h>

Data Fields

INT16U u16ArgBlockID
 Big endian.
 
INT8U u8PortMode
 
INT8U u8ValidationBackup
 
INT8U u8IQBehavior
 
INT8U u8PortCycleTime
 
INT16U u16VendorID
 Big endian.
 
INT32U u32DeviceID
 Big endian.
 
INT16U u16FSPTime2Ready
 
INT32U u32FSCPAuthenticity1
 
INT32U u32FSCPAuthenticity2
 
INT8U u8FSPPort
 
INT16U u16FSPAuthentCRC
 
INT8U u8FSPProtVersion
 
INT8U u8FSPProtMode
 
INT16U u16FSPWatchdogTime
 
INT16U u16FSPIOStructCRC
 
INT32U u32FSPTechParCRC
 
INT16U u16FSPProtParCRC
 
INT8U u8IODescVersion
 
INT8U u8SPDUInLength
 
INT8U u8TotalOfInBits
 
INT8U u8TotalOfInOctets
 
INT8U u8TotalOfInInt16
 
INT8U u8TotalOfInInt32
 
INT8U u8SPDUOutLength
 
INT8U u8TotalOfOutBits
 
INT8U u8TotalOfOutOctets
 
INT8U u8TotalOfOutInt16
 
INT8U u8TotalOfOutInt32
 

Detailed Description

This structure is used to store FS port configuration.

The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_FSPortConfigList = 0x8100.