void EC_API_SLV_PDO_registerAssignmentChanges | ( | EC_API_SLV_SHandle_t * | pEcSlaveApi_p, |
void * | pContext_p, | ||
EC_API_SLV_PDO_CBAssignmentChanges_t | cbFunc_p | ||
) |
Register callback for PDO assignment changes.
PDO assignment can be modified by the master in PREOP state. Thus, the PDO assignment changes can be reported using this callback. PDO assignments are declared in objects 0x1C12 and 0x1C13.
[in] | pEcSlaveApi_p | The pointer to the EtherCAT API instance. |
[in] | pContext_p | Context for callback. |
[in] | cbFunc_p | Callback. |