AM64x MCU+ SDK  08.06.00
SDFM_GpioParams Struct Reference

Detailed Description

Structure defining SDFM base address and values to toggle GPIO pins.

Used to toggle the gpio based on different threshold conditions

Data Fields

volatile uint32_t write_val
 
volatile uint32_t set_val_addr
 
volatile uint32_t clr_val_addr
 

Field Documentation

◆ write_val

volatile uint32_t SDFM_GpioParams::write_val

◆ set_val_addr

volatile uint32_t SDFM_GpioParams::set_val_addr

◆ clr_val_addr

volatile uint32_t SDFM_GpioParams::clr_val_addr