AM64x MCU+ SDK  08.06.00
SDFM_ChCtrl Struct Reference

Detailed Description

Structure defining SDFM channel control fields.

Used by driver to enable / disable individual SD
channels.

Data Fields

volatile uint32_t sdfm_ch_id
 
volatile uint16_t enable_comparator
 
volatile uint16_t output_data_format
 
volatile uint16_t reserved1
 
volatile uint16_t reserved2
 

Field Documentation

◆ sdfm_ch_id

volatile uint32_t SDFM_ChCtrl::sdfm_ch_id

< stores the channel ids for different selected channel bit-field to enable comparators for individual SDFM channels, BitN:ChN, non-zero to enable

◆ enable_comparator

volatile uint16_t SDFM_ChCtrl::enable_comparator

bit-field to set the output data format for individual SDFM channels, BitN:ChN

◆ output_data_format

volatile uint16_t SDFM_ChCtrl::output_data_format

reserved

◆ reserved1

volatile uint16_t SDFM_ChCtrl::reserved1

reserved

◆ reserved2

volatile uint16_t SDFM_ChCtrl::reserved2