#include <appPerm.h>
Data Fields | |
EI_APP_PERM_SCfgHeader_t | permHdr |
uint32_t | ipAddr |
uint32_t | ipNwMask |
uint32_t | ipGateway |
uint32_t | nameServer1 |
uint32_t | nameServer2 |
char | aDomainName [48] |
uint8_t | configurationMethod |
char | aHostName [64] |
uint8_t | ttlValue |
bool | acdActive |
uint8_t | acdState |
uint8_t | aAcdAddr [6] |
uint8_t | aAcdHdr [28] |
uint16_t | encapInactTimeout |
EI_API_ADP_UIntfConf_t | intfConfig [2] |
bool | ptpEnable |
bool | portEnable |
uint16_t | portLogAnnounceInterval |
int16_t | portLogSyncInterval |
uint8_t | domainNumber |
char | aUserDescription [128] |
EI_API_ADP_SQos_t | qosParameter |
EI_API_ADP_SMcastConfig_t | mcastConfig |
bool | quickConnectEnabled |