EtherNet/IP™ Adapter  2.01.00
EI_API_ADP_SMcastConfig Struct Reference

General multi-cast attribute parameter collection. More...

#include <EI_API_def.h>

Data Fields

uint8_t allocControl
 
uint8_t reserved
 
uint16_t numMcast
 
uint32_t mcastStartAddr
 

Detailed Description

General multi-cast attribute parameter collection.

IP multi-cast address configuration.

Examples
appPerm.c.