uint32_t EC_API_SLV_CoE_getObjectLength | ( | EC_API_SLV_SHandle_t * | pEcSlaveApi_p, |
EC_API_SLV_SCoE_Object_t * | pObject_p, | ||
uint32_t * | length_p | ||
) |
This function returns the object length.
This function returns the object length including subIndex 0 (16 bit).
[in] | pEcSlaveApi_p | The pointer to the EtherCAT API instance. |
[in] | pObject_p | Pointer to the object instance. |
[out] | length_p | Object length. |