uint32_t EC_API_SLV_CoE_getObjectEntryLength | ( | EC_API_SLV_SHandle_t * | pEcSlaveApi_p, |
EC_API_SLV_SCoE_ObjEntry_t * | pObjEntry_p, | ||
uint32_t * | length_p | ||
) |
This function returns the object entry length.
[in] | pEcSlaveApi_p | The pointer to the EtherCAT API instance. |
[in] | pObjEntry_p | Pointer to the object entry instance. |
[out] | length_p | Object entry length. |