This file contains the type definitions and helper macros for the CPSW MAC port module interface.
Go to the source code of this file.
Data Structures | |
struct | CpswMacPort_TxShortIpgCfg |
Configuration of transmit short inter packet gap feature. More... | |
struct | CpswMacPort_PortTxShortIpgCfg |
MAC port's short gap configuration. More... | |
struct | CpswMacPort_InterVlanRoutingCfg |
Port interVLAN configuration parameters. More... | |
struct | CpswMacPort_FifoStats |
FIFO related statistics of a MAC port. More... | |
struct | CpswMacPort_IpTsCfg |
Port IP configuration for time synchronization events. More... | |
struct | CpswMacPort_TsEventCfg |
Port configuration for time synchronization. More... | |
struct | CpswMacPort_EnableTsEventInArgs |
Input args for CPSW_MACPORT_IOCTL_ENABLE_CPTS_EVENT. More... | |
struct | CpswMacPort_EstTimestampCfg |
EST timestamping configuration parameters. More... | |
struct | CpswMacPort_Cfg |
MAC port module configuration parameters. More... | |
Macros | |
#define | CPSW_MACPORT_PUBLIC_IOCTL(x) |
Helper macro to create IOCTL commands for CPSW MAC port module. More... | |
#define | CPSW_MACPORT_EST_TIME_INTERVAL_MIN (0x010U) |
EST non-zero minimum time interval, in wireside clocks. Needed to guarantee that next fetch value has time to be fetched before current fetch count is over. More... | |
#define | CPSW_MACPORT_EST_TIME_INTERVAL_MAX (0x3FFFU) |
EST maximum time interval (14-bit), in wireside clocks. More... | |
#define | CPSW_MACPORT_EST_TIME_STEP_1G (8U) |
Time interval step in nsecs for 1 Gbps link. More... | |
#define | CPSW_MACPORT_EST_TIME_STEP_100M (40U) |
Time interval step in nsecs for 100 Mbps link. More... | |
#define | CPSW_MACPORT_EST_TIME_STEP_10M (400U) |
Time interval step in nsecs for a 10 Mbps link. More... | |
#define | CPSW_MACPORT_EST_TIME_MIN(speed) (CPSW_MACPORT_EST_TIME_STEP_##speed * CPSW_MACPORT_EST_TIME_INTERVAL_MIN) |
Min time interval in nsecs for given link speed. More... | |
#define | CPSW_MACPORT_EST_TIME_MAX(speed) (CPSW_MACPORT_EST_TIME_STEP_##speed * CPSW_MACPORT_EST_TIME_INTERVAL_MAX) |
Max time interval in nsecs for given link speed. More... | |
#define | CPSW_MACPORT_EST_ALLOWCNT_FACTOR_1G (1U) |
EST allow count scaling factor for 1 Gbps link. More... | |
#define | CPSW_MACPORT_EST_ALLOWCNT_FACTOR_100M (2U) |
EST allow count scaling factor for 100 Mbps link. More... | |
#define | CPSW_MACPORT_EST_ALLOWCNT_FACTOR_10M (2U) |
EST allow count scaling factor for 10 Mbps link. More... | |
#define | CPSW_MACPORT_EST_GUARD_BAND(maxPktSize, speed) |
Guard band duration in nsecs for given link speed and maximum packet size in previous time interval. More... | |
Functions | |
void | CpswMacPort_initCfg (CpswMacPort_Cfg *macPortCfg) |
Initialize CPSW MAC port configuration parameters. More... | |