AM64x MCU+ SDK  08.04.00
CpswMacPort_EstTimestampCfg Struct Reference

Detailed Description

EST timestamping configuration parameters.

Data Fields

Enet_MacPort macPort
 
CpswMacPort_EstTimestampMode mode
 
uint8_t priority
 
uint8_t domain
 

Field Documentation

◆ macPort

Enet_MacPort CpswMacPort_EstTimestampCfg::macPort

Port number.

◆ mode

CpswMacPort_EstTimestampMode CpswMacPort_EstTimestampCfg::mode

Timestamping mode. Determines what packets are timestamped.

◆ priority

uint8_t CpswMacPort_EstTimestampCfg::priority

Priority that timestamps will be generated on. Applicable for CPSW_MACPORT_EST_TIMESTAMP_ONEPRI and CPSW_MACPORT_EST_TIMESTAMP_FIRST_ONEPRI.

◆ domain

uint8_t CpswMacPort_EstTimestampCfg::domain

CPTS EST timestamp domain. It can be used to indicate and identify that an event came from EST.