EtherNet/IP™ Adapter  1.04.10
User Reference Manual

◆ EI_API_ADP_setTimeSyncRevisionData()

uint32_t EI_API_ADP_setTimeSyncRevisionData ( T pAdp_p,
const char *  pRevisionData_p 
)

Set the RevisionData attribute of the Time Sync object of the adapter(Instance Attribute ID: 22).

RevisionData specifies the revision data of the device that contains the clock. The format is:

  • The hardware revision of the clock followed by a semicolon.
  • The firmware revision of the clock followed by a semicolon.
  • The software revision of the clock.

For example: 1.2;2.3;3.0.1 The format is UTF-8 Unicode. The maximum number of symbols is 32. Subfields that don't apply may be null or blank (e.g. 1.2;2.3; or ;;3.4).

Remarks
The maximum length of the revision data is set to 32. If parameter pRevisionData_p exceeds 32 characters An error EI_API_ADP_eERR_LENGTH is returned. The format must be like the format described in

. Otherwise it is returned EI_API_ADP_eERR_TIMESYNC_WRONG_FORMAT.

Parameters
[in]pAdp_pPointer to the adapter.
[in]pRevisionData_pNew product name as NULL (\0) terminated cstring.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
EI_API_ADP_eERR_LENGTHIllegal parameter length.
EI_API_ADP_eERR_TIMESYNC_WRONG_FORMATUnaccepted format. E.g. format "1.2;2.3;"
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
char revisionData[] = "1.2;2.3;";
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_setTimeSyncRevisionData(pEI_API_ADP, revisionData);
See also
EI_API_ADP_getTimeSyncRevisionData EI_API_ADP_EError_t
EI_API_ADP_setTimeSyncRevisionData
ETHIP_API uint32_t EI_API_ADP_setTimeSyncRevisionData(T *pAdp_p, const char *pRevisionData_p)
Set the RevisionData attribute of the Time Sync object of the adapter(Instance Attribute ID: 22).
Definition: EI_API_ADP_main.c:3008
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:285