EtherNet/IP™ Adapter  1.04.10
User Reference Manual

◆ EI_API_ADP_getTimeSyncRevisionData()

uint32_t EI_API_ADP_getTimeSyncRevisionData ( T pAdp_p,
char *  pRevisionData_p 
)

Get the Revision member of the RevisionData attribute of the Time Sync object (Instance Attribute ID: 22).

Function that returns the Revision member of the RevisionData attribute for the adapter selected by parameter pAdp_p in output parameter pRevisionData_p.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pRevisionData_pchar pointer to RevisionData of the adapter Time Sync object specified by parameter pAdp_p.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
char revisionData[32];
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getTimeSyncRevisionData(pEI_API_ADP, revisionData);
See also
EI_API_ADP_setTimeSyncRevisionData EI_API_ADP_EError_t
EI_API_ADP_getTimeSyncRevisionData
ETHIP_API uint32_t EI_API_ADP_getTimeSyncRevisionData(T *pAdp_p, char *pRevisionData_p)
Get the Revision member of the RevisionData attribute of the Time Sync object (Instance Attribute ID:...
Definition: EI_API_ADP_main.c:2928
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:285