AM64x MCU+ SDK  08.03.00

Introduction

The CPSW statistics module implements only the IOCTLs defined in the generic Enet Statistics API. There are no additional CPSW-specific IOCTLs.

The CPSW host port module provides additional IOCTL commands than those supported by the generci Enet Host Port API set.

CPSW host port clocks:

Compile-time configuration:

Data Structures

struct  CpswHostPort_FifoStats
 FIFO related statistics of the host port. More...
 
struct  CpswHostPort_Cfg
 Host port module configuration parameters. More...
 

Functions

void CpswHostPort_initCfg (CpswHostPort_Cfg *hostPortCfg)
 Initialize CPSW host port configuration parameters. More...
 

Enumerations

enum  CpswHostPort_Ioctl { CPSW_HOSTPORT_IOCTL_GET_FIFO_STATS = CPSW_HOSTPORT_PUBLIC_IOCTL(0U), CPSW_HOSTPORT_GET_FLOW_ID_OFFSET = CPSW_HOSTPORT_PUBLIC_IOCTL(1U) }
 CPSW MAC port IOCTL commands. More...
 

Macros

#define CPSW_HOSTPORT_PUBLIC_IOCTL(x)
 Helper macro to create IOCTL commands for CPSW host port module. More...
 

Macro Definition Documentation

◆ CPSW_HOSTPORT_PUBLIC_IOCTL

#define CPSW_HOSTPORT_PUBLIC_IOCTL (   x)
Value:
ENET_IOCTL_HOSTPORT_BASE | \
ENET_IOCTL_PER_CPSW | \
ENET_IOCTL_MIN(x))

Helper macro to create IOCTL commands for CPSW host port module.

Enumeration Type Documentation

◆ CpswHostPort_Ioctl

CPSW MAC port IOCTL commands.

Enumerator
CPSW_HOSTPORT_IOCTL_GET_FIFO_STATS 

Get host port's FIFO statistics.

IOCTL parameters:

CPSW_HOSTPORT_GET_FLOW_ID_OFFSET 

Get host port flow Id offset.

IOCTL parameters:

  • inArgs: None
  • outArgs: uint32_t

Function Documentation

◆ CpswHostPort_initCfg()

void CpswHostPort_initCfg ( CpswHostPort_Cfg hostPortCfg)

Initialize CPSW host port configuration parameters.

Parameters
hostPortCfgConfiguration parameters to be initialized
ENET_IOCTL_TYPE_PUBLIC
@ ENET_IOCTL_TYPE_PUBLIC
Definition: enet_ioctl.h:167