#include <PN_API_SNMP.h>
Data Fields | |
uint16_t | sysContactLength |
uint8_t | aSysContact [PN_API_SNMP_MAX_SNMP_SYSTEM_VALUE_BUFFER] |
uint16_t | sysNameLength |
uint8_t | aSysName [PN_API_SNMP_MAX_SNMP_SYSTEM_VALUE_BUFFER] |
uint16_t | sysLocationLength |
uint8_t | aSysLocation [PN_API_SNMP_MAX_SNMP_SYSTEM_VALUE_BUFFER] |
uint16_t | lldpMessageTxInterval |
uint8_t | lldpMessageTxHoldMultiplier |
uint8_t | lldpReinitDelay |
uint16_t | lldpTxDelay |
uint16_t | lldpNotificationInterval |
PN_API_SNMP_SPort_t | port1 |
PN_API_SNMP_SPort_t | port2 |
uint8_t | lldpConfigManAddrPortsTxEnable |