EtherNet/IP™ Adapter  1.04.01
User Reference Manual

◆ EI_API_ADP_getDomainNumber()

uint32_t EI_API_ADP_getDomainNumber ( T pAdp_p,
uint8_t *  pDomainNumber_p 
)

Get the DomainNumber attribute of the Time Sync Object (Instance Attribute ID: 18).

Function that returns the DomainNumber attribute in the Time Sync object of the EtherNet/IP adapter selected by parameter pAdp_p in output parameter pDomainNumber_p.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pDomainNumber_puint8_t pointer to DomainNumber attribute.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint8_t domainNumber;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getDomainNumber(pEI_API_ADP, &domainNumber);
See also
EI_API_ADP_setDomainNumber EI_API_ADP_EError_t
EI_API_ADP_getDomainNumber
ETHIP_API uint32_t EI_API_ADP_getDomainNumber(T *pAdp_p, uint8_t *pDomainNumber_p)
Get the DomainNumber attribute of the Time Sync Object (Instance Attribute ID: 18).
Definition: EI_API_ADP_main.c:2363
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:234