The Time Sync Object provides a CIP interface to the IEEE 1588 (IEC 61588) Standard for a Precision Clock Synchronization Protocol for Networked Measurement and Control Systems, commonly referred to as the Precision Time Protocol (PTP). Refer to the IEEE 1588 (IEC 61588) Standard for additional details.
Any device supporting CIP Sync shall provide a single instance (Instance 1) of the Time Sync Object.
| Attribute ID | Access Rule | NV | Name | Data Type | Value | Description |
|---|---|---|---|---|---|---|
| 1 | Get ¹, Set | NV | PTPEnable | BOOL | 0 | PTPEnable specifies the enable status for the Precision Time Protocol on the device.
|
| 13 | PortEnableCfg | STRUCT of | PTP port enable config | |||
| NumberOfPorts | UINT | Number of PTP ports | ||||
| ARRAY of STRUCT | ||||||
| PortNumber | UINT | PTP port number | ||||
| Get ¹, Set | NV | PortEnable | UINT | PTP port enable | ||
| 14 | PortLogAnnounceIntervalCfg | STRUCT of | PTP port log announce interval config | |||
| NumberOfPorts | UINT | Number of PTP ports | ||||
| ARRAY of STRUCT | PTP port log announce interval of each port | |||||
| PortNumber | UINT | PTP port number | ||||
| Get ¹, Set | NV | PortLogAnnounceInterval | UINT | PTP port log announce interval | ||
| 15 | PortLogSyncIntervalCfg | STRUCT of | PTP port log sync interval config | |||
| NumberOfPorts | UINT | Number of PTP ports | ||||
| ARRAY of STRUCT | ||||||
| PortNumber | UINT | PTP port number | ||||
| Get ¹, Set | NV | PortLogSyncInterval | INT | PTP port log sync interval | ||
| 18 | Get ¹, Set | NV | DomainNumber | USINT | Domain number | |
| 19 | Get | V | ClockType | WORD | 0x0190, End-to-End Transparent Clock, Ordinary Clock, Slave Only | Clock type |
| 20 | Get, Set ² | V | ManufactureIdentity | USINT[4] (implemented as char*) | Manufacture identity | |
| 21 | ProductDescription | STRUCT of | Product description | |||
| Size | UDINT | Size of product description | ||||
| Get, Set ² | V | Description | ARRAY of USINT | Description | ||
| 22 | RevisionData | STRUCT of | Revision data | |||
| Size | UDINT | Size of revision data | ||||
| Get, Set ² | V | Revision | ARRAY of USINT | Revision | ||
| 23 | UserDescription | STRUCT of | User description | |||
| Size | UDINT | Size of user description | ||||
| Get, Set ² | V | Description | ARRAY of USINT | Description |
Table Footnotes:
¹ Get access only with application's Get function
² Set access only with application's Set function
Functions | |
| uint32_t | EI_API_ADP_setTimeSyncSupported (T *pAdp_p) |
| Enable Time Sync Object support. More... | |
| uint32_t | EI_API_ADP_getPtpEnable (T *pAdp_p, bool *pPtpEnable_p) |
| Get the PTPEnable attribute of the Time Sync Object (Instance Attribute ID: 1). More... | |
| uint32_t | EI_API_ADP_setPtpEnable (T *pAdp_p, bool ptpEnable_p) |
| Enable or disable PTP functionality in the Time Sync Object of the current adapter (Instance Attribute ID: 1). More... | |
| uint32_t | EI_API_ADP_getPortEnable (T *pAdp_p, bool *pPortEnable_p) |
| Get the PortEnable attribute state of the Time Sync Object (Instance Attribute ID: 13). More... | |
| uint32_t | EI_API_ADP_setPortEnable (T *pAdp_p, bool portEnable_p) |
| Set the port state of the Time Sync Object of the current adapter enable or disable (Instance Attribute ID: 13). More... | |
| uint32_t | EI_API_ADP_getPortLogAnnounceInterval (T *pAdp_p, uint16_t *pPortLogAnnounceInterval_p) |
| Get the PortLogAnnounceInterval attribute of the Time Sync Object (Instance Attribute ID: 14). More... | |
| uint32_t | EI_API_ADP_setPortLogAnnounceInterval (T *pAdp_p, uint16_t portLogAnnounceInterval_p) |
| Set the PortLogAnnounceInterval of the Time Sync object of the adapter (Instance Attribute ID: 14). More... | |
| uint32_t | EI_API_ADP_getPortLogSyncInterval (T *pAdp_p, int16_t *pPortLogSyncInterval_p) |
| Get the PortLogSyncInterval member value of attribute PortLogSyncIntervalCfg of the Time Sync object (Instance Attribute ID: 15). More... | |
| uint32_t | EI_API_ADP_setPortLogSyncInterval (T *pAdp_p, uint16_t portLogSyncInterval_p) |
| Set the PortLogSyncInterval in attribute of the Time Sync object of the adapter (Instance Attribute ID: 15). More... | |
| uint32_t | EI_API_ADP_getDomainNumber (T *pAdp_p, uint8_t *pDomainNumber_p) |
| Get the DomainNumber attribute of the Time Sync Object (Instance Attribute ID: 18). More... | |
| uint32_t | EI_API_ADP_setDomainNumber (T *pAdp_p, uint8_t domainNumber_p) |
| Set the DomainNumber attribute of the Time Sync object of the adapter (Instance Attribute ID: 18). More... | |
| uint32_t | EI_API_ADP_getTimeSyncManufactureID (T *pAdp_p, char *pManufactureID_p) |
| Get the ManufactureIdentity attribute of the Time Sync Object (Instance Attribute ID: 20). More... | |
| uint32_t | EI_API_ADP_setTimeSyncManufactureID (T *pAdp_p, const char *pManufactureID_p) |
| Set the ManufactureIdentity attribute of the Time Sync object of the adapter (Instance Attribute ID: 20). More... | |
| uint32_t | EI_API_ADP_getTimeSyncProductDescription (T *pAdp_p, char *pProductDesc_p) |
| Get the Description member of the ProductDescription attribute of the Time Sync Object (Instance Attribute ID: 21). More... | |
| uint32_t | EI_API_ADP_setTimeSyncProductDescription (T *pAdp_p, const char *pProductDesc_p) |
| Set the Description member of the ProductDescription attribute of the Time Sync object of the adapter (Instance Attribute ID: 21). More... | |
| uint32_t | EI_API_ADP_getTimeSyncRevisionData (T *pAdp_p, char *pRevisionData_p) |
| Get the Revision member of the RevisionData attribute of the Time Sync object (Instance Attribute ID: 22). More... | |
| uint32_t | EI_API_ADP_setTimeSyncRevisionData (T *pAdp_p, const char *pRevisionData_p) |
| Set the RevisionData attribute of the Time Sync object of the adapter(Instance Attribute ID: 22). More... | |
| uint32_t | EI_API_ADP_getTimeSyncUserDescription (T *pAdp_p, char *pUserDescription_p) |
| Get the Description member of the UserDescription attribute of the Time Sync object (Instance Attribute ID: 23). More... | |
| uint32_t | EI_API_ADP_setTimeSyncUserDescription (T *pAdp_p, const char *pUserDescription_p) |
| Set the Description member of UserDescription attribute of the Time Sync object of the adapter (Instance Attribute ID: 23). More... | |