EtherNet/IP™ Adapter  1.04.01
User Reference Manual

◆ EI_API_ADP_setPortEnable()

uint32_t EI_API_ADP_setPortEnable ( T pAdp_p,
bool  portEnable_p 
)

Set the port state of the Time Sync Object of the current adapter enable or disable (Instance Attribute ID: 13).

Function that sets the PortEnable state in the PortEnableCfg attribute for the EtherNet/IP adapter selected by parameter pAdp_p in output parameter pPortEnable.

Parameters
[in]pAdp_pPointer to the adapter.
[in]portEnable_pTime Sync's network port state.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// Set network port state enable in Time Sync object
errCode = EI_API_ADP_setPortEnable(pEI_API_ADP, true);
See also
EI_API_ADP_getPortEnable EI_API_ADP_EError_t
EI_API_ADP_setPortEnable
ETHIP_API uint32_t EI_API_ADP_setPortEnable(T *pAdp_p, bool portEnable_p)
Set the port state of the Time Sync Object of the current adapter enable or disable (Instance Attribu...
Definition: EI_API_ADP_main.c:2025
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:234