This file contains the type definitions and helper macros for the Ethernet PHY interface.
Go to the source code of this file.
Data Structures | |
struct | EnetPhy_Version |
PHY version (ID). More... | |
struct | EnetPhy_LinkCfg |
Link speed and duplexity configuration. More... | |
struct | EnetPhy_FsmTimeoutCfg |
PHY State-Machine time-out values. More... | |
struct | EnetPhy_Cfg |
PHY configuration parameters. More... | |
struct | EnetPhy_Mdio |
MDIO driver. More... | |
struct | EnetPhy_State |
PHY driver FSM state. More... | |
struct | EnetPhy_Obj |
PHY driver object. More... | |
Macros | |
#define | ENETPHY_IS_ADDR_VALID(addr) ((addr) <= 31U) |
Check if PHY address is valid (0 - 31). More... | |
#define | ENETPHY_BIT(n) (1U << (n)) |
Macro to set bit at given bit position. More... | |
#define | ENETPHY_IS_BIT_SET(val, n) (((val) & ENETPHY_BIT(n)) != 0U) |
Macro to check if bit at given bit position is set. More... | |
#define | ENETPHY_ARRAYSIZE(x) (sizeof(x) / sizeof(x[0])) |
Macro to get the size of an array. More... | |
#define | ENETPHY_EXTENDED_CFG_SIZE_MAX (128U) |
Max extended configuration size, arbitrarily chosen. More... | |
#define | ENETPHY_FSM_TICK_PERIOD_MS (100U) |
Enet PHY State Machine tick period. More... | |
#define | ENETPHY_INVALID_PHYADDR (~0U) |
Invalid PHY address indicator. More... | |
Ethernet PHY driver error codes | |
#define | ENETPHY_SOK (CSL_PASS) |
Success. More... | |
#define | ENETPHY_EFAIL (CSL_EFAIL) |
Generic failure error condition (typically caused by hardware). More... | |
#define | ENETPHY_EBADARGS (CSL_EBADARGS) |
Bad arguments (i.e. NULL pointer). More... | |
#define | ENETPHY_EINVALIDPARAMS (CSL_EINVALID_PARAMS) |
Invalid parameters (i.e. value out-of-range). More... | |
#define | ENETPHY_ETIMEOUT (CSL_ETIMEOUT) |
Time out while waiting for a given condition to happen. More... | |
#define | ENETPHY_EALLOC (CSL_EALLOC) |
Allocation failure. More... | |
#define | ENETPHY_EPERM (CSL_EALLOC - 4) |
Operation not permitted. More... | |
#define | ENETPHY_ENOTSUPPORTED (CSL_EALLOC - 5) |
Operation not supported. More... | |
Ethernet PHY link capability masks | |
#define | ENETPHY_LINK_CAP_HD10 ENETPHY_BIT(1) |
10-Mbps, half-duplex capability mask. More... | |
#define | ENETPHY_LINK_CAP_FD10 ENETPHY_BIT(2) |
10-Mbps, full-duplex capability mask. More... | |
#define | ENETPHY_LINK_CAP_HD100 ENETPHY_BIT(3) |
100-Mbps, half-duplex capability mask. More... | |
#define | ENETPHY_LINK_CAP_FD100 ENETPHY_BIT(4) |
100-Mbps, full-duplex capability mask. More... | |
#define | ENETPHY_LINK_CAP_HD1000 ENETPHY_BIT(5) |
1-Gbps, half-duplex capability mask. More... | |
#define | ENETPHY_LINK_CAP_FD1000 ENETPHY_BIT(6) |
1-Gbps, full-duplex capability mask. More... | |
#define | ENETPHY_LINK_CAP_10 |
10-Mbps, full and half-duplex capability mask. More... | |
#define | ENETPHY_LINK_CAP_100 |
100-Mbps, full and half-duplex capability mask. More... | |
#define | ENETPHY_LINK_CAP_1000 |
1-Gbps, full and half-duplex capability mask. More... | |
#define | ENETPHY_LINK_CAP_ALL |
Auto-negotiation mask with all duplexity and speed values set. More... | |
Typedefs | |
typedef EnetPhy_Mdio * | EnetPhy_MdioHandle |
MDIO driver handle. More... | |
typedef struct EnetPhy_Drv_s * | EnetPhyDrv_Handle |
PHY specific driver handle. More... | |
typedef struct EnetPhy_Obj_s * | EnetPhy_Handle |
PHY driver object handle. More... | |
Functions | |
void | EnetPhy_initCfg (EnetPhy_Cfg *phyCfg) |
Initialize PHY config params. More... | |
void | EnetPhy_setExtendedCfg (EnetPhy_Cfg *phyCfg, const void *extendedCfg, uint32_t extendedCfgSize) |
Set PHY extended parameters. More... | |
EnetPhy_Handle | EnetPhy_open (const EnetPhy_Cfg *phyCfg, EnetPhy_Mii mii, const EnetPhy_LinkCfg *linkCfg, uint32_t macPortCaps, EnetPhy_MdioHandle hMdio, void *mdioArgs) |
Open the PHY driver. More... | |
void | EnetPhy_close (EnetPhy_Handle hPhy) |
Close the PHY driver. More... | |
EnetPhy_LinkStatus | EnetPhy_tick (EnetPhy_Handle hPhy) |
Run PHY state machine. More... | |
int32_t | EnetPhy_getId (EnetPhy_Handle hPhy, EnetPhy_Version *version) |
Get PHY id. More... | |
bool | EnetPhy_isAlive (EnetPhy_Handle hPhy) |
Get PHY alive status. More... | |
bool | EnetPhy_isLinked (EnetPhy_Handle hPhy) |
Get link status. More... | |
int32_t | EnetPhy_getLinkCfg (EnetPhy_Handle hPhy, EnetPhy_LinkCfg *linkCfg) |
Get link configuration. More... | |
int32_t | EnetPhy_readReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t *val) |
Read PHY register. More... | |
int32_t | EnetPhy_writeReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t val) |
Write PHY register. More... | |
int32_t | EnetPhy_rmwReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t mask, uint16_t val) |
Read-modify-write PHY register. More... | |
int32_t | EnetPhy_readExtReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t *val) |
Read PHY extended register. More... | |
int32_t | EnetPhy_writeExtReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t val) |
Write PHY extended register. More... | |
int32_t | EnetPhy_rmwExtReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t mask, uint16_t val) |
Read-modify-write PHY extended register. More... | |
int32_t | EnetPhy_readC45Reg (EnetPhy_Handle hPhy, uint8_t mmd, uint32_t reg, uint16_t *val) |
Read PHY register using Clause-45 frame. More... | |
int32_t | EnetPhy_writeC45Reg (EnetPhy_Handle hPhy, uint8_t mmd, uint32_t reg, uint16_t val) |
Write PHY register using Clause-45 frame. More... | |
int32_t | EnetPhy_rmwC45Reg (EnetPhy_Handle hPhy, uint8_t mmd, uint32_t reg, uint16_t mask, uint16_t val) |
Read-modify-write PHY register using Clause-45 frame. More... | |
void | EnetPhy_printRegs (EnetPhy_Handle hPhy) |
Print all PHY registers. More... | |