uint32_t EI_API_ADP_setQuickConnectSupported | ( | T * | pAdp_p | ) |
Enable QuickConnect Support.
Enable QuickConnect Support. This function should only be used for EtherNet_IP Quick Connect applications.
Description | |
---|---|
0 | Disable |
1 | Enable |
[in] | pAdp_p | Pointer to the adapter. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |