uint32_t EI_API_ADP_getQuickConnectEnabled | ( | T * | pAdp_p, |
uint8_t * | pQuickConnectEnabled_p | ||
) |
Get the current adapter QuickConnect state (Instance Attribute ID: 12).
Function that returns the adapter QuickConnect state.
[in] | pAdp_p | Pointer to the adapter. |
[out] | pQuickConnectEnabled_p | Pointer of type uint8_t to the adapter QuickConnect state. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |