EtherNet/IP™ Adapter  1.02.01
User Reference Manual

◆ EI_API_CIP_createAssembly()

uint32_t EI_API_CIP_createAssembly ( T *  pCipNode_p,
uint16_t  assemblyInstanceId_p,
EI_API_CIP_EAr_t  accessRule_p 
)

Create a new assembly instance.

This function creates a new assembly instance with the given ID.

Parameters
[in]pCipNode_pPointer to the CIP node.
[in]assemblyInstanceId_pInstance identifier.
[in]accessRule_pParameter to define assembly access rule.
Returns
EI_API_CIP_EError_t as uint32_t value.
Return values
EI_API_CIP_eERR_OKSuccess.
EI_API_CIP_eERR_NODE_INVALIDCIP node is invalid, possibly EI_API_CIP_NODE_new() was not called.
EI_API_CIP_eERR_ASSEMBLY_ALREADY_EXISTSThe assembly with the given ID already exists.
EI_API_CIP_eERR_MEMALLOCMemory allocation error.
EI_API_CIP_eERR_GENERALGeneral CIP error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
EI_API_CIP_NODE_T* pEI_API_CIP_NODE = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint16_t assemblyInstanceId;
// Create a new adapter first
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// Create a CIP node next
pEI_API_CIP_NODE = EI_API_CIP_NODE_new();
...
// Under pEI_API_CIP_NODE, create assembly instance with ID = 100, with read-write access
assemblyInstanceId = 0x64;
errCode = EI_API_CIP_createAssembly(pEI_API_CIP_NODE, assemblyInstanceId, EI_API_CIP_eAR_GET_AND_SET);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:195
ETHIP_API uint32_t EI_API_CIP_createAssembly(T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_EAr_t accessRule_p)
Create a new assembly instance.
Definition: EI_API_CIP_main.c:5329
@ EI_API_CIP_eAR_GET_AND_SET
Definition: EI_API_def.h:131
ETHIP_API T * EI_API_CIP_NODE_new(void)
Create a new CIP node.
Definition: EI_API_CIP_main.c:69
See also
EI_API_CIP_addAssemblyMember EI_API_CIP_getAssemblySize EI_API_CIP_getAssemblyData EI_API_CIP_setAssemblyData EI_API_CIP_EAr_t EI_API_CIP_EError_t