EtherNet/IP™ Adapter  1.02.01
User Reference Manual

Overview

Functions

uint32_t EI_API_CIP_createAssembly (T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_EAr_t accessRule_p)
 Create a new assembly instance. More...
 
uint32_t EI_API_CIP_addAssemblyMember (T *pCipNode_p, uint16_t assemblyInstanceId_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attributeId_p)
 Add an member to an assembly member list. More...
 
uint32_t EI_API_CIP_getAssemblySize (T *pCipNode_p, uint16_t assemblyInstanceId_p, uint16_t *pSize_p)
 Get assembly instance attribute Size. More...
 
uint32_t EI_API_CIP_getAssemblyData (T *pCipNode_p, uint16_t assemblyInstanceId_p, void *pDestinationBuffer_p, uint16_t destinationBufferLength_p)
 Get assembly instance attribute data. More...
 
uint32_t EI_API_CIP_setAssemblyData (T *pCipNode_p, uint16_t assemblyInstanceId_p, void *pSourceBuffer_p, uint16_t sourceBufferLength_p)
 Set assembly instance attribute data. More...