Functions | |
void | EIP_DLR_init (EIP_DLRHandle dlrHandle) |
API to initialize the DLR driver. More... | |
void | EIP_DLR_start (EIP_DLRHandle dlrHandle) |
API to start the DLR driver Calling this enables DLR on the device. More... | |
void | EIP_DLR_stop (EIP_DLRHandle dlrHandle) |
API to stop the DLR driver Halt DLR. Calling this disables DLR on the device. More... | |
void | EIP_DLR_port0ISR (uintptr_t arg) |
Fast ISR for Port 0, bypasses the buffer copy and NDK. More... | |
void | EIP_DLR_port1ISR (uintptr_t arg) |
Fast ISR for Port 1, bypasses the buffer copy and NDK. More... | |
void | EIP_DLR_beaconTimeoutISR_P0 (uintptr_t arg) |
ISR for beacon timeout for Port 0. More... | |
void | EIP_DLR_beaconTimeoutISR_P1 (uintptr_t arg) |
ISR for beacon timeout for Port 1. More... | |
void | EIP_DLR_port0ProcessLinkBrk (uint8_t linkStatus, void *arg2) |
Process DLR state machine in the event of a link break on Port0. More... | |
void | EIP_DLR_port1ProcessLinkBrk (uint8_t linkStatus, void *arg2) |
Process DLR state machine in the event of a link break on Port1. More... | |
void | EIP_DLR_neighborTimeoutISR0 (ClockP_Object *obj, void *arg) |
ISR for Neighbor timeout timer for port 0. More... | |
void | EIP_DLR_neighborTimeoutISR1 (ClockP_Object *obj, void *arg) |
ISR for Neighbor timeout timer for port 1. More... | |
void | EIP_DLR_addVlanID (uint8_t *src, uint16_t vlanID) |
void | EIP_DLR_genNCReqFrame (EIP_DLRHandle dlrHandle, uint8_t *src, uint8_t sourcePort) |
void | EIP_DLR_genNCResFrame (uint8_t *src, uint8_t sourcePort, uint8_t reqSrcPort, uint32_t sequenceId) |
void | EIP_DLR_genNeighborLinkStatFrame (EIP_DLRHandle dlrHandle, uint8_t *src, uint8_t sourcePort, uint8_t linkOrNeighbor, uint8_t linkStatus) |
void | EIP_DLR_initDLRFrameHeader (uint8_t *src, uint8_t *header) |
void | EIP_DLR_addSignOnNumNodes (uint8_t *src, uint16_t numNodes) |
void | EIP_DLR_processDLRFrame (EIP_DLRHandle dlrHandle, uint8_t *pktBuffer, uint8_t portNum, uint16_t size) |
Processes a sign on and Neighbor check request frame. More... | |
void | EIP_DLR_dRAMInit (EIP_DLRHandle dlrHandle) |
void | EIP_DLR_resetStateMachine (EIP_DLRHandle dlrHandle) |
Initialize the state machine when it goes back to idle state. More... | |
void | EIP_DLR_setDefaultValue (EIP_DLRHandle dlrHandle) |
void | EIP_DLR_switchToFault (EIP_DLRHandle dlrHandle) |
void | EIP_DLR_switchToNormal (EIP_DLRHandle dlrHandle) |
int32_t | EIP_DLR_isrInit (EIP_DLRHandle dlrHandle) |
void | EIP_DLR_periodicProcessing (ClockP_Object *obj, void *userArg) |
void | EIP_DLR_addToExceptionList (EIP_DLRHandle dlrHandle, uint8_t *macId) |
void | EIP_DLR_clearExceptionList (EIP_DLRHandle dlrHandle) |
uint8_t | EIP_DLR_checkSupervisorException (uint8_t *macId, EIP_DLRHandle dlrHandle) |
void | EIP_DLR_addModuleIPAddress (EIP_DLRHandle dlrHandle, uint32_t newIP) |
void | EIP_DLR_setDivider_WD_IEP (EIP_DLRHandle dlrHandle) |
Sets the clock divider to 1us for IEP watch dog timers. More... | |
void | EIP_DLR_enable_WD_IEP (EIP_DLRHandle dlrHandle, uint8_t id) |
Enable the IEP Watch dog timers. More... | |
void | EIP_DLR_disable_WD_IEP (EIP_DLRHandle dlrHandle, uint8_t id) |
Disable the IEP Watch dog timers. More... | |
void | EIP_DLR_setTimeout_WD_IEP (EIP_DLRHandle dlrHandle, uint16_t periodInMicroSec, uint8_t id) |
Set the timeout value in watchdog. More... | |
void | EIP_DLR_set_pdi_wd_trigger_mode (EIP_DLRHandle dlrHandle, uint32_t mode) |
Set the PDI WD trigger mode. More... | |
void EIP_DLR_init | ( | EIP_DLRHandle | dlrHandle | ) |
API to initialize the DLR driver.
Initializes variables and timers & clocks, call once at the beginning
dlrHandle | [in] DLR driver handle |
void EIP_DLR_start | ( | EIP_DLRHandle | dlrHandle | ) |
API to start the DLR driver Calling this enables DLR on the device.
dlrHandle | [in] DLR driver handle |
void EIP_DLR_stop | ( | EIP_DLRHandle | dlrHandle | ) |
API to stop the DLR driver Halt DLR. Calling this disables DLR on the device.
dlrHandle | [in] DLR driver handle |
void EIP_DLR_port0ISR | ( | uintptr_t | arg | ) |
Fast ISR for Port 0, bypasses the buffer copy and NDK.
arg | [in] user argument. DLR handle |
void EIP_DLR_port1ISR | ( | uintptr_t | arg | ) |
Fast ISR for Port 1, bypasses the buffer copy and NDK.
arg | [in] user argument. DLR handle |
void EIP_DLR_beaconTimeoutISR_P0 | ( | uintptr_t | arg | ) |
ISR for beacon timeout for Port 0.
arg | [in] user argument. DLR handle |
void EIP_DLR_beaconTimeoutISR_P1 | ( | uintptr_t | arg | ) |
ISR for beacon timeout for Port 1.
arg | [in] user argument. DLR handle |
void EIP_DLR_port0ProcessLinkBrk | ( | uint8_t | linkStatus, |
void * | arg2 | ||
) |
Process DLR state machine in the event of a link break on Port0.
linkStatus | [in] link status of the port. Up/Down. 1/0 |
arg2 | [in] argument DLR handle |
void EIP_DLR_port1ProcessLinkBrk | ( | uint8_t | linkStatus, |
void * | arg2 | ||
) |
Process DLR state machine in the event of a link break on Port1.
linkStatus | [in] link status of the port. Up/Down. 1/0 |
arg2 | [in] argument DLR handle |
void EIP_DLR_neighborTimeoutISR0 | ( | ClockP_Object * | obj, |
void * | arg | ||
) |
ISR for Neighbor timeout timer for port 0.
obj | [in] Clock object associated with this callback |
arg | [in] user argument. DLR handle |
void EIP_DLR_neighborTimeoutISR1 | ( | ClockP_Object * | obj, |
void * | arg | ||
) |
ISR for Neighbor timeout timer for port 1.
obj | [in] Clock object associated with this callback |
arg | [in] user argument. DLR handle |
void EIP_DLR_addVlanID | ( | uint8_t * | src, |
uint16_t | vlanID | ||
) |
void EIP_DLR_genNCReqFrame | ( | EIP_DLRHandle | dlrHandle, |
uint8_t * | src, | ||
uint8_t | sourcePort | ||
) |
void EIP_DLR_genNCResFrame | ( | uint8_t * | src, |
uint8_t | sourcePort, | ||
uint8_t | reqSrcPort, | ||
uint32_t | sequenceId | ||
) |
void EIP_DLR_genNeighborLinkStatFrame | ( | EIP_DLRHandle | dlrHandle, |
uint8_t * | src, | ||
uint8_t | sourcePort, | ||
uint8_t | linkOrNeighbor, | ||
uint8_t | linkStatus | ||
) |
void EIP_DLR_initDLRFrameHeader | ( | uint8_t * | src, |
uint8_t * | header | ||
) |
void EIP_DLR_addSignOnNumNodes | ( | uint8_t * | src, |
uint16_t | numNodes | ||
) |
void EIP_DLR_processDLRFrame | ( | EIP_DLRHandle | dlrHandle, |
uint8_t * | pktBuffer, | ||
uint8_t | portNum, | ||
uint16_t | size | ||
) |
Processes a sign on and Neighbor check request frame.
dlrHandle | [in] DLR handle |
pktBuffer | [in] pointer to bytestream |
portNum | [in] Port number wherer the packet arrived |
size | [in] size of packet |
void EIP_DLR_dRAMInit | ( | EIP_DLRHandle | dlrHandle | ) |
void EIP_DLR_resetStateMachine | ( | EIP_DLRHandle | dlrHandle | ) |
Initialize the state machine when it goes back to idle state.
dlrHandle | [in] DLR handle |
void EIP_DLR_setDefaultValue | ( | EIP_DLRHandle | dlrHandle | ) |
void EIP_DLR_switchToFault | ( | EIP_DLRHandle | dlrHandle | ) |
void EIP_DLR_switchToNormal | ( | EIP_DLRHandle | dlrHandle | ) |
int32_t EIP_DLR_isrInit | ( | EIP_DLRHandle | dlrHandle | ) |
void EIP_DLR_periodicProcessing | ( | ClockP_Object * | obj, |
void * | userArg | ||
) |
void EIP_DLR_addToExceptionList | ( | EIP_DLRHandle | dlrHandle, |
uint8_t * | macId | ||
) |
void EIP_DLR_clearExceptionList | ( | EIP_DLRHandle | dlrHandle | ) |
uint8_t EIP_DLR_checkSupervisorException | ( | uint8_t * | macId, |
EIP_DLRHandle | dlrHandle | ||
) |
void EIP_DLR_addModuleIPAddress | ( | EIP_DLRHandle | dlrHandle, |
uint32_t | newIP | ||
) |
void EIP_DLR_setDivider_WD_IEP | ( | EIP_DLRHandle | dlrHandle | ) |
Sets the clock divider to 1us for IEP watch dog timers.
dlrHandle | [in] DLR handle |
void EIP_DLR_enable_WD_IEP | ( | EIP_DLRHandle | dlrHandle, |
uint8_t | id | ||
) |
Enable the IEP Watch dog timers.
dlrHandle | [in] DLR handle |
id | [in] 0/1 for WD_PD and WD_PDI respectively |
void EIP_DLR_disable_WD_IEP | ( | EIP_DLRHandle | dlrHandle, |
uint8_t | id | ||
) |
Disable the IEP Watch dog timers.
dlrHandle | [in] DLR handle |
id | [in] 0/1 for WD_PD/WD_PDI respectively |
void EIP_DLR_setTimeout_WD_IEP | ( | EIP_DLRHandle | dlrHandle, |
uint16_t | periodInMicroSec, | ||
uint8_t | id | ||
) |
Set the timeout value in watchdog.
dlrHandle | [in] DLR handle |
periodInMicroSec | [in] Timeout value in microseconds |
id | [in] watch dog ID |
void EIP_DLR_set_pdi_wd_trigger_mode | ( | EIP_DLRHandle | dlrHandle, |
uint32_t | mode | ||
) |
Set the PDI WD trigger mode.
dlrHandle | [in] DLR handle |
mode | [in] mode to be set in DGIO ctrl reg |