AM62x MCU+ SDK  12.00.00

Detailed Description

DSS Global MFLAG Config parameters.

Data Fields

uint32_t globalMflagStart
 
uint32_t globalMflagCtrl
 

Field Documentation

◆ globalMflagStart

uint32_t CSL_DssGlobalMFlagCfg::globalMflagStart

Mflag start for DMA master port, used to drive mflag signal when DMA buffer is empty at the beginning of pipeline. Refer CSL_DssMflagStartMode for values

◆ globalMflagCtrl

uint32_t CSL_DssGlobalMFlagCfg::globalMflagCtrl

Mflag Control Signal. Refer CSL_DssMflagCtrl for values