AM62x MCU+ SDK  12.00.00

Introduction

This is hardware include layer for DSS common region.

Files

file  csl_dssCommon.h
 DSS Common layer interface file.
 

Data Structures

struct  CSL_DssGlobalMFlagCfg
 DSS Global MFLAG Config parameters. More...
 
struct  CSL_DssCbaCfg
 DSS CBA Config parameters. More...
 

Functions

void CSL_dssModuleReset (CSL_dss_commRegs *commRegs)
 Reset the DSS Module. Application should make sure Video Ports are disabled before calling this API. More...
 
uint32_t CSL_dssIsOldiResetDone (const CSL_dss_commRegs *commRegs)
 Get OLDI reset status. More...
 
void CSL_dssEnableDispcIntr (CSL_dss_commRegs *commRegs, uint32_t intrMask, uint32_t intrEnable)
 Enable/disable the interrupts at DSS top level. More...
 
void CSL_dssEnablePipeIntr (CSL_dss_commRegs *commRegs, uint32_t vidPipeId, uint32_t intrMask, uint32_t intrEnable)
 Enable/disable the interrupts for Video Pipe. More...
 
void CSL_dssEnableVpIntr (CSL_dss_commRegs *commRegs, uint32_t portId, uint32_t intrMask, uint32_t intrEnable)
 Enable/disable the interrupts for Video Port. More...
 
void CSL_dssClearDispcIntr (CSL_dss_commRegs *commRegs, uint32_t intrMask)
 Clear the interrupts at DSS top level. More...
 
void CSL_dssClearPipeIntr (CSL_dss_commRegs *commRegs, uint32_t vidPipeId, uint32_t intrMask)
 Clear the interrupts for Video Pipe. More...
 
void CSL_dssClearVpIntr (CSL_dss_commRegs *commRegs, uint32_t portId, uint32_t intrMask)
 Clear the interrupts for Video Port. More...
 
uint32_t CSL_dssGetDispcIntrStatus (const CSL_dss_commRegs *commRegs)
 Get the top level interrupt status of DSS. More...
 
uint32_t CSL_dssGetPipeIntrStatus (const CSL_dss_commRegs *commRegs, uint32_t vidPipeId)
 Get the interrupt status of Video Pipe. More...
 
uint32_t CSL_dssGetVpIntrStatus (const CSL_dss_commRegs *commRegs, uint32_t portId)
 Get the interrupt status of Video Port. More...
 
void CSL_dssSetGlobalMflagConfig (CSL_dss_commRegs *commRegs, const CSL_DssGlobalMFlagCfg *mflagCfg)
 Set the global MFLAG configuration. More...
 
void CSL_dssGlobalVpEnable (CSL_dss_commRegs *commRegs, uint32_t portIdMask, uint32_t enable)
 Enable the global VP enable bit. This allows setting multiple outputs synchronously. The 'OR' result of different masks can be used as input parameter. More...
 
void CSL_dssGlobalVpGoBitEnable (CSL_dss_commRegs *commRegs, uint32_t portIdMask)
 Enable the global VP go bit. This allows setting multiple outputs synchronously. The 'OR' result of different masks can be used as input parameter. More...
 
void CSL_dssSetCbaConfig (CSL_dss_commRegs *commRegs, const CSL_DssCbaCfg *cbaCfg)
 Set the CBA configuration. More...
 
static void CSL_dssGlobalMFlagCfgInit (CSL_DssGlobalMFlagCfg *mflagCfg)
 CSL_DssGlobalMFlagCfg structure init function. More...
 
static void CSL_dssCbaCfgInit (CSL_DssCbaCfg *cbaCfg)
 CSL_DssCbaCfg structure init function. More...
 

Typedefs

typedef CSL_dss_commonRegs CSL_dss_commRegs
 DSS Common Registers. More...
 

DISPC Interrupt Mask

#define CSL_DSS_DISPC_INTR_VIDL1_MASK   ((uint32_t) 0x20U)
 Video Lite Pipeline 1 Interrupt. More...
 
#define CSL_DSS_DISPC_INTR_VID1_MASK   ((uint32_t) 0x10U)
 Video PipeLine 1 Interrupt. More...
 
#define CSL_DSS_DISPC_INTR_VP2_MASK   ((uint32_t) 0x02U)
 Video Port 2 Interrupt. More...
 
#define CSL_DSS_DISPC_INTR_VP1_MASK   ((uint32_t) 0x01U)
 Video Port 1 Interrupt. More...
 

Video Pipeline Interrupt Mask

#define CSL_DSS_VID_PIPE_INTR_SAFETYVIOLATION_MASK    ((uint32_t) CSL_DSS_COMMON_VID_IRQENABLE_0_SAFETYREGION_EN_MASK)
 Interrupt due to safety violation. More...
 
#define CSL_DSS_VID_PIPE_INTR_WINDOWEND_MASK    ((uint32_t) CSL_DSS_COMMON_VID_IRQENABLE_0_VIDENDWINDOW_EN_MASK)
 Interrupt due to video window end. More...
 
#define CSL_DSS_VID_PIPE_INTR_BUFUNDERFLOW_MASK    ((uint32_t) CSL_DSS_COMMON_VID_IRQENABLE_0_VIDBUFFERUNDERFLOW_EN_MASK)
 Interrupt due to buffer underflow. More...
 
#define CSL_DSS_VID_PIPE_INTR_ALL_MASK
 All Video Pipe interrupts. More...
 

Video Port Interrupt Mask

#define CSL_DSS_VP_INTR_FRAMEDONE_MASK    ((uint32_t) CSL_DSS_COMMON_VP_IRQENABLE_0_VPFRAMEDONE_EN_MASK)
 Frame Done for Video Port. More...
 
#define CSL_DSS_VP_INTR_VSYNC_MASK    ((uint32_t) CSL_DSS_COMMON_VP_IRQENABLE_0_VPVSYNC_EN_MASK)
 Vertical Synchronization for Video Port. More...
 
#define CSL_DSS_VP_INTR_ODDVSYNC_MASK    ((uint32_t) CSL_DSS_COMMON_VP_IRQENABLE_0_VPVSYNC_ODD_EN_MASK)
 VSYNC for odd field from interlace mode only. More...
 
#define CSL_DSS_VP_INTR_PROGLINENUM_MASK    ((uint32_t) CSL_DSS_COMMON_VP_IRQENABLE_0_VPPROGRAMMEDLINENUMBER_EN_MASK)
 Display scan has reached the programmed user line number. More...
 
#define CSL_DSS_VP_INTR_SYNCLOST_MASK    ((uint32_t) CSL_DSS_COMMON_VP_IRQENABLE_0_VPSYNCLOST_EN_MASK)
 Synchronization Lost for Video Port. More...
 
#define CSL_DSS_VP_INTR_ACBIASCOUNT_MASK    ((uint32_t) CSL_DSS_COMMON_VP_IRQENABLE_0_ACBIASCOUNTSTATUS_EN_MASK)
 AC Bias transition counter has decremented to zero. More...
 
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION0_MASK    ((uint32_t) 0x40U)
 Interrupt due to region 0 safety violation. More...
 
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION1_MASK    ((uint32_t) 0x80U)
 Interrupt due to region 1 safety violation. More...
 
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION2_MASK    ((uint32_t) 0x100U)
 Interrupt due to region 2 safety violation. More...
 
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION3_MASK    ((uint32_t) 0x200U)
 Interrupt due to region 3 safety violation. More...
 
#define CSL_DSS_VP_INTR_SECURITYVIOLATION_MASK    ((uint32_t) CSL_DSS_COMMON_VP_IRQENABLE_0_SECURITYVIOLATION_EN_MASK)
 Interrupt due to security violation. More...
 
#define CSL_DSS_VP_INTR_GOBITCLEAR_MASK    ((uint32_t) CSL_DSS_COMMON_VP_IRQENABLE_0_VPSYNC_EN_MASK)
 Go bit clear interrupt for VP. More...
 
#define CSL_DSS_VP_INTR_ALL_MASK
 All Video Port interrupts. More...
 

Mflag Start Mode

#define CSL_DSS_MFLAG_START_NORMAL    ((uint32_t) CSL_DSS_COMMON_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_START_VAL_MFLAGNORMALSTARTMODE)
 Mflag of each pipe is kept at 0 until preload is reached. More...
 
#define CSL_DSS_MFLAG_START_FORCED    ((uint32_t) CSL_DSS_COMMON_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_START_VAL_MFLAGFORCESTARTMODE)
 Mflag is driven as per Mflag Ctrl. More...
 

Mflag Control

#define CSL_DSS_MFLAG_CTRL_DISABLED    ((uint32_t) CSL_DSS_COMMON_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_CTRL_VAL_MFLAGDIS)
 Mflag is disabled. More...
 
#define CSL_DSS_MFLAG_CTRL_FORCE_ENABLE    ((uint32_t) CSL_DSS_COMMON_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_CTRL_VAL_MFLAGFORCE)
 Mflag is force enabled. More...
 
#define CSL_DSS_MFLAG_CTRL_DYNAMIC    ((uint32_t) CSL_DSS_COMMON_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_CTRL_VAL_MFLAGEN)
 Mflag signal is set dynamically as per rules. More...
 

Macro Definition Documentation

◆ CSL_DSS_DISPC_INTR_VIDL1_MASK

#define CSL_DSS_DISPC_INTR_VIDL1_MASK   ((uint32_t) 0x20U)

Video Lite Pipeline 1 Interrupt.

◆ CSL_DSS_DISPC_INTR_VID1_MASK

#define CSL_DSS_DISPC_INTR_VID1_MASK   ((uint32_t) 0x10U)

Video PipeLine 1 Interrupt.

◆ CSL_DSS_DISPC_INTR_VP2_MASK

#define CSL_DSS_DISPC_INTR_VP2_MASK   ((uint32_t) 0x02U)

Video Port 2 Interrupt.

◆ CSL_DSS_DISPC_INTR_VP1_MASK

#define CSL_DSS_DISPC_INTR_VP1_MASK   ((uint32_t) 0x01U)

Video Port 1 Interrupt.

◆ CSL_DSS_VID_PIPE_INTR_SAFETYVIOLATION_MASK

#define CSL_DSS_VID_PIPE_INTR_SAFETYVIOLATION_MASK    ((uint32_t) CSL_DSS_COMMON_VID_IRQENABLE_0_SAFETYREGION_EN_MASK)

Interrupt due to safety violation.

◆ CSL_DSS_VID_PIPE_INTR_WINDOWEND_MASK

#define CSL_DSS_VID_PIPE_INTR_WINDOWEND_MASK    ((uint32_t) CSL_DSS_COMMON_VID_IRQENABLE_0_VIDENDWINDOW_EN_MASK)

Interrupt due to video window end.

◆ CSL_DSS_VID_PIPE_INTR_BUFUNDERFLOW_MASK

#define CSL_DSS_VID_PIPE_INTR_BUFUNDERFLOW_MASK    ((uint32_t) CSL_DSS_COMMON_VID_IRQENABLE_0_VIDBUFFERUNDERFLOW_EN_MASK)

Interrupt due to buffer underflow.

◆ CSL_DSS_VID_PIPE_INTR_ALL_MASK

#define CSL_DSS_VID_PIPE_INTR_ALL_MASK
Value:
CSL_DSS_VID_PIPE_INTR_WINDOWEND_MASK | \
CSL_DSS_VID_PIPE_INTR_BUFUNDERFLOW_MASK)

All Video Pipe interrupts.

◆ CSL_DSS_VP_INTR_FRAMEDONE_MASK

#define CSL_DSS_VP_INTR_FRAMEDONE_MASK    ((uint32_t) CSL_DSS_COMMON_VP_IRQENABLE_0_VPFRAMEDONE_EN_MASK)

Frame Done for Video Port.

◆ CSL_DSS_VP_INTR_VSYNC_MASK

#define CSL_DSS_VP_INTR_VSYNC_MASK    ((uint32_t) CSL_DSS_COMMON_VP_IRQENABLE_0_VPVSYNC_EN_MASK)

Vertical Synchronization for Video Port.

◆ CSL_DSS_VP_INTR_ODDVSYNC_MASK

#define CSL_DSS_VP_INTR_ODDVSYNC_MASK    ((uint32_t) CSL_DSS_COMMON_VP_IRQENABLE_0_VPVSYNC_ODD_EN_MASK)

VSYNC for odd field from interlace mode only.

◆ CSL_DSS_VP_INTR_PROGLINENUM_MASK

#define CSL_DSS_VP_INTR_PROGLINENUM_MASK    ((uint32_t) CSL_DSS_COMMON_VP_IRQENABLE_0_VPPROGRAMMEDLINENUMBER_EN_MASK)

Display scan has reached the programmed user line number.

◆ CSL_DSS_VP_INTR_SYNCLOST_MASK

#define CSL_DSS_VP_INTR_SYNCLOST_MASK    ((uint32_t) CSL_DSS_COMMON_VP_IRQENABLE_0_VPSYNCLOST_EN_MASK)

Synchronization Lost for Video Port.

◆ CSL_DSS_VP_INTR_ACBIASCOUNT_MASK

#define CSL_DSS_VP_INTR_ACBIASCOUNT_MASK    ((uint32_t) CSL_DSS_COMMON_VP_IRQENABLE_0_ACBIASCOUNTSTATUS_EN_MASK)

AC Bias transition counter has decremented to zero.

◆ CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION0_MASK

#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION0_MASK    ((uint32_t) 0x40U)

Interrupt due to region 0 safety violation.

◆ CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION1_MASK

#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION1_MASK    ((uint32_t) 0x80U)

Interrupt due to region 1 safety violation.

◆ CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION2_MASK

#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION2_MASK    ((uint32_t) 0x100U)

Interrupt due to region 2 safety violation.

◆ CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION3_MASK

#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION3_MASK    ((uint32_t) 0x200U)

Interrupt due to region 3 safety violation.

◆ CSL_DSS_VP_INTR_SECURITYVIOLATION_MASK

#define CSL_DSS_VP_INTR_SECURITYVIOLATION_MASK    ((uint32_t) CSL_DSS_COMMON_VP_IRQENABLE_0_SECURITYVIOLATION_EN_MASK)

Interrupt due to security violation.

◆ CSL_DSS_VP_INTR_GOBITCLEAR_MASK

#define CSL_DSS_VP_INTR_GOBITCLEAR_MASK    ((uint32_t) CSL_DSS_COMMON_VP_IRQENABLE_0_VPSYNC_EN_MASK)

Go bit clear interrupt for VP.

◆ CSL_DSS_VP_INTR_ALL_MASK

#define CSL_DSS_VP_INTR_ALL_MASK
Value:
CSL_DSS_VP_INTR_VSYNC_MASK | \
CSL_DSS_VP_INTR_ODDVSYNC_MASK | \
CSL_DSS_VP_INTR_PROGLINENUM_MASK | \
CSL_DSS_VP_INTR_SYNCLOST_MASK | \
CSL_DSS_VP_INTR_ACBIASCOUNT_MASK | \
CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION0_MASK | \
CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION1_MASK | \
CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION2_MASK | \
CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION3_MASK | \
CSL_DSS_VP_INTR_SECURITYVIOLATION_MASK | \
CSL_DSS_VP_INTR_GOBITCLEAR_MASK)

All Video Port interrupts.

◆ CSL_DSS_MFLAG_START_NORMAL

#define CSL_DSS_MFLAG_START_NORMAL    ((uint32_t) CSL_DSS_COMMON_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_START_VAL_MFLAGNORMALSTARTMODE)

Mflag of each pipe is kept at 0 until preload is reached.

◆ CSL_DSS_MFLAG_START_FORCED

#define CSL_DSS_MFLAG_START_FORCED    ((uint32_t) CSL_DSS_COMMON_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_START_VAL_MFLAGFORCESTARTMODE)

Mflag is driven as per Mflag Ctrl.

◆ CSL_DSS_MFLAG_CTRL_DISABLED

#define CSL_DSS_MFLAG_CTRL_DISABLED    ((uint32_t) CSL_DSS_COMMON_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_CTRL_VAL_MFLAGDIS)

Mflag is disabled.

◆ CSL_DSS_MFLAG_CTRL_FORCE_ENABLE

#define CSL_DSS_MFLAG_CTRL_FORCE_ENABLE    ((uint32_t) CSL_DSS_COMMON_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_CTRL_VAL_MFLAGFORCE)

Mflag is force enabled.

◆ CSL_DSS_MFLAG_CTRL_DYNAMIC

#define CSL_DSS_MFLAG_CTRL_DYNAMIC    ((uint32_t) CSL_DSS_COMMON_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_CTRL_VAL_MFLAGEN)

Mflag signal is set dynamically as per rules.

Typedef Documentation

◆ CSL_dss_commRegs

DSS Common Registers.

DSS7 UL has two common blocks, hence define a generic structure to have common APIs

Function Documentation

◆ CSL_dssModuleReset()

void CSL_dssModuleReset ( CSL_dss_commRegs commRegs)

Reset the DSS Module. Application should make sure Video Ports are disabled before calling this API.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration

◆ CSL_dssIsOldiResetDone()

uint32_t CSL_dssIsOldiResetDone ( const CSL_dss_commRegs commRegs)

Get OLDI reset status.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
Returns
Reset Done Status. TRUE: Reset is complete FALSE: Reset is ongoing

◆ CSL_dssEnableDispcIntr()

void CSL_dssEnableDispcIntr ( CSL_dss_commRegs commRegs,
uint32_t  intrMask,
uint32_t  intrEnable 
)

Enable/disable the interrupts at DSS top level.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
intrMaskInterrupt Mask. Refer CSL_DssDispcIntrMask for values
intrEnableEnable/Disable the interrupt TRUE: Enable interrupt FALSE: Disable interrupt

◆ CSL_dssEnablePipeIntr()

void CSL_dssEnablePipeIntr ( CSL_dss_commRegs commRegs,
uint32_t  vidPipeId,
uint32_t  intrMask,
uint32_t  intrEnable 
)

Enable/disable the interrupts for Video Pipe.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
vidPipeIdVideo Pipe for which interrupt should be configured. Valid Values: CSL_DSS_VID_PIPE_ID_VID1 CSL_DSS_VID_PIPE_ID_VIDL1
intrMaskInterrupt Mask. Refer CSL_DssVidPipeIntrMask for values
intrEnableEnable/Disable the interrupt TRUE: Enable interrupt FALSE: Disable interrupt

◆ CSL_dssEnableVpIntr()

void CSL_dssEnableVpIntr ( CSL_dss_commRegs commRegs,
uint32_t  portId,
uint32_t  intrMask,
uint32_t  intrEnable 
)

Enable/disable the interrupts for Video Port.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
portIdVideo Port for which interrupt should be configured. Valid Values: CSL_DSS_VP_ID_1 CSL_DSS_VP_ID_2
intrMaskInterrupt Mask. Refer CSL_DssVpIntrMask for values
intrEnableEnable/Disable the interrupt TRUE: Enable interrupt FALSE: Disable interrupt

◆ CSL_dssClearDispcIntr()

void CSL_dssClearDispcIntr ( CSL_dss_commRegs commRegs,
uint32_t  intrMask 
)

Clear the interrupts at DSS top level.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
intrMaskInterrupt Mask. Refer CSL_DssDispcIntrMask for values

◆ CSL_dssClearPipeIntr()

void CSL_dssClearPipeIntr ( CSL_dss_commRegs commRegs,
uint32_t  vidPipeId,
uint32_t  intrMask 
)

Clear the interrupts for Video Pipe.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
vidPipeIdVideo Pipe for which interrupt should be cleared. Valid Values: CSL_DSS_VID_PIPE_ID_VID1 CSL_DSS_VID_PIPE_ID_VIDL1
intrMaskInterrupt Mask. Refer CSL_DssVidPipeIntrMask for values

◆ CSL_dssClearVpIntr()

void CSL_dssClearVpIntr ( CSL_dss_commRegs commRegs,
uint32_t  portId,
uint32_t  intrMask 
)

Clear the interrupts for Video Port.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
portIdVideo Port for which interrupt should be cleared. Valid Values: CSL_DSS_VP_ID_1 CSL_DSS_VP_ID_2
intrMaskInterrupt Mask. Refer CSL_DssVpIntrMask for values

◆ CSL_dssGetDispcIntrStatus()

uint32_t CSL_dssGetDispcIntrStatus ( const CSL_dss_commRegs commRegs)

Get the top level interrupt status of DSS.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
Returns
Interrupt status

◆ CSL_dssGetPipeIntrStatus()

uint32_t CSL_dssGetPipeIntrStatus ( const CSL_dss_commRegs commRegs,
uint32_t  vidPipeId 
)

Get the interrupt status of Video Pipe.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
vidPipeIdVideo Pipe for which interrupt status should be read. Valid Values: CSL_DSS_VID_PIPE_ID_VID1 CSL_DSS_VID_PIPE_ID_VIDL1
Returns
Interrupt status

◆ CSL_dssGetVpIntrStatus()

uint32_t CSL_dssGetVpIntrStatus ( const CSL_dss_commRegs commRegs,
uint32_t  portId 
)

Get the interrupt status of Video Port.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
portIdVideo Port for which interrupt status should be read. Valid Values: CSL_DSS_VP_ID_1 CSL_DSS_VP_ID_2
Returns
Interrupt status

◆ CSL_dssSetGlobalMflagConfig()

void CSL_dssSetGlobalMflagConfig ( CSL_dss_commRegs commRegs,
const CSL_DssGlobalMFlagCfg mflagCfg 
)

Set the global MFLAG configuration.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
mflagCfgPointer to CSL_DssGlobalMFlagCfg structure. This parameter should not be NULL

◆ CSL_dssGlobalVpEnable()

void CSL_dssGlobalVpEnable ( CSL_dss_commRegs commRegs,
uint32_t  portIdMask,
uint32_t  enable 
)

Enable the global VP enable bit. This allows setting multiple outputs synchronously. The 'OR' result of different masks can be used as input parameter.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
portIdMaskVideo Port for which enable bit should be set. Refer CSL_DssVpIdMask for details.
enableEnable/Disable the ports TRUE: Enable ports synchronously FALSE: Disable ports synchronously

◆ CSL_dssGlobalVpGoBitEnable()

void CSL_dssGlobalVpGoBitEnable ( CSL_dss_commRegs commRegs,
uint32_t  portIdMask 
)

Enable the global VP go bit. This allows setting multiple outputs synchronously. The 'OR' result of different masks can be used as input parameter.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
portIdMaskVideo Port for which go bit should be set. Refer CSL_DssVpIdMask for details.

◆ CSL_dssSetCbaConfig()

void CSL_dssSetCbaConfig ( CSL_dss_commRegs commRegs,
const CSL_DssCbaCfg cbaCfg 
)

Set the CBA configuration.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
cbaCfgPointer to CSL_DssCbaCfg structure. This parameter should not be NULL

◆ CSL_dssGlobalMFlagCfgInit()

static void CSL_dssGlobalMFlagCfgInit ( CSL_DssGlobalMFlagCfg mflagCfg)
inlinestatic

CSL_DssGlobalMFlagCfg structure init function.

Parameters
mflagCfgPointer to CSL_DssGlobalMFlagCfg structure

◆ CSL_dssCbaCfgInit()

static void CSL_dssCbaCfgInit ( CSL_DssCbaCfg cbaCfg)
inlinestatic

CSL_DssCbaCfg structure init function.

Parameters
cbaCfgPointer to CSL_DssCbaCfg structure
CSL_DSS_VP_INTR_FRAMEDONE_MASK
#define CSL_DSS_VP_INTR_FRAMEDONE_MASK
Frame Done for Video Port.
Definition: csl_dssCommon.h:118
CSL_DSS_VID_PIPE_INTR_SAFETYVIOLATION_MASK
#define CSL_DSS_VID_PIPE_INTR_SAFETYVIOLATION_MASK
Interrupt due to safety violation.
Definition: csl_dssCommon.h:96