AM62x MCU+ SDK  12.00.00
sdl_soc_mtog.h File Reference

Go to the source code of this file.

Macros

#define SDL_INSTANCE_WKUP_MTOG0   1U
 
#define SDL_INSTANCE_MAIN_MTOG0   2U
 
#define SDL_INSTANCE_MTOG_MAX   (SDL_INSTANCE_MAIN_MTOG0 + 1U)
 

Typedefs

typedef uint8_t SDL_MTOG_Inst
 MTOG Instance supported. More...
 

Functions

int32_t SDL_MTOG_getBaseaddr (SDL_MTOG_Inst instance, uint32_t *baseAddr)
 This API is used to get the base address of the instance. More...