AM62x MCU+ SDK  12.00.00
sdl Directory Reference

Directories

directory  dcc
 
directory  dpl
 
directory  ecc
 
directory  esm
 
directory  include
 
directory  lbist
 
directory  mcrc
 
directory  mtog
 
directory  pbist
 
directory  pok
 
directory  r5
 
directory  rom_checksum
 
directory  rti
 
directory  stog
 
directory  vtm
 

Files

file  sdl_dcc.h [code]
 
file  sdl_ecc.h [code]
 Header file contains enumerations, structure definitions and function.
 
file  sdl_esm.h [code]
 This file contains the SDL ESM API's.
 
file  sdl_exception.h [code]
 Header file contains enumerations, structure definitions and function declarations for SDL EXCEPTION interface.
 
file  sdl_exception_priv.h [code]
 
file  sdl_lbist.h [code]
 
file  sdl_mcrc.h [code]
 
file  sdl_mtog.h [code]
 
file  sdl_pbist.h [code]
 This file contains the SDL PBIST API's.
 
file  sdl_pok.h [code]
 This file contains the prototypes of the APIs present in the device abstraction layer file of POK. This also contains some related macros.
 
file  sdl_rom_checksum.h [code]
 This file contains the SDL ROM Checksum API's.
 
file  sdl_rti.h [code]
 
file  sdl_vtm.h [code]
 This file contains the SDL VTM API's.
 
file  sdlr_tog.h [code]