AM62x MCU+ SDK  12.00.00
Release Notes 12.00.00

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.
Attention
MCU+SDK on A53 is provided as is for customers as a reference to implement/validate on their own SW Stack & OS. TI will not support these features on the E2E forum as these are not part of the MCU+SDK product. If these features need to be productized, TI can recommend third parties who can help.

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM62x M4F, R5F, A53 SK-AM62 (referred as am62x-sk in code), SK-AM62-LP (referred as am62x-sk-lp in code), SK-AM62-SIP (referred as am62x-sip-sk in code) Windows 10 64b or Ubuntu 22.04 64b

Features Added in This Release

Note
Update of OSPI tuning algorithm on this SDK causes increase in tuning time. Refer OSPI NOR Flash Performance
Attention
DeepSleep low power mode (LPM) is not supported if the DM R5 is used for a general purpose application. This is because when the SoC goes to any LPM, the context of peripherals used by DM R5 will be lost. To use DM R5 for a general purpose application, disable LPM support. Refer Disabling Low Power Mode to know how to disable LPM.
Feature Module
PADCFG drive strength adjustment through SYSCFG Pinmux
LBIST/PBIST initiated in SBL EMMC SBL
Enable WKUP-R5F ATCM SBL
Watchdog support for DM R5/WKUP-R5F WDT
Save/Restore of FPU registers on context switch enabled by default on A53 FreeRTOS
MMCSD drive strength as a configurable option MMCSD
Add 8S-8S-8S protocol support OSPI
Route SecProxy event for MCU cores DM
Interrupt mode in SCIClient SCI Client
Move task stack allocation to application layer SCI Server
Add WFI in MCU only mode to save power LPM

Dependent Tools and Compiler Information

Attention
It is recommended to use the TIFS version provided with the release for ensuring compatibility between TIFS and device manager. Using the TIFS from different MCU+SDK release is not recomended and may cause TIFS/ DM functionality to break.
Tools/Components Supported CPUs Version
Code Composer Studio M4F, R5F, A53 20.3.1
SysConfig M4F, R5F, A53 1.24.2, build 4234
TI ARM CLANG M4F, R5F 4.0.1.LTS
GCC AARCH64 A53 9.2-2019.12
FreeRTOS Kernel M4F, R5F, A53 11.1.0

SDK Components

SYSFW / TIFS

Version 12.00.02
Release Notes LINK
User Guide LINK

Key Features

OS Kernel

OS Supported CPUs SysConfig Support
FreeRTOS Kernel M4F, R5F, A53 NA
FreeRTOS POSIX M4F, A53 NA
No RTOS M4F, R5F, A53 NA

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support
Address Translate M4F, R5F Yes FreeRTOS, NORTOS
Cache R5F, A53 Yes FreeRTOS, NORTOS
Clock M4F, R5F, A53 Yes FreeRTOS, NORTOS
CycleCounter M4F, R5F, A53 NA FreeRTOS, NORTOS
Debug M4F, R5F, A53 Yes FreeRTOS, NORTOS
Heap M4F, R5F, A53 NA FreeRTOS, NORTOS
Hwi M4F, R5F, A53 Yes FreeRTOS, NORTOS
MPU M4F, R5F, A53 Yes FreeRTOS, NORTOS
Semaphore M4F, R5F, A53 NA FreeRTOS, NORTOS
Task M4F, R5F, A53 NA FreeRTOS
Timer M4F, R5F, A53 Yes FreeRTOS, NORTOS

Secondary Bootloader (SBL)

SBL Mode Supported CPUs SysConfig Support PHY Support DMA Support OS support
OSPI NOR R5F Yes Yes Yes NORTOS
OSPI NAND R5F Yes Yes Yes NORTOS
EMMC R5F Yes NA NA NORTOS
UART R5F Yes NA No NORTOS

Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
TSN A53 NO FreeRTOS gPTP IEEE 802.1 AS-2020 compliant gPTP stack, End Nodes and Bridge mode support, YANG data model configuration Multi-Clock Domain
LwIP A53 YES FreeRTOS TCP/UDP IP networking stack with and without checksum offload enabled, TCP/UDP IP networking stack with server and client functionality, basic Socket APIs, netconn APIs and raw APIs, DHCP, ping, TCP iperf, scatter-gather, DSCP priority mapping, LwIP bridge, shared memory driver Other LwIP features
Ethernet driver (ENET) A53 YES FreeRTOS Ethernet as port using CPSW, MAC loopback and PHY loopback, Layer 2 MAC, Packet Timestamping, CPSW Switch, Policer and Classifier, MDIO Manual Mode, CBS (IEEE 802.1Qav) on CPSW, IET (IEEE 802.1Qbu) on CPSW, Strapped PHY (Early Ethernet), cut through switch on CPSW RMII mode

SOC Device Drivers

Note
See the updated MCASP usage guidelines in MCASP for changes in MCASP driver
Peripheral Domain Supported CPUs SysConfig Support
DDR Main R5F Yes
DSS Main A53 Yes
ECAP Main A53 Yes
EPWM Main M4F, A53 Yes
EQEP Main A53 Yes
GPIO MCU M4F, R5F Yes
Main M4F, R5F, A53 Yes
GPMC Main R5F, A53 Yes
I2C Main M4F, R5F, A53 Yes
MCU M4F, R5F Yes
Wakeup M4F, R5F Yes
IPC Main M4F, R5F, A53 Yes
MCAN Main R5F, A53 Yes
MCU M4F Yes
MCASP Main A53 Yes
MCSPI Main M4F, R5F, A53 Yes
MCU M4F, R5F Yes
MMCSD Main R5F, A53 Yes
OSPI Main R5F, A53 Yes
Pinmux Main M4F, R5F, A53 Yes
MCU M4F, R5F Yes
Wakeup M4F, R5F Yes
PMU Wakeup R5F Yes
RTC Main R5F, A53 Yes
SOC NA M4F, R5F, A53 Yes
SCIClient NA M4F, R5F, A53 Yes
Spinlock Main A53 Yes
Wakeup R5F Yes
UART Main M4F, R5F, A53 Yes
MCU M4F, R5F Yes
Wakeup R5F Yes
UDMA Main R5F, A53 Yes
WDT Main A53 Yes
Wakeup R5F Yes
Note
Refer Accessing main and wakeup domain peripherals from MCU domain for accessing main/wakeup peripherals from MCU Domain.

Board Device Drivers

Peripheral Supported CPUs SysConfig Support
EEPROM A53 Yes
Ethernet PHY A53 Yes
Flash R5F, A53 Yes
LED M4F, R5F, A53 Yes

Software Diagnostic Library (SDL)

SDL Module Supported CPUs SysConfig Support
ESM M4F, R5F No
MCRC M4F, R5F No
RTI M4F, R5F No
DCC M4F, R5F No
VTM M4F, R5F No
STOG M4F, R5F No
PBIST M4F, R5F No
MTOG M4F No
POK M4F, R5F No
ECC M4F, R5F No
LBIST M4F No
ROM Checksum R5F No

Fixed Issues

ID Head Line Module
EXT_SITMPUSW-245 MCU+ SDK LPDDR4 Driver starts DDR Training/Leveling Sequence twice DDR
EXT_SITMPUSW-293 Sciclient driver uses incorrect context for the TISCI_MSG_KEYRING_IMPORT DM
EXT_SITMPUSW-309 LPM: Spurious wake up on MCU only mode DM
EXT_SITMPUSW-303 DM does not handle NACK properly for LPM msgs and RM board config msg DM
EXT_SITMPUSW-291 Wait for Status mechanism via Sciclient API call fails during self reset DM
EXT_SITMPUSW-312 Incorrect context description of SCICLIENT_CONTEXT_DM2TIFS DM
EXT_SITMPUSW-288 LPM: Unable to enter LPM in Interrupt Mode DM
EXT_SITMPUSW-251 MCU+ SDK Example Projects using incorrect ARMv7 MPU Attributes for Peripheral Register Region Examples
EXT_SITMPUSW-297 Flash Params Not Reflected In Syscfg FLASH
EXT_SITMPUSW-301 OSPI_norFlashInit1s1s1s has an implementation of wait for 500 milliseconds instead of microseconds Flash
EXT_SITMPUSW-304 AM62x: Critical section protection not added in vPortTimerTickHandler for A53 FreeRTOS
EXT_SITMPUSW-282 Sysconfig not generating code for GPIO Trigger GPIO
EXT_SITMPUSW-279 I2C close is not working properly during error conditions I2C
EXT_SITMPUSW-306 Missing call to I2C_lld_recoverBus on polling mode I2C
EXT_SITMPUSW-277 MCASP: tx.evtCtl Used Instead of rx.evtCtl for REVTCTL Configuration MCASP
EXT_SITMPUSW-276 MCASP: intCfgTx.intrNum Used Instead of intCfgRx.intrNum in Interrupt Check MCASP
EXT_SITMPUSW-114 MMCSD_enableBootPartition implements two mutually exclusive concepts as one function MMCSD
EXT_SITMPUSW-295 Flash Close Logic Requires OSPI Handle to be reset to 1S-1S-1S OSPI
EXT_SITMPUSW-280 OSPI Indac Mode Should Check for odd bytes OSPI
EXT_SITMPUSW-256 Incorrect calculation of rowColEnd in the ext_otp_writeMmr OTP
EXT_SITMPUSW-292 Bootloader_socOpenFirewalls is called before System_init in the SBLs SBL
EXT_SITMPUSW-214 WDT: Hang due to no valid argument check in APIs Watchdog
EXT_EP-13267 SDL ESM: Wrong instance argument in SDL_ESM_loInterruptHandler causing misidentification of ESM0 interrupts SDL-ESM

Known Issues

ID Head Line Module
EXT_SITMPUSW-153 MCU+ SDK CCS Project Build Generates Invalid/Redundant Boot Image Files Build
EXT_SITMPUSW-87 Sysconfig crashing when adding large number of GPIO pins GPIO
EXT_SITMPUSW-28 Outstanding mailbox messages prevent suspend IPC
EXT_SITMPUSW-222 MMCSD field Card Type is not ordered logically in the Sysconfig MMCSD
EXT_SITMPUSW-220 SBL_SD bootloaders report incorrect boot image size SBL
EXT_SITMPUSW-214 Spinlock: Missing NULL Pointer Validation for Base Address Parameter in Spinlock APIs Spinlock
EXT_SITMPUSW-324 UART_udmaIsrTx does not handles continuous Callbacks properly UART
EXT_EP-12275 AM62x: ECC: SDL_WKUP_R5FSS0_PULSAR_UL_CPU0_ECC_AGGR and SDL_DMASS0_DMSS_AM62_ECCAGGR aggregators are failing SDL-ECC
PROC_SDL-8868 AM62x: ECC: ecc_test_app is failing SDL-ECC
EXT_EP-12276 ECC: Firewall related aggregators failures SDL-ECC
EXT_EP-12278 ECC Aggregator SMS0_SMS_HSM_ECC Aggr fails on AM62x SDL-ECC
EXT_EP-12279 CSI RX ECC aggregators are failing on AM62P/AM62X SDL-ECC

Limitations

S.No Head Line Module
1 The ROM startup model for runtime initializations in TI ARM CLANG is not supported/tested in the SDK NA
2 PHY mode not supported for OSPI NAND SBL on DDR mode. It is supported for SDR mode only Bootloader
3 LPM is not supported with SBL boot flow. It is supported only with SPL boot flow. Bootloader

Upgrade and Compatibility Information

This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.

The below table captures the list of migration document sections when migrating from one version to another. The migration for a partcluar module will be applicable, if you are migrating from older version listed to newer version listed on the table below.

Module Migration guide Older version Newer version
Bootloader Bootloader Migration Guidelines<= 10.01.00 >= 11.00.00
NETWORKING Version Updates from earlier SDKs to Latest<= 11.01.00 >= 11.02.00
OSPI OSPI Migration Guide<= 11.01.00 >= 11.02.00
Watchdog Migration Guide 11.02 to 12.00<= 11.02.00 >= 12.00.00
SCI Server Migration Guide 11.02 to 12.00<= 11.02.00 >= 12.00.00
SBL Linker Migration Guide 11.02 to 12.00<= 11.02.00 >= 12.00.00

Networking

Module Affected API Change
TSN notify_linkchange notify_linkchange function is renamed to cb_lld_notify_linkchange, include path <tsn_combase/tilld/cb_lld_ethernet.h> in the file that uses cb_lld_notify_linkchange.