AM62x MCU+ SDK  09.02.00
GPMC_timingParams Struct Reference

Detailed Description

GPMC timing parameters.

Data Fields

uint32_t csOnTime
 
uint32_t csRdOffTime
 
uint32_t csWrOffTime
 
uint32_t advOnTime
 
uint32_t advRdOffTime
 
uint32_t advWrOffTime
 
uint32_t advAadMuxOnTime
 
uint32_t advAadMuxRdOffTime
 
uint32_t advAadMuxWrOffTime
 
uint32_t weOnTtime
 
uint32_t weOffTime
 
uint32_t oeOnTime
 
uint32_t oeOffTime
 
uint32_t oeAadMuxOnTime
 
uint32_t oeAadMuxOffTime
 
uint32_t pageBurstAccess
 
uint32_t rdAccessTime
 
uint32_t wrAcessTime
 
uint32_t rdCycleTime
 
uint32_t wrCycleTime
 
uint32_t wrDataOnMuxBusTime
 
uint32_t cycle2CycleDelay
 
uint32_t cycleDelaySameChipSel
 
uint32_t cycleDelayDiffChipSel
 
uint32_t busTurnAroundTime
 

Field Documentation

◆ csOnTime

uint32_t GPMC_timingParams::csOnTime

◆ csRdOffTime

uint32_t GPMC_timingParams::csRdOffTime

Chip Select Read de-assertion time.

◆ csWrOffTime

uint32_t GPMC_timingParams::csWrOffTime

Chip Select Write de-assertion time.

◆ advOnTime

uint32_t GPMC_timingParams::advOnTime

ADV Assertion time.

◆ advRdOffTime

uint32_t GPMC_timingParams::advRdOffTime

ADV Read de-assertion time.

◆ advWrOffTime

uint32_t GPMC_timingParams::advWrOffTime

ADV Write de-assertion time.

◆ advAadMuxOnTime

uint32_t GPMC_timingParams::advAadMuxOnTime

ADV Assertion time in an AADMultiplexed access.

◆ advAadMuxRdOffTime

uint32_t GPMC_timingParams::advAadMuxRdOffTime

ADV Read de-assertion time in an AADMultiplexed access.

◆ advAadMuxWrOffTime

uint32_t GPMC_timingParams::advAadMuxWrOffTime

ADV Write de-assertion time in an AADMultiplexed access.

◆ weOnTtime

uint32_t GPMC_timingParams::weOnTtime

WE assertion time.

◆ weOffTime

uint32_t GPMC_timingParams::weOffTime

WE de-assertion time.

◆ oeOnTime

uint32_t GPMC_timingParams::oeOnTime

OE assertion time.

◆ oeOffTime

uint32_t GPMC_timingParams::oeOffTime

OE de-assertion time.

◆ oeAadMuxOnTime

uint32_t GPMC_timingParams::oeAadMuxOnTime

OE assertion time in an AADMultiplexed access.

◆ oeAadMuxOffTime

uint32_t GPMC_timingParams::oeAadMuxOffTime

OE de-assertion time in an AADMultiplexed access.

◆ pageBurstAccess

uint32_t GPMC_timingParams::pageBurstAccess

Multiple access word delay.

◆ rdAccessTime

uint32_t GPMC_timingParams::rdAccessTime

Start-cycle to first valid delay.

◆ wrAcessTime

uint32_t GPMC_timingParams::wrAcessTime

Delay from StartAccessTime to the CLK rising edge.

◆ rdCycleTime

uint32_t GPMC_timingParams::rdCycleTime

Total read cycle time.

◆ wrCycleTime

uint32_t GPMC_timingParams::wrCycleTime

Total write cycle time.

◆ wrDataOnMuxBusTime

uint32_t GPMC_timingParams::wrDataOnMuxBusTime

Write Data on Mux Bus Time.

◆ cycle2CycleDelay

uint32_t GPMC_timingParams::cycle2CycleDelay

Chip Select high pulse delay between two successive accesses.

◆ cycleDelaySameChipSel

uint32_t GPMC_timingParams::cycleDelaySameChipSel

Value to control adding of cycle2cycle delay between two successive accesses to the same chip select.

◆ cycleDelayDiffChipSel

uint32_t GPMC_timingParams::cycleDelayDiffChipSel

Value to control adding of cycle2cycle delay between two successive accesses to the different chip select.

◆ busTurnAroundTime

uint32_t GPMC_timingParams::busTurnAroundTime

Bus turn around time between two successive accesses to the same chip-select (read to write) or to a different chip-select(read to read and read to write) in GPMC_FCLK cycles.