AM62x MCU+ SDK  09.02.00

Introduction

This file containing the GPMC API.

The GPMC header file should be included in an application as follows:

#include <drivers/gpmc.h>

Data Structures

struct  GPMC_nandCmdParams
 Data structure to set NAND command parameters. More...
 
struct  GPMC_Transaction
 GPMC_Transaction data structure is used with GPMC_transactionInit(), GPMC_nandReadData() and GPMC_nandWriteData(). More...
 
struct  GPMC_Params
 GPMC driver instance parameters. More...
 
struct  GPMC_AddrRegion
 GPMC Address Region. More...
 
struct  GPMC_Object
 GPMC driver object. More...
 
struct  GPMC_timingParams
 GPMC timing parameters. More...
 
struct  GPMC_HwAttrs
 GPMC instance attributes. More...
 
struct  GPMC_Config
 GPMC Driver configuration structure. More...
 

Functions

static void GPMC_Params_init (GPMC_Params *params)
 Function to initialize the GPMC_Params struct to its defaults. More...
 
void GPMC_init (void)
 This function initializes the GPMC module. More...
 
void GPMC_deinit (void)
 This function de-initializes the GPMC module. More...
 
GPMC_Handle GPMC_open (uint32_t index, const GPMC_Params *prms)
 This function opens a given GPMC peripheral. More...
 
void GPMC_close (GPMC_Handle handle)
 Function to close a GPMC peripheral specified by the GPMC handle. More...
 
uint32_t GPMC_getInputClk (GPMC_Handle handle)
 This function returns the input clk frequency GPMC was programmed at. More...
 
GPMC_Handle GPMC_getHandle (uint32_t driverInstanceIndex)
 This function returns the handle of an open GPMC Instance from the instance index. More...
 
void GPMC_writeNandCommandParamsInit (GPMC_nandCmdParams *cmdParams)
 Function to initialise GPMC_nandCmdParams structure to default values. More...
 
int32_t GPMC_writeNandCommand (GPMC_Handle handle, GPMC_nandCmdParams *cmdParams)
 Function to write NAND command parameters. More...
 
void GPMC_transactionInit (GPMC_Transaction *trans)
 Function to initialise GPMC_Transaction structure to default values. More...
 
int32_t GPMC_nandReadData (GPMC_Handle handle, GPMC_Transaction *trans)
 Function to read data from NAND flash using DMA or CPU prefetch/post write engine. More...
 
int32_t GPMC_nandWriteData (GPMC_Handle handle, GPMC_Transaction *trans)
 Function to write data to NANDflash using CPU prefetch/post write engine. More...
 
int32_t GPMC_setDeviceSize (GPMC_Handle handle)
 Function to set device width for GPMC instance connected to external device. More...
 
int32_t GPMC_setDeviceType (GPMC_Handle handle)
 Function to set device type (NANDLIKE OR NORLIKE) for GPMC instance connected to external device. More...
 
int32_t GPMC_configureTimingParameters (GPMC_Handle handle)
 Function to configure GPMC timing parameters. More...
 
int32_t GPMC_eccValueSizeSet (GPMC_Handle handle, uint32_t eccSize, uint32_t eccSizeVal)
 Function to set ECC used and unused bytes size in nibbles. More...
 
int32_t GPMC_eccBchConfigureElm (GPMC_Handle handle, uint8_t numSectors)
 Function to configure ELM module for error correction. More...
 
int32_t GPMC_eccEngineBCHConfig (GPMC_Handle handle, uint32_t eccSteps)
 Function to configure GPMC ECC engine for BCH algorithm. More...
 
int32_t GPMC_eccEngineEnable (GPMC_Handle handle)
 Function to enable GPMC ECC engine. More...
 
void GPMC_eccResultRegisterClear (GPMC_Handle handle)
 Function to clear GPMC ECC result register. More...
 
int32_t GPMC_eccBchFillSyndromeValue (GPMC_Handle handle, uint32_t sector, uint32_t *bchData)
 Function to fill BCH syndrome value per sector to ELM module. More...
 
int32_t GPMC_eccBchStartErrorProcessing (GPMC_Handle handle, uint8_t sector)
 Function to start error processing for a sector by ELM module. More...
 
int32_t GPMC_eccBchCheckErrorProcessingStatus (GPMC_Handle handle, uint32_t sector)
 Function to get error processing status for a sector by ELM module. More...
 
int32_t GPMC_eccBchSectorGetError (GPMC_Handle handle, uint32_t sector, uint32_t *errCount, uint32_t *errLoc)
 Function to get number of errors per sector by ELM module. More...
 
int32_t GPMC_eccCalculateBchSyndromePolynomial (GPMC_Handle handle, uint8_t *pEccdata, uint32_t sector)
 Function to compute BCH syndrome polynomial for NAND write operation. More...
 
int32_t GPMC_eccGetBchSyndromePolynomial (GPMC_Handle handle, uint32_t sector, uint32_t *bchData)
 Function to get BCH syndrome polynomial per sector NAND read operation. More...
 
int32_t GPMC_configurePrefetchPostWriteEngine (GPMC_Handle handle)
 Function to configure GPMC PREFETCH read and POST write engine. More...
 
int32_t GPMC_disableFlashWriteProtect (GPMC_Handle handle)
 Function to disable WRITE protect line. More...
 
int32_t GPMC_enableFlashWriteProtect (GPMC_Handle handle)
 Function to disable WRITE protect line. More...
 

Typedefs

typedef void * GPMC_Handle
 A handle that is returned from a GPMC_open() call. More...
 
typedef void(* GPMC_CallbackFxn) (GPMC_Handle handle, GPMC_Transaction *transaction)
 The definition of a callback function used by the GPMC driver when used in GPMC_OPERATING_MODE_CALLBACK mode. More...
 

Enumerations

enum  GPMC_nandEccAlgo {
  GPMC_NAND_ECC_ALGO_NONE = 0x00U, GPMC_NAND_ECC_ALGO_HAMMING_1BIT, GPMC_NAND_ECC_ALGO_BCH_4BIT, GPMC_NAND_ECC_ALGO_BCH_8BIT,
  GPMC_NAND_ECC_ALGO_BCH_16BIT
}
 GPMC ECC engine algoritms. More...
 
enum  GPMC_OperatingMode { GPMC_OPERATING_MODE_BLOCKING = 0, GPMC_OPERATING_MODE_CALLBACK, GPMC_OPERATING_MODE_POLLING }
 GPMC driver operating modes. More...
 
enum  GPMC_TransferMode { GPMC_TRANSFER_MODE_BLOCKING = 0, GPMC_TRANSFER_MODE_CALLBACK }
 GPMC data transfer modes. More...
 
enum  GPMC_TransactionType { GPMC_TRANSACTION_TYPE_READ = 0, GPMC_TRANSACTION_TYPE_WRITE, GPMC_TRANSACTION_TYPE_READ_CMDREG, GPMC_TRANSACTION_TYPE_WRITE_CMDREG }
 Type of the GPMC transaction for read and write. More...
 
enum  GPMC_TransactionStatus {
  GPMC_TRANSFER_COMPLETED = 0, GPMC_TRANSFER_STARTED, GPMC_TRANSFER_CANCELED, GPMC_TRANSFER_FAILED,
  GPMC_TRANSFER_CSN_DEASSERT, GPMC_TRANSFER_TIMEOUT
}
 Transaction status codes that are set by the GPMC driver. More...
 

Macros

#define GPMC_CS_TIMING_CONFIG(CSWrOffTime, CSRdOffTime, CSExtDelayFlag, CSOnTime)
 This macro used to make the conf value which is used to configure the CS signal timing configuration. More...
 
#define GPMC_ADV_TIMING_CONFIG(ADVAADMuxWrOffTime, ADVAADMuxRdOffTime, ADVWrOffTime, ADVRdOffTime, ADVExtDelayFlag, ADVAADMuxOnTime, ADVOnTime)
 This macro used to make the conf value which is used to configure the ADV# signal timing configuration. More...
 
#define GPMC_WE_OE_TIMING_CONFIG(WEOffTime, WEExtDelayFlag, WEOnTime, OEAADMuxOffTime, OEOffTime, OEExtDelayFlag, OEAADMuxOnTime, OEOnTime)
 This macro used to make the conf value which is used to configure the WE# and OE# signal timing configuration.
. More...
 
#define GPMC_RDACCESS_CYCLETIME_TIMING_CONFIG(rdCycleTime, wrCycleTime, rdAccessTime, pageBurstAccessTime)
 This macro used to make the conf value which is used to configure the read access and cycle time timing configuration.
. More...
 
#define GPMC_CYCLE2CYCLE_BUSTURNAROUND_TIMING_CONFIG(cycle2CycleDelay, cycle2CycleDelaySameCSCfg, cycle2CycleDelayDiffCSCfg, busTAtime)
 This macro used to make the conf value which is used to configure the cycle to cycle and bus turn around time timing configuration.
. More...
 
#define GPMC_DMA_COPY_LOWER_LIMIT   (512U)
 size in bytes More...
 
#define GPMC_CS_BASE_ADDR_SHIFT   (24U)
 GPMC CHIP select base address shift value. More...
 
#define GPMC_ECC_WRAP_MODE1   (1)
 GPMC ECC Wrap mode for ECC value computation. More...
 
#define GPMC_CMD_INVALID   (0xFFFFFFFFU)
 Invalid value for params initialisation. More...
 

GPMC CHIP select

Macros which can be used as to select CHIP select instance for GPMC.

#define GPMC_CHIP_SELECT_CS0   (0U)
 
#define GPMC_CHIP_SELECT_CS1   (1U)
 
#define GPMC_CHIP_SELECT_CS2   (2U)
 
#define GPMC_CHIP_SELECT_CS3   (3U)
 

GPMC Interupt status flags

Macros which can be used as 'interupt' parameter to GPMC_interuptStatusGet, GPMC_interuptStatusClear APIs.

#define GPMC_FIFOEVENT_STATUS   (0U)
 
#define GPMC_TERMINALCOUNT_STATUS   (1U)
 
#define GPMC_WAIT0EDGEDETECTION_STATUS   (2U)
 
#define GPMC_WAIT1EDGEDETECTION_STATUS   (3U)
 

GPMC Interupt Flags

Macros which can be used as 'mode' parameter to GPMC_prefetchPostWriteConfigEnable API.

#define GPMC_FIFOEVENT_INT   (0U)
 
#define GPMC_TERMINALCOUNT_INT   (1U)
 
#define GPMC_WAIT0EDGEDETECTION_INT   (2U)
 
#define GPMC_WAIT1EDGEDETECTION_INT   (3U)
 
#define GPMC_PREFETCH_ACCESSMODE_READ   (0U)
 
#define GPMC_PREFETCH_ACCESSMODE_WRITE   (1U)
 

GPMC ECC algorithm

Macros which can be used to set GPMC ECC engine algorithm.

#define GPMC_ECC_ALGORITHM_HAMMINGCODE   (0U)
 
#define GPMC_ECC_ALGORITHM_BCH   (1U)
 

GPMC ECC error correvel level.

Macros which can be used to set GPMC ECC engine error correction level.

#define GPMC_ECC_BCH_ERRCORRCAP_UPTO_4BITS   (0U)
 
#define GPMC_ECC_BCH_ERRCORRCAP_UPTO_8BITS   (1U)
 
#define GPMC_ECC_BCH_ERRCORRCAP_UPTO_16BITS   (2U)
 

GPMC ECC Result Register

Macros which can be used to select ECC result register for GPMC ECC engine.

#define GPMC_ECCPOINTER_RESULT_1   (1U)
 
#define GPMC_ECCPOINTER_RESULT_2   (2U)
 
#define GPMC_ECCPOINTER_RESULT_3   (3U)
 
#define GPMC_ECCPOINTER_RESULT_4   (4U)
 
#define GPMC_ECCPOINTER_RESULT_5   (5U)
 
#define GPMC_ECCPOINTER_RESULT_6   (6U)
 
#define GPMC_ECCPOINTER_RESULT_7   (7U)
 
#define GPMC_ECCPOINTER_RESULT_8   (8U)
 
#define GPMC_ECCPOINTER_RESULT_9   (9U)
 

GPMC ECC Size Config

Macros which can be used to set length of used and unsued bytes in the ECC value.

#define GPMC_ECC_SIZE_0   (0U)
 
#define GPMC_ECC_SIZE_1   (1U)
 

GPMC ECC Result Register Size

Macros which can be used to set ECC size for ECC result register.

#define GPMC_ECC_RESULT_1   (1U)
 
#define GPMC_ECC_RESULT_2   (2U)
 
#define GPMC_ECC_RESULT_3   (3U)
 
#define GPMC_ECC_RESULT_4   (4U)
 
#define GPMC_ECC_RESULT_5   (5U)
 
#define GPMC_ECC_RESULT_6   (6U)
 
#define GPMC_ECC_RESULT_7   (7U)
 
#define GPMC_ECC_RESULT_8   (8U)
 
#define GPMC_ECC_RESULT_9   (9U)
 

GPMC BCH RESULT

Macros which can be used to get BCH syndrome polynomial in GPMC_eccBchResultGet API.

#define GPMC_BCH_RESULT0   (0U)
 
#define GPMC_BCH_RESULT1   (1U)
 
#define GPMC_BCH_RESULT2   (2U)
 
#define GPMC_BCH_RESULT3   (3U)
 
#define GPMC_BCH_RESULT4   (4U)
 
#define GPMC_BCH_RESULT5   (5U)
 
#define GPMC_BCH_RESULT6   (6U)
 

GPMC CHIP Select SIZE

Macros which can be used to set chip select address size.

#define GPMC_CS_MASK_ADDR_SIZE_256MB   (0x00U)
 
#define GPMC_CS_MASK_ADDR_SIZE_128MB   (0x08U)
 
#define GPMC_CS_MASK_ADDR_SIZE_64MB   (0x0cU)
 
#define GPMC_CS_MASK_ADDR_SIZE_32MB   (0x0eU)
 
#define GPMC_CS_MASK_ADDR_SIZE_16MB   (0x0fU)
 

Macro Definition Documentation

◆ GPMC_CHIP_SELECT_CS0

#define GPMC_CHIP_SELECT_CS0   (0U)

◆ GPMC_CHIP_SELECT_CS1

#define GPMC_CHIP_SELECT_CS1   (1U)

◆ GPMC_CHIP_SELECT_CS2

#define GPMC_CHIP_SELECT_CS2   (2U)

◆ GPMC_CHIP_SELECT_CS3

#define GPMC_CHIP_SELECT_CS3   (3U)

◆ GPMC_FIFOEVENT_STATUS

#define GPMC_FIFOEVENT_STATUS   (0U)

◆ GPMC_TERMINALCOUNT_STATUS

#define GPMC_TERMINALCOUNT_STATUS   (1U)

◆ GPMC_WAIT0EDGEDETECTION_STATUS

#define GPMC_WAIT0EDGEDETECTION_STATUS   (2U)

◆ GPMC_WAIT1EDGEDETECTION_STATUS

#define GPMC_WAIT1EDGEDETECTION_STATUS   (3U)

◆ GPMC_FIFOEVENT_INT

#define GPMC_FIFOEVENT_INT   (0U)

◆ GPMC_TERMINALCOUNT_INT

#define GPMC_TERMINALCOUNT_INT   (1U)

◆ GPMC_WAIT0EDGEDETECTION_INT

#define GPMC_WAIT0EDGEDETECTION_INT   (2U)

◆ GPMC_WAIT1EDGEDETECTION_INT

#define GPMC_WAIT1EDGEDETECTION_INT   (3U)

◆ GPMC_PREFETCH_ACCESSMODE_READ

#define GPMC_PREFETCH_ACCESSMODE_READ   (0U)

◆ GPMC_PREFETCH_ACCESSMODE_WRITE

#define GPMC_PREFETCH_ACCESSMODE_WRITE   (1U)

◆ GPMC_ECC_ALGORITHM_HAMMINGCODE

#define GPMC_ECC_ALGORITHM_HAMMINGCODE   (0U)

◆ GPMC_ECC_ALGORITHM_BCH

#define GPMC_ECC_ALGORITHM_BCH   (1U)

◆ GPMC_ECC_BCH_ERRCORRCAP_UPTO_4BITS

#define GPMC_ECC_BCH_ERRCORRCAP_UPTO_4BITS   (0U)

◆ GPMC_ECC_BCH_ERRCORRCAP_UPTO_8BITS

#define GPMC_ECC_BCH_ERRCORRCAP_UPTO_8BITS   (1U)

◆ GPMC_ECC_BCH_ERRCORRCAP_UPTO_16BITS

#define GPMC_ECC_BCH_ERRCORRCAP_UPTO_16BITS   (2U)

◆ GPMC_ECCPOINTER_RESULT_1

#define GPMC_ECCPOINTER_RESULT_1   (1U)

◆ GPMC_ECCPOINTER_RESULT_2

#define GPMC_ECCPOINTER_RESULT_2   (2U)

◆ GPMC_ECCPOINTER_RESULT_3

#define GPMC_ECCPOINTER_RESULT_3   (3U)

◆ GPMC_ECCPOINTER_RESULT_4

#define GPMC_ECCPOINTER_RESULT_4   (4U)

◆ GPMC_ECCPOINTER_RESULT_5

#define GPMC_ECCPOINTER_RESULT_5   (5U)

◆ GPMC_ECCPOINTER_RESULT_6

#define GPMC_ECCPOINTER_RESULT_6   (6U)

◆ GPMC_ECCPOINTER_RESULT_7

#define GPMC_ECCPOINTER_RESULT_7   (7U)

◆ GPMC_ECCPOINTER_RESULT_8

#define GPMC_ECCPOINTER_RESULT_8   (8U)

◆ GPMC_ECCPOINTER_RESULT_9

#define GPMC_ECCPOINTER_RESULT_9   (9U)

◆ GPMC_ECC_SIZE_0

#define GPMC_ECC_SIZE_0   (0U)

◆ GPMC_ECC_SIZE_1

#define GPMC_ECC_SIZE_1   (1U)

◆ GPMC_ECC_RESULT_1

#define GPMC_ECC_RESULT_1   (1U)

◆ GPMC_ECC_RESULT_2

#define GPMC_ECC_RESULT_2   (2U)

◆ GPMC_ECC_RESULT_3

#define GPMC_ECC_RESULT_3   (3U)

◆ GPMC_ECC_RESULT_4

#define GPMC_ECC_RESULT_4   (4U)

◆ GPMC_ECC_RESULT_5

#define GPMC_ECC_RESULT_5   (5U)

◆ GPMC_ECC_RESULT_6

#define GPMC_ECC_RESULT_6   (6U)

◆ GPMC_ECC_RESULT_7

#define GPMC_ECC_RESULT_7   (7U)

◆ GPMC_ECC_RESULT_8

#define GPMC_ECC_RESULT_8   (8U)

◆ GPMC_ECC_RESULT_9

#define GPMC_ECC_RESULT_9   (9U)

◆ GPMC_BCH_RESULT0

#define GPMC_BCH_RESULT0   (0U)

◆ GPMC_BCH_RESULT1

#define GPMC_BCH_RESULT1   (1U)

◆ GPMC_BCH_RESULT2

#define GPMC_BCH_RESULT2   (2U)

◆ GPMC_BCH_RESULT3

#define GPMC_BCH_RESULT3   (3U)

◆ GPMC_BCH_RESULT4

#define GPMC_BCH_RESULT4   (4U)

◆ GPMC_BCH_RESULT5

#define GPMC_BCH_RESULT5   (5U)

◆ GPMC_BCH_RESULT6

#define GPMC_BCH_RESULT6   (6U)

◆ GPMC_CS_MASK_ADDR_SIZE_256MB

#define GPMC_CS_MASK_ADDR_SIZE_256MB   (0x00U)

◆ GPMC_CS_MASK_ADDR_SIZE_128MB

#define GPMC_CS_MASK_ADDR_SIZE_128MB   (0x08U)

◆ GPMC_CS_MASK_ADDR_SIZE_64MB

#define GPMC_CS_MASK_ADDR_SIZE_64MB   (0x0cU)

◆ GPMC_CS_MASK_ADDR_SIZE_32MB

#define GPMC_CS_MASK_ADDR_SIZE_32MB   (0x0eU)

◆ GPMC_CS_MASK_ADDR_SIZE_16MB

#define GPMC_CS_MASK_ADDR_SIZE_16MB   (0x0fU)

◆ GPMC_CS_TIMING_CONFIG

#define GPMC_CS_TIMING_CONFIG (   CSWrOffTime,
  CSRdOffTime,
  CSExtDelayFlag,
  CSOnTime 
)
Value:
((uint32_t) (((CSWrOffTime) << CSL_GPMC_CONFIG2_CSWROFFTIME_SHIFT) \
& CSL_GPMC_CONFIG2_CSWROFFTIME_MASK) | \
(((CSRdOffTime) << CSL_GPMC_CONFIG2_CSRDOFFTIME_SHIFT) \
& CSL_GPMC_CONFIG2_CSRDOFFTIME_MASK) | \
(((CSExtDelayFlag) << CSL_GPMC_CONFIG2_CSEXTRADELAY_SHIFT) \
& CSL_GPMC_CONFIG2_CSEXTRADELAY_MASK) | \
(((CSOnTime) << CSL_GPMC_CONFIG2_CSONTIME_SHIFT) \
& CSL_GPMC_CONFIG2_CSONTIME_MASK))

This macro used to make the conf value which is used to configure the CS signal timing configuration.

Parameters
CSWrOffTimeCS# de-assertion time from start cycle time for write accesses in GPMC_FCLK cycles.
CSRdOffTimeCS# de-assertion time from start cycle time for read accesses in GPMC_FCLK cycles
CSExtDelayFlagFlag to indicate whether to add half GPMC_FCLK delay to CS or not.
This can take one of the following values :
CSL_GPMC_CONFIG2_CSEXTRADELAY_DELAYED : CS# Timing control signal is delayed of half GPMC_FCLK cycle.
CSL_GPMC_CONFIG2_CSEXTRADELAY_NOTDELAYED : CS# Timing control signal is not delayed.
CSOnTimeCS# assertion time from start cycle time in GPMC_FCLK cycles.

◆ GPMC_ADV_TIMING_CONFIG

#define GPMC_ADV_TIMING_CONFIG (   ADVAADMuxWrOffTime,
  ADVAADMuxRdOffTime,
  ADVWrOffTime,
  ADVRdOffTime,
  ADVExtDelayFlag,
  ADVAADMuxOnTime,
  ADVOnTime 
)
Value:
((uint32_t) (((ADVAADMuxWrOffTime) << \
CSL_GPMC_CONFIG3_ADVAADMUXWROFFTIME_SHIFT) & \
CSL_GPMC_CONFIG3_ADVAADMUXWROFFTIME_MASK) | \
(((ADVAADMuxRdOffTime) << CSL_GPMC_CONFIG3_ADVAADMUXRDOFFTIME_SHIFT) & \
CSL_GPMC_CONFIG3_ADVAADMUXRDOFFTIME_MASK) | \
(((ADVWrOffTime) << CSL_GPMC_CONFIG3_ADVWROFFTIME_SHIFT) & \
CSL_GPMC_CONFIG3_ADVWROFFTIME_MASK) | \
(((ADVRdOffTime) << CSL_GPMC_CONFIG3_ADVRDOFFTIME_SHIFT) & \
CSL_GPMC_CONFIG3_ADVRDOFFTIME_MASK) | \
(((ADVExtDelayFlag) << CSL_GPMC_CONFIG3_ADVEXTRADELAY_SHIFT) & \
CSL_GPMC_CONFIG3_ADVEXTRADELAY_MASK) | \
(((ADVAADMuxOnTime) << CSL_GPMC_CONFIG3_ADVAADMUXONTIME_SHIFT) & \
CSL_GPMC_CONFIG3_ADVAADMUXONTIME_MASK) | \
(((ADVOnTime) << CSL_GPMC_CONFIG3_ADVONTIME_SHIFT) & \
CSL_GPMC_CONFIG3_ADVONTIME_MASK))

This macro used to make the conf value which is used to configure the ADV# signal timing configuration.

Parameters
ADVAADMuxWrOffTimeADV# de-assertion time in GPMC_FCLK cycles for first address phase when using the AAD-Mux prorocol.
ADVAADMuxRdOffTimeADV# de-assertion time in GPMC_FCLK cycles for first address phase when using the AAD-Mux prorocol.
ADVWrOffTimeADV# de-assertion time in GPMC_FCLK cycles from start cycle time for write accesses
ADVRdOffTimeADV# de-assertion time in GPMC_FCLK cycles from start cycle time for write accesses
ADVExtDelayFlagFlag to indicate whether to add half GPMC_FCLK delay to ADV or not.
This can take one of the following values :
CSL_GPMC_CONFIG3_ADVEXTRADELAY_DELAYED : ADV# Timing control signal is delayed of half GPMC_FCLK cycle.
CSL_GPMC_CONFIG3_ADVEXTRADELAY_NOTDELAYED : ADV# Timing control signal is not delayed.
ADVAADMuxOnTimeADV# assertion time in GPMC_FCLK cycles for first address phase when using the AAD-Multiplexed protocol.
ADVOnTimeADV# assertion time from start cycle time in GPMC_FCLK cycles.

◆ GPMC_WE_OE_TIMING_CONFIG

#define GPMC_WE_OE_TIMING_CONFIG (   WEOffTime,
  WEExtDelayFlag,
  WEOnTime,
  OEAADMuxOffTime,
  OEOffTime,
  OEExtDelayFlag,
  OEAADMuxOnTime,
  OEOnTime 
)
Value:
((uint32_t) (((WEOffTime) << \
CSL_GPMC_CONFIG4_WEOFFTIME_SHIFT) & \
CSL_GPMC_CONFIG4_WEOFFTIME_MASK) | \
(((WEExtDelayFlag) << \
CSL_GPMC_CONFIG4_WEEXTRADELAY_SHIFT) & CSL_GPMC_CONFIG4_WEEXTRADELAY_MASK) | \
(((WEOnTime) << \
CSL_GPMC_CONFIG4_WEONTIME_SHIFT) & CSL_GPMC_CONFIG4_WEONTIME_MASK) | \
(((OEAADMuxOffTime) << \
CSL_GPMC_CONFIG4_OEAADMUXOFFTIME_SHIFT) & \
CSL_GPMC_CONFIG4_OEAADMUXOFFTIME_MASK) | \
(((OEOffTime) << \
CSL_GPMC_CONFIG4_OEOFFTIME_SHIFT) & CSL_GPMC_CONFIG4_OEOFFTIME_MASK) | \
(((OEExtDelayFlag) << \
CSL_GPMC_CONFIG4_OEEXTRADELAY_SHIFT) & CSL_GPMC_CONFIG4_OEEXTRADELAY_MASK) | \
(((OEAADMuxOnTime) << \
CSL_GPMC_CONFIG4_OEAADMUXONTIME_SHIFT) & \
CSL_GPMC_CONFIG4_OEAADMUXONTIME_MASK) | \
(((OEOnTime) << \
CSL_GPMC_CONFIG4_OEONTIME_SHIFT) & CSL_GPMC_CONFIG4_OEONTIME_MASK))

This macro used to make the conf value which is used to configure the WE# and OE# signal timing configuration.
.

Parameters
WEOffTimeWE# de-assertion time in GPMC_FCLK cycles from start cycle time.
WEExtDelayFlagFlag to indicate whether to add half GPMC_FCLK delay to WE or not.
This can take one of the following values :
CSL_GPMC_CONFIG4_WEEXTRADELAY_DELAYED : WE# Timing control signal is delayed of half GPMC_FCLK cycle.
CSL_GPMC_CONFIG4_WEEXTRADELAY_NOTDELAYED : WE# Timing control signal is not delayed.
WEOnTimeWE# assertion time in GPMC_FCLK cycles from start cycle time.
OEAADMuxOffTimeOE# de-assertion time in GPMC_FCLK cycles for first address phase when using the AAD-Mux prorocol.
OEOffTimeOE# de-assertion time in GPMC_FCLK cycles from start cycle time.
OEExtDelayFlagFlag to indicate whether to add half GPMC_FCLK delay to OE or not.
This can take one of the following values : CSL_GPMC_CONFIG4_OEEXTRADELAY_DELAYED : OE# Timing control signal is delayed of half GPMC_FCLK cycle.
CSL_GPMC_CONFIG4_OEEXTRADELAY_NOTDELAYED : OE# Timing control signal is not delayed.
OEAADMuxOnTimeOE# assertion time in GPMC_FCLK cycles for first address phase when using the AAD-Mux prorocol.
OEOnTimeOE# assertion time in GPMC_FCLK cycles from start cycle time.

◆ GPMC_RDACCESS_CYCLETIME_TIMING_CONFIG

#define GPMC_RDACCESS_CYCLETIME_TIMING_CONFIG (   rdCycleTime,
  wrCycleTime,
  rdAccessTime,
  pageBurstAccessTime 
)
Value:
((uint32_t) (((rdCycleTime) << \
CSL_GPMC_CONFIG5_RDCYCLETIME_SHIFT) & \
CSL_GPMC_CONFIG5_RDCYCLETIME_MASK) | \
(((wrCycleTime) << \
CSL_GPMC_CONFIG5_WRCYCLETIME_SHIFT) & CSL_GPMC_CONFIG5_WRCYCLETIME_MASK) | \
(((rdAccessTime) << \
CSL_GPMC_CONFIG5_RDACCESSTIME_SHIFT) & CSL_GPMC_CONFIG5_RDACCESSTIME_MASK) | \
(((pageBurstAccessTime) << \
CSL_GPMC_CONFIG5_PAGEBURSTACCESSTIME_SHIFT) & \
CSL_GPMC_CONFIG5_PAGEBURSTACCESSTIME_MASK))

This macro used to make the conf value which is used to configure the read access and cycle time timing configuration.
.

Parameters
rdCycleTimeTotal read cycle time in GPMC_FCLK cycles.
wrCycleTimeTotal write cycle time in GPMC_FCLK cycles.
rdAccessTimeRead access time (Delay between start cycle time and first data valid) in GPMC_FCLK cycles.
pageBurstAccessTimePage burest access time (Delay between successive words in a multiple access)in GPMC_FCLK cycles.

◆ GPMC_CYCLE2CYCLE_BUSTURNAROUND_TIMING_CONFIG

#define GPMC_CYCLE2CYCLE_BUSTURNAROUND_TIMING_CONFIG (   cycle2CycleDelay,
  cycle2CycleDelaySameCSCfg,
  cycle2CycleDelayDiffCSCfg,
  busTAtime 
)
Value:
((uint32_t) (((cycle2CycleDelay) << \
CSL_GPMC_CONFIG6_CYCLE2CYCLEDELAY_SHIFT) & \
CSL_GPMC_CONFIG6_CYCLE2CYCLEDELAY_MASK) | \
(((cycle2CycleDelaySameCSCfg) << \
CSL_GPMC_CONFIG6_CYCLE2CYCLESAMECSEN_SHIFT) & \
CSL_GPMC_CONFIG6_CYCLE2CYCLESAMECSEN_MASK) | \
(((cycle2CycleDelayDiffCSCfg) << \
CSL_GPMC_CONFIG6_CYCLE2CYCLEDIFFCSEN_SHIFT) & \
CSL_GPMC_CONFIG6_CYCLE2CYCLEDIFFCSEN_MASK) | \
(((busTAtime) << \
CSL_GPMC_CONFIG6_BUSTURNAROUND_SHIFT) & CSL_GPMC_CONFIG6_BUSTURNAROUND_MASK))

This macro used to make the conf value which is used to configure the cycle to cycle and bus turn around time timing configuration.
.

Parameters
cycle2CycleDelayCycle to cycle delay (Chip select high pulse delay between two successive accesses)in GPMC_FCLK cycles.
cycle2CycleDelaySameCSCfgSpecified whether to add the cycle to cycle delay between two successive accesses or not (to the same chip-select).
This can take one of the following values :
CSL_GPMC_CONFIG6_CYCLE2CYCLESAMECSEN_C2CDELAY : To add the delay.
CSL_GPMC_CONFIG6_CYCLE2CYCLESAMECSEN_NOC2CDELAY : Don't add the delay.
cycle2CycleDelayDiffCSCfgSpecified whether to add the cycle to cycle delay between two successive accesses or not (to the diffrent chip-select).
This can take one of the following values :
CSL_GPMC_CONFIG6_CYCLE2CYCLEDIFFCSEN_C2CDELAY : To add the delay.
CSL_GPMC_CONFIG6_CYCLE2CYCLEDIFFCSEN_NOC2CDELAY : Don't add the delay.
busTAtimeBus turn aroung time between two successive accesses to the same chip-select (read to write) or to a diff chip-select in GPMC_FCLK cycles.

◆ GPMC_DMA_COPY_LOWER_LIMIT

#define GPMC_DMA_COPY_LOWER_LIMIT   (512U)

size in bytes

◆ GPMC_CS_BASE_ADDR_SHIFT

#define GPMC_CS_BASE_ADDR_SHIFT   (24U)

GPMC CHIP select base address shift value.

◆ GPMC_ECC_WRAP_MODE1

#define GPMC_ECC_WRAP_MODE1   (1)

GPMC ECC Wrap mode for ECC value computation.

◆ GPMC_CMD_INVALID

#define GPMC_CMD_INVALID   (0xFFFFFFFFU)

Invalid value for params initialisation.

Typedef Documentation

◆ GPMC_Handle

typedef void* GPMC_Handle

A handle that is returned from a GPMC_open() call.

◆ GPMC_CallbackFxn

typedef void(* GPMC_CallbackFxn) (GPMC_Handle handle, GPMC_Transaction *transaction)

The definition of a callback function used by the GPMC driver when used in GPMC_OPERATING_MODE_CALLBACK mode.

Parameters
GPMC_HandleGPMC_Handle
GPMC_Transaction*GPMC_Transaction*

Enumeration Type Documentation

◆ GPMC_nandEccAlgo

GPMC ECC engine algoritms.

Enumerator
GPMC_NAND_ECC_ALGO_NONE 
GPMC_NAND_ECC_ALGO_HAMMING_1BIT 
GPMC_NAND_ECC_ALGO_BCH_4BIT 
GPMC_NAND_ECC_ALGO_BCH_8BIT 
GPMC_NAND_ECC_ALGO_BCH_16BIT 

◆ GPMC_OperatingMode

GPMC driver operating modes.

Enumerator
GPMC_OPERATING_MODE_BLOCKING 

Interupt based blocking mode

GPMC_OPERATING_MODE_CALLBACK 

Interupt based callback mode

GPMC_OPERATING_MODE_POLLING 

Non interupt base blocking mode

◆ GPMC_TransferMode

GPMC data transfer modes.

Enumerator
GPMC_TRANSFER_MODE_BLOCKING 

GPMC driver transaction blocks execution. This mode can only be used when called within a Task context and is interrupt based.

GPMC_TRANSFER_MODE_CALLBACK 

GPMC driver transaction does not block code execution and will call a callback function. This mode can be used in a Task, Swi, or Hwi context.

◆ GPMC_TransactionType

Type of the GPMC transaction for read and write.

Enumerator
GPMC_TRANSACTION_TYPE_READ 

Read transaction

GPMC_TRANSACTION_TYPE_WRITE 

Write transaction

GPMC_TRANSACTION_TYPE_READ_CMDREG 

Read transaction with command register

GPMC_TRANSACTION_TYPE_WRITE_CMDREG 

Write transaction with command register

◆ GPMC_TransactionStatus

Transaction status codes that are set by the GPMC driver.

Enumerator
GPMC_TRANSFER_COMPLETED 
GPMC_TRANSFER_STARTED 
GPMC_TRANSFER_CANCELED 
GPMC_TRANSFER_FAILED 
GPMC_TRANSFER_CSN_DEASSERT 
GPMC_TRANSFER_TIMEOUT 

Function Documentation

◆ GPMC_Params_init()

static void GPMC_Params_init ( GPMC_Params params)
inlinestatic

Function to initialize the GPMC_Params struct to its defaults.

Parameters
paramsPointer to GPMC_Params structure for initialization

◆ GPMC_init()

void GPMC_init ( void  )

This function initializes the GPMC module.

◆ GPMC_deinit()

void GPMC_deinit ( void  )

This function de-initializes the GPMC module.

◆ GPMC_open()

GPMC_Handle GPMC_open ( uint32_t  index,
const GPMC_Params prms 
)

This function opens a given GPMC peripheral.

Precondition
GPMC controller has been initialized using GPMC_init()
Parameters
indexIndex of config to use in the GPMC_Config array
prmsPointer to parameters GPMC_Params to open the driver instance.
Returns
A GPMC_Handle on success or a NULL on an error or if it has been opened already
See also
GPMC_init()
GPMC_close()

◆ GPMC_close()

void GPMC_close ( GPMC_Handle  handle)

Function to close a GPMC peripheral specified by the GPMC handle.

Precondition
GPMC_open() has to be called first
Parameters
handleGPMC_Handle returned from GPMC_open()
See also
GPMC_open()

◆ GPMC_getInputClk()

uint32_t GPMC_getInputClk ( GPMC_Handle  handle)

This function returns the input clk frequency GPMC was programmed at.

Precondition
GPMC controller has been opened using GPMC_open()
Parameters
handleAn GPMC_Handle returned from an GPMC_open()
Returns
GPMC RCLK in Hertz

◆ GPMC_getHandle()

GPMC_Handle GPMC_getHandle ( uint32_t  driverInstanceIndex)

This function returns the handle of an open GPMC Instance from the instance index.

Precondition
GPMC controller has been opened using GPMC_open()
Parameters
driverInstanceIndexIndex of config to use in the OSPI_Config array
Returns
An GPMC_Handle if it has been opened already or NULL otherwise
See also
GPMC_init()
GPMC_open()

◆ GPMC_writeNandCommandParamsInit()

void GPMC_writeNandCommandParamsInit ( GPMC_nandCmdParams cmdParams)

Function to initialise GPMC_nandCmdParams structure to default values.

Parameters
cmdParamsPointer to GPMC_nandCmdParams structure

◆ GPMC_writeNandCommand()

int32_t GPMC_writeNandCommand ( GPMC_Handle  handle,
GPMC_nandCmdParams cmdParams 
)

Function to write NAND command parameters.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
cmdParamsPointer to GPMC_nandCmdParams structure
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_transactionInit()

void GPMC_transactionInit ( GPMC_Transaction trans)

Function to initialise GPMC_Transaction structure to default values.

Parameters
transPointer to GPMC_Transaction structure

◆ GPMC_nandReadData()

int32_t GPMC_nandReadData ( GPMC_Handle  handle,
GPMC_Transaction trans 
)

Function to read data from NAND flash using DMA or CPU prefetch/post write engine.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
transPointer to GPMC_Transaction structure
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_nandWriteData()

int32_t GPMC_nandWriteData ( GPMC_Handle  handle,
GPMC_Transaction trans 
)

Function to write data to NANDflash using CPU prefetch/post write engine.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
transPointer to GPMC_Transaction structure
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_setDeviceSize()

int32_t GPMC_setDeviceSize ( GPMC_Handle  handle)

Function to set device width for GPMC instance connected to external device.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_setDeviceType()

int32_t GPMC_setDeviceType ( GPMC_Handle  handle)

Function to set device type (NANDLIKE OR NORLIKE) for GPMC instance connected to external device.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_configureTimingParameters()

int32_t GPMC_configureTimingParameters ( GPMC_Handle  handle)

Function to configure GPMC timing parameters.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccValueSizeSet()

int32_t GPMC_eccValueSizeSet ( GPMC_Handle  handle,
uint32_t  eccSize,
uint32_t  eccSizeVal 
)

Function to set ECC used and unused bytes size in nibbles.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
eccSizeParam to set GPMC_ECC_SIZE_0 (used bytes) or GPMC_ECC_SIZE_1 unused bytes
eccSizeValECC used or ununsed bytes value in nibbles.
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccBchConfigureElm()

int32_t GPMC_eccBchConfigureElm ( GPMC_Handle  handle,
uint8_t  numSectors 
)

Function to configure ELM module for error correction.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
numSectorsNumber of 512 bytes sector in a NAND page.
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccEngineBCHConfig()

int32_t GPMC_eccEngineBCHConfig ( GPMC_Handle  handle,
uint32_t  eccSteps 
)

Function to configure GPMC ECC engine for BCH algorithm.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
eccStepsNumber of 512 bytes sectors to process BCH syndrome polynomial computation.
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccEngineEnable()

int32_t GPMC_eccEngineEnable ( GPMC_Handle  handle)

Function to enable GPMC ECC engine.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccResultRegisterClear()

void GPMC_eccResultRegisterClear ( GPMC_Handle  handle)

Function to clear GPMC ECC result register.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()

◆ GPMC_eccBchFillSyndromeValue()

int32_t GPMC_eccBchFillSyndromeValue ( GPMC_Handle  handle,
uint32_t  sector,
uint32_t *  bchData 
)

Function to fill BCH syndrome value per sector to ELM module.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
sectorSector number
bchDataPointer to syndrome polynomial value.
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccBchStartErrorProcessing()

int32_t GPMC_eccBchStartErrorProcessing ( GPMC_Handle  handle,
uint8_t  sector 
)

Function to start error processing for a sector by ELM module.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
sectorSector number
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccBchCheckErrorProcessingStatus()

int32_t GPMC_eccBchCheckErrorProcessingStatus ( GPMC_Handle  handle,
uint32_t  sector 
)

Function to get error processing status for a sector by ELM module.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
sectorSector number
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccBchSectorGetError()

int32_t GPMC_eccBchSectorGetError ( GPMC_Handle  handle,
uint32_t  sector,
uint32_t *  errCount,
uint32_t *  errLoc 
)

Function to get number of errors per sector by ELM module.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
sectorSector number
errCountPointer to store number of errors in a sector
errLocPointer to store error locations in a sector
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccCalculateBchSyndromePolynomial()

int32_t GPMC_eccCalculateBchSyndromePolynomial ( GPMC_Handle  handle,
uint8_t *  pEccdata,
uint32_t  sector 
)

Function to compute BCH syndrome polynomial for NAND write operation.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
sectorSector number
pEccdataPointer to store BCH syndrome polynomial.
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccGetBchSyndromePolynomial()

int32_t GPMC_eccGetBchSyndromePolynomial ( GPMC_Handle  handle,
uint32_t  sector,
uint32_t *  bchData 
)

Function to get BCH syndrome polynomial per sector NAND read operation.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
sectorSector number
bchDataPointer to store BCH syndrome polynomial.
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_configurePrefetchPostWriteEngine()

int32_t GPMC_configurePrefetchPostWriteEngine ( GPMC_Handle  handle)

Function to configure GPMC PREFETCH read and POST write engine.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_disableFlashWriteProtect()

int32_t GPMC_disableFlashWriteProtect ( GPMC_Handle  handle)

Function to disable WRITE protect line.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_enableFlashWriteProtect()

int32_t GPMC_enableFlashWriteProtect ( GPMC_Handle  handle)

Function to disable WRITE protect line.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
Returns
SystemP_SUCCESS or SystemP_FAILURE

Variable Documentation

◆ gGpmcConfig

GPMC_Config gGpmcConfig[]
extern

Externally defined driver configuration array.

◆ gGpmcConfigNum

uint32_t gGpmcConfigNum
extern

Externally defined driver configuration array size.

gpmc.h